AM62Px MCU+ SDK  11.01.01

Detailed Description

Response for TISCI_MSG_MIN_CONTEXT_RESTORE.

Parameters
hdrTISCI header to provide ACK/NAK flags to the host.

This response is sent from the TIFS to the R5 SPL to indicate that now standard firmware can be executed. This response is sent after DDR firewalls have been fully restored by TIFS.

Data Fields

struct tisci_header hdr
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_min_context_restore_resp::hdr