AM62Px MCU+ SDK  11.01.01

Detailed Description

Response for TISCI_MSG_LPM_GET_NEXT_HOST_STATE.

Parameters
hdrTISCI header to provide ACK/NAK flags to the host.
stateThe expected state of host in selected low power mode.

Note: If the mode selection is not yet locked, this API returns invalid state.

Data Fields

struct tisci_header hdr
 
uint8_t state
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_lpm_get_next_host_state_resp::hdr

◆ state

uint8_t tisci_msg_lpm_get_next_host_state_resp::state