AM62Px MCU+ SDK  11.01.01

Detailed Description

Request for TISCI_MSG_FIRMWARE_LOAD.

Parameters
hdrTISCI header to provide ACK/NAK flags to the host.
image_addrSPS memory address to load FS stub from.
image_sizeSize of the FS stub image.

Data Fields

struct tisci_header hdr
 
uint32_t image_addr
 
uint32_t image_size
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_firmware_load_req::hdr

◆ image_addr

uint32_t tisci_msg_firmware_load_req::image_addr

◆ image_size

uint32_t tisci_msg_firmware_load_req::image_size