AM62Px MCU+ SDK  11.01.01

Detailed Description

Request for TISCI_MSG_DM_ABORT_SLEEP.

Parameters
hdrTISCI header to provide ACK/NAK flags to the host.

This message is sent from the DM firmware to the TIFS firmware during lpm suspend sequence to indicate that DM was not able to successfully suspend the SOC and DM is aborting the sleep cycle. On receiving this message TIFS will wake from WFI and the same message will be forwarded to the power master to wake it from WFI.

Data Fields

struct tisci_header hdr
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_dm_abort_sleep_req::hdr