AM62Px MCU+ SDK  11.01.01
SDL_ECC_InjectErrorConfig_t Struct Reference

Detailed Description


\brief This structure defines the inject error configuration

Data Fields

uint32_t * pErrMem
 
uint32_t flipBitMask
 
uint16_t chkGrp
 

Field Documentation

◆ pErrMem

uint32_t* SDL_ECC_InjectErrorConfig_t::pErrMem

Address to inject error

◆ flipBitMask

uint32_t SDL_ECC_InjectErrorConfig_t::flipBitMask

Bit location to flip bits

◆ chkGrp

uint16_t SDL_ECC_InjectErrorConfig_t::chkGrp

Group checker (for Interconnect RAM ID's only)