AM62Px MCU+ SDK  11.01.01
EnetUdma_SGListEntry Struct Reference

Detailed Description

Packet data structure.

This structure contains packet info used by application for getting/passing the packet data with DMA module.

Transmit Packet scatter gather list entry.

This structure contains info on scatter-gather fragments used for transmitting packets when packets are split into list of discontinuous fragments called scatter-gather list. Each sg list has a fragment of the packet

Data Fields

uint8_t * bufPtr
 
uint8_t * origBufPtr
 
uint32_t segmentFilledLen
 
uint32_t segmentAllocLen
 
bool disableCacheOps
 

Field Documentation

◆ bufPtr

uint8_t* EnetUdma_SGListEntry::bufPtr

Pointer to scatter fragment

This is applicable only to CPDMA devices. when ts_encap or vlan_encap are enabled the TimeStamp info and other packet encapsulated data will be prepended to the packet. As the buf ptr provided by CPDMA only points to the start of the buffer, CPDMA driver(Software) moves the bufPtr to point to the start of actual ethernet packet.

◆ origBufPtr

uint8_t* EnetUdma_SGListEntry::origBufPtr

Pointer to scatter fragment given by Hardware(UDMA). This change is added to align the SGList with CPDMA

◆ segmentFilledLen

uint32_t EnetUdma_SGListEntry::segmentFilledLen

Length of valid data in the scatter fragment

◆ segmentAllocLen

uint32_t EnetUdma_SGListEntry::segmentAllocLen

Length of allocated buffer for scatter fragment

◆ disableCacheOps

bool EnetUdma_SGListEntry::disableCacheOps