|
AM62Px MCU+ SDK
11.01.01
|
|
Go to the documentation of this file.
42 #ifndef SDL_SOC_POK_H_
43 #define SDL_SOC_POK_H_
44 #include <sdl/esm/sdl_ip_esm.h>
46 #include <sdl/include/am62px/sdlr_soc_baseaddress.h>
47 #include <sdl/include/am62px/sdlr_mcu_ctrl_mmr.h>
48 #include <sdl/include/am62px/sdlr_intr_wkup_esm0.h>
78 #define SDL_FIRST_POK_ID (0)
80 #define SDL_POK_VDDA_PMIC_IN_ID (SDL_FIRST_POK_ID)
82 #define SDL_POK_VDDS_DDRIO_ID (1)
84 #define SDL_POK_VDDR_CORE_ID (2)
86 #define SDL_POK_VMON_CAP_MCU_GENERAL_ID (3)
88 #define SDL_POK_VDDSHV_MAIN_1P8_ID (4)
90 #define SDL_POK_VDDSHV_MAIN_3P3_ID (5)
92 #define SDL_POK_VDD_MCU_OV_ID (6)
94 #define SDL_POR_VDDA_MCU_UV_ID (7)
96 #define SDL_POR_VDD_MCU_UV_ID (8)
98 #define SDL_POR_VDDA_MCU_OV_ID (9)
101 #define SDL_LAST_POK_ID (SDL_POR_VDDA_MCU_OV_ID)
107 #define SDL_POK_PRG_FIRST_ID (0)
109 #define SDL_POK_PRG_PP_0_ID (1)
111 #define SDL_POK_PRG_PP_1_ID (2)
114 #define SDL_POK_PRG_LAST_ID (SDL_POK_PRG_PP_1_ID)
119 #define SDL_POK_MMR_BASE (SDL_WKUP_CTRL_MMR1_CFG0_BASE)
120 #define MCU_ESM_INSTANCE (SDL_WKUP_ESM0_CFG_BASE)
121 #define MCU_ESM_INTID (SDLR_WKUP_ESM0_ESM_LVL_EVENT_ESM0_ESM_INT_HI_LVL_0)
123 #define MCU_ESM_ERR_SIG_VDDA_PMIC_IN_UV (SDLR_WKUP_ESM0_ESM_PLS_EVENT0_MCU_PRG_MCU0_POK_PGOOD_UV_OUT_N_TO_ESM_3)
124 #define MCU_ESM_ERR_SIG_VDD_MCU_UV (SDLR_WKUP_ESM0_ESM_PLS_EVENT0_MCU_PRG_MCU0_POK_PGOOD_UV_OUT_N_TO_ESM_0 )
125 #define MCU_ESM_ERR_SIG_VDD_MCU_OV (SDLR_WKUP_ESM0_ESM_PLS_EVENT0_MCU_PRG_MCU0_POK_PGOOD_UV_OUT_N_TO_ESM_4)
126 #define MCU_ESM_ERR_SIG_VDDS_DDRIO_UV (SDLR_WKUP_ESM0_ESM_PLS_EVENT0_MCU_PRG_MCU_5POKS0_POK_PGOOD_UV_OUT_N_TO_ESM_4)
127 #define MCU_ESM_ERR_SIG_VDDS_DDRIO_OV (SDLR_WKUP_ESM0_ESM_PLS_EVENT0_MCU_PRG_MCU_5POKS0_POK_PGOOD_OV_OUT_N_TO_ESM_4)
128 #define MCU_ESM_ERR_SIG_VDDR_CORE_UV (SDLR_WKUP_ESM0_ESM_PLS_EVENT0_MCU_PRG_MCU_5POKS0_POK_PGOOD_UV_OUT_N_TO_ESM_3)
129 #define MCU_ESM_ERR_SIG_VDDR_CORE_OV (SDLR_WKUP_ESM0_ESM_PLS_EVENT0_MCU_PRG_MCU_5POKS0_POK_PGOOD_OV_OUT_N_TO_ESM_3)
130 #define MCU_ESM_ERR_SIG_VMON_CAP_MCU_GENERAL_UV (SDLR_WKUP_ESM0_ESM_PLS_EVENT0_MCU_PRG_MCU_5POKS0_POK_PGOOD_UV_OUT_N_TO_ESM_2 )
131 #define MCU_ESM_ERR_SIG_VMON_CAP_MCU_GENERAL_OV (SDLR_WKUP_ESM0_ESM_PLS_EVENT0_MCU_PRG_MCU_5POKS0_POK_PGOOD_OV_OUT_N_TO_ESM_2)
132 #define MCU_ESM_ERR_SIG_VDDSHV_MAIN_1P8_UV (SDLR_WKUP_ESM0_ESM_PLS_EVENT0_MCU_PRG_MCU_5POKS0_POK_PGOOD_UV_OUT_N_TO_ESM_1)
133 #define MCU_ESM_ERR_SIG_VDDSHV_MAIN_1P8_OV (SDLR_WKUP_ESM0_ESM_PLS_EVENT0_MCU_PRG_MCU_5POKS0_POK_PGOOD_OV_OUT_N_TO_ESM_1)
134 #define MCU_ESM_ERR_SIG_VDDSHV_MAIN_3P3_UV (SDLR_WKUP_ESM0_ESM_PLS_EVENT0_MCU_PRG_MCU_5POKS0_POK_PGOOD_UV_OUT_N_TO_ESM_0)
135 #define MCU_ESM_ERR_SIG_VDDSHV_MAIN_3P3_OV (SDLR_WKUP_ESM0_ESM_PLS_EVENT0_MCU_PRG_MCU_5POKS0_POK_PGOOD_OV_OUT_N_TO_ESM_0)
136 #define MCU_ESM_ERR_SIG_VDDA_MCU_UV (SDLR_WKUP_ESM0_ESM_PLS_EVENT0_MCU_PRG_MCU0_POK_PGOOD_UV_OUT_N_TO_ESM_2)
137 #define MCU_ESM_ERR_SIG_VDDA_MCU_OV (SDLR_WKUP_ESM0_ESM_PLS_EVENT0_MCU_PRG_MCU0_POK_PGOOD_UV_OUT_N_TO_ESM_1)
141 #define ESM_ERR_SIG_VDDA_PMIC_IN_UV MCU_ESM_ERR_SIG_VDDA_PMIC_IN_UV
142 #define ESM_ERR_SIG_VDD_MCU_UV MCU_ESM_ERR_SIG_VDD_MCU_UV
143 #define ESM_ERR_SIG_VDD_MCU_OV MCU_ESM_ERR_SIG_VDD_MCU_OV
144 #define ESM_ERR_SIG_VDDS_DDRIO_UV MCU_ESM_ERR_SIG_VDDS_DDRIO_UV
145 #define ESM_ERR_SIG_VDDS_DDRIO_OV MCU_ESM_ERR_SIG_VDDS_DDRIO_OV
146 #define ESM_ERR_SIG_VDDR_CORE_UV MCU_ESM_ERR_SIG_VDDR_CORE_UV
147 #define ESM_ERR_SIG_VDDR_CORE_OV MCU_ESM_ERR_SIG_VDDR_CORE_OV
148 #define ESM_ERR_SIG_VMON_CAP_MCU_GENERAL_UV MCU_ESM_ERR_SIG_VMON_CAP_MCU_GENERAL_UV
149 #define ESM_ERR_SIG_VMON_CAP_MCU_GENERAL_OV MCU_ESM_ERR_SIG_VMON_CAP_MCU_GENERAL_OV
150 #define ESM_ERR_SIG_VDDSHV_MAIN_1P8_UV MCU_ESM_ERR_SIG_VDDSHV_MAIN_1P8_UV
151 #define ESM_ERR_SIG_VDDSHV_MAIN_1P8_OV MCU_ESM_ERR_SIG_VDDSHV_MAIN_1P8_OV
152 #define ESM_ERR_SIG_VDDSHV_MAIN_3P3_UV MCU_ESM_ERR_SIG_VDDSHV_MAIN_3P3_UV
153 #define ESM_ERR_SIG_VDDSHV_MAIN_3P3_OV MCU_ESM_ERR_SIG_VDDSHV_MAIN_3P3_OV
154 #define ESM_ERR_SIG_VDDA_MCU_UV MCU_ESM_ERR_SIG_VDDA_MCU_UV
155 #define ESM_ERR_SIG_VDDA_MCU_OV MCU_ESM_ERR_SIG_VDDA_MCU_OV
161 #define ESM_INSTANCE MCU_ESM_INSTANCE
162 #define ESM_INTID MCU_ESM_INTID
int8_t SDL_PRG_Inst
Definition: sdl_soc_pok.h:104
uint8_t instance
Definition: tisci_dkek.h:1
SDL_POK_InstanceType
Definition: sdl_soc_pok.h:169
This file contains the SDL DPL API's.
@ SDL_POK_MCU_CTRL_MMR0
Definition: sdl_soc_pok.h:170
bool SDL_POK_getBaseaddr(SDL_POK_InstanceType instance, uint32_t *pbaseAddress)
int8_t SDL_POK_Inst
Definition: sdl_soc_pok.h:75