AM62Px MCU+ SDK  11.01.01
pok/v1/sdl_pok.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) Texas Instruments Incorporated 2023-25
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  *
32  */
33 
47 #ifndef SDL_POK_H_
48 #define SDL_POK_H_
49 
50 /* ========================================================================== */
51 /* Include Files */
52 /* ========================================================================== */
53 
54 #include <sdl/dpl/sdl_dpl.h>
55 #include <sdl/pok/v1/sdl_pok_def.h>
56 #include <sdl/pok/v1/sdl_ip_pok.h>
57 
58 #ifdef __cplusplus
59 extern "C" {
60 #endif
61 
62 /* ========================================================================== */
63 /* Macros & Typedefs */
64 /* ========================================================================== */
65 
66 /* None */
67 
68 /* ========================================================================== */
69 /* Structure & Enumeration Declarations */
70 /* ========================================================================== */
71 
102 typedef struct SDL_Pok_Static_Reg_read{
103  uint8_t hystCtrl;
105  uint8_t hystCtrlOV;
107  uint8_t voltDetMode;
109  uint8_t trim;
111  uint8_t trimOV;
113  uint8_t deglitch;
115  bool porBGapOK;
120 
121 /* ========================================================================== */
122 /* Function Declarations */
123 /* ========================================================================== */
124 
135 int32_t SDL_POK_enablePP(SDL_PRG_Inst instance, bool enable);
136 
151 
162 
176 
179 /* ========================================================================== */
180 /* Static Function Definitions */
181 /* ========================================================================== */
182 
183 /* None */
184 
185 /* ========================================================================== */
186 /* Internal/Private Structure Declarations */
187 /* ========================================================================== */
188 
189 /* None */
190 
191 #ifdef __cplusplus
192 }
193 #endif
194 
195 #endif /* SDL_POK_H_ */
sdl_pok_def.h
Header file containing various enumerations, structure definitions and function declarations for the ...
SDL_POK_staticRegs::porBGapOK
bool porBGapOK
Definition: pok/v1/sdl_pok.h:115
SDL_POK_staticRegs::hystCtrl
uint8_t hystCtrl
Definition: pok/v1/sdl_pok.h:103
SDL_PRG_Inst
int8_t SDL_PRG_Inst
Definition: sdl_soc_pok.h:104
instance
uint8_t instance
Definition: tisci_dkek.h:1
SDL_POK_config
POK Configuration structure.
Definition: sdl_pok_def.h:418
SDL_POK_getStaticRegisters
int32_t SDL_POK_getStaticRegisters(SDL_POK_Inst instance, SDL_POK_staticRegs *pStaticRegs)
POK Function to get the Static Registers. This function reads the values of the static registers such...
SDL_POK_staticRegs
POK Static Registers structure.
Definition: pok/v1/sdl_pok.h:102
sdl_dpl.h
This file contains the SDL DPL API's.
SDL_POK_staticRegs::hystCtrlOV
uint8_t hystCtrlOV
Definition: pok/v1/sdl_pok.h:105
SDL_POK_staticRegs::trimOV
uint8_t trimOV
Definition: pok/v1/sdl_pok.h:111
SDL_POK_verifyConfig
int32_t SDL_POK_verifyConfig(SDL_POK_Inst instance, SDL_POK_config *pConfig)
POK Function to verify the written configuration. This function checks the provided config against th...
SDL_POK_staticRegs::trim
uint8_t trim
Definition: pok/v1/sdl_pok.h:109
SDL_POK_staticRegs::voltDetMode
uint8_t voltDetMode
Definition: pok/v1/sdl_pok.h:107
SDL_POK_staticRegs::deglitch
uint8_t deglitch
Definition: pok/v1/sdl_pok.h:113
SDL_POK_staticRegs::porModuleStatus
uint8_t porModuleStatus
Definition: pok/v1/sdl_pok.h:117
SDL_POK_enablePP
int32_t SDL_POK_enablePP(SDL_PRG_Inst instance, bool enable)
POK Function to enable or disable ping/pong mode for a specified PRG. Only supported for v1 version o...
SDL_POK_init
int32_t SDL_POK_init(SDL_POK_Inst instance, SDL_POK_config *pConfig)
POK module configuration API.
SDL_POK_Inst
int8_t SDL_POK_Inst
Definition: sdl_soc_pok.h:75