AM62Px MCU+ SDK  11.01.01
ECC_AGGR Data Structures

Introduction

Data Structures

struct  SDL_ECC_InitConfig_t
 
struct  SDL_ECC_InjectErrorConfig_t
 
struct  SDL_ECC_ErrorInfo_t
 
struct  SDL_Ecc_AggrErrorInfo
 This structure contains error forcing information used by the SDL_ecc_aggrForceEccRamError function. More...
 
struct  SDL_Ecc_AggrEccRamErrorStatusInfo
 This structure contains error status information returned by the SDL_ecc_aggrGetEccRamGetErrorStatus function. More...
 
struct  SDL_Ecc_AggrEDCInterconnectErrorInfo
 This structure contains error forcing information used by the SDL_ecc_aggrForceEDCInterconnectError function. More...
 
struct  SDL_Ecc_AggrEDCInterconnectErrorStatusInfo
 This structure contains error status information returned by the SDL_ecc_aggrGetEDCInterconnectErrorStatus function. More...
 
struct  SDL_ecc_aggrEnableCtrl
 This structure contains the ECC aggr enable error config. More...
 
struct  SDL_ecc_aggrStatusCtrl
 This structure contains the ECC aggr status config. More...
 
struct  SDL_ECC_staticRegs
 This structure contains the static register group for Ecc aggregator used by the SDL_ecc_aggrReadStaticRegs function. More...