|
AM62Px MCU+ SDK
11.01.01
|
|
Go to the documentation of this file.
47 #ifndef ENET_MOD_STATS_H_
48 #define ENET_MOD_STATS_H_
66 #define ENET_STATS_PUBLIC_IOCTL(x) (ENET_IOCTL_TYPE_PUBLIC | \
67 ENET_IOCTL_STATS_BASE | \
77 typedef enum EnetStats_Ioctl_e
154 #if ENET_CFG_IS_ON(CPSW_NPAC_PORT)
@ ENET_STATS_IOCTL_GET_VERSION
Get the hardware version of the Stats module.
Definition: enet_mod_stats.h:86
@ ENET_STATS_IOCTL_PRINT_REGS
Print Stats registers.
Definition: enet_mod_stats.h:95
#define ENET_STATS_PUBLIC_IOCTL(x)
Helper macro to create IOCTL commands for STATS module.
Definition: enet_mod_stats.h:66
@ ENET_STATS_IOCTL_RESET_HOSTPORT_STATS
Reset host port statistics.
Definition: enet_mod_stats.h:140
@ ENET_STATS_IOCTL_GET_HOSTPORT_STATS
Get host port statistics.
Definition: enet_mod_stats.h:111
@ ENET_STATS_IOCTL_GET_MACPORT_STATS
Get MAC port statistics.
Definition: enet_mod_stats.h:126
EnetStats_Ioctl
Statistics IOCTL commands.
Definition: enet_mod_stats.h:78
@ ENET_STATS_IOCTL_RESET_MACPORT_STATS
Reset MAC port statistics.
Definition: enet_mod_stats.h:153
This file contains the type definitions and helper macros for the Enet Module interface.