AM62Px MCU+ SDK  11.01.01
DSS Safety Test

Introduction

This example tests the Freeze frame detection and Data integrity check safety features for video pipeline and video port. DSS supports the following safety check regions to implement the safety features:

  • Video pipelines: One safety check region at the output of each video pipeline.
  • Video port outputs: Up to four sub-regions within the active video output area of the final display output of each video port.

The safety region in the video pipeline captures data only if the embedded alpha data is not equal to 0 (that is, non-transparent pixels). The safety regions in the display video port output captures all active video pixels within the region boundary. The (up to four) regions in the display output should be typically non-overlapping areas of the screen, but the hardware does not restrict them to be non-overlapping.

The example configures freeze frame detection for two regions and data integrity check for rest of the two regions on Video port. The example also configures data integrity check for VIDL piepline. The data integrity check failure is created by corruting frame buffer so that previous frame buffer is different from current frame buffer.

Safety region configurations are available as part of driver sysconfig feature shown below.

Video Port Safety Region

Video Pipeline Safety Region

The example configures OLDI LVDS panel for Video Port 1. Please refer SK-LCD1 for panel details. The Video port timinng parameters are configured with respect to SK-LCD1. Timing parameters can be configured using sysconfig option.

The example integrates bootloading funtionality with SBL on OSPI bootmedia. It also integrates Device manager functionality. The SBL stage 2 thread boots all the cores along with HLOS like Linux. Refer SBL Booting Linux From OSPI for boot flow sequence.

Supported Combinations

Parameter Value
CPU + OS wkup-r5fss0-0 freertos
Toolchain ti-arm-clang
Board am62px-sk
Example folder examples/drivers/dss/dss_safety_test

Steps to Run the Example

  • This example integrates SBL on OSPI bootmedia which needs to be flashed on the EVM flash, along with sample application images for MCU R5 CPUs, HSM M4F and Linux Appimage.
  • There is a default flash config file as shown below which flashes this SBL and the IPC RPMsg Linux echo applications
      ${SDK_INSTALL_PATH}/tools/boot/sbl_prebuilt/am62px-sk/default_sbl_ospi_linux_hs_fs.cfg
    
  • Update the wkup-r5 image in the flash config with dss_safety_test image.
      # 2nd stage bootloader with DM is flashed at 0x80000 or to whatever offset your bootloader is configured for
      --file=../../examples/drivers/dss/dss_safety_test/am62px-sk/wkup-r5fss0-0_freertos/ti-arm-clang/dss_safety_test.release.appimage.hs_fs --operation=flash --flash-offset=0x80000
    
  • To flash to the EVM, refer to Flash a Hello World example . Only when giving the flash config file, point to the default_sbl_ospi_linux_hs_fs.cfg shown above.
  • Example, assuming SDK is installed at C:/ti/mcu_plus_sdk and this example and IPC application is built using makefiles, and Linux Appimage is already created, in Windows,
        cd C:/ti/mcu_plus_sdk/tools/boot
        python uart_uniflash.py -p COM13 --cfg=C:/ti/mcu_plus_sdk/tools/boot/sbl_prebuilt/am62px-sk/default_sbl_ospi_linux_hs_fs.cfg
    
  • If Linux PC is used, assuming SDK is installed at ~/ti/mcu_plus_sdk
      cd ~/ti/mcu_plus_sdk
      python uart_uniflash.py -p /dev/ttyUSB0 --cfg=~/ti/mcu_plus_sdk/tools/boot/sbl_prebuilt/am62px-sk/default_sbl_ospi_linux_hs_fs.cfg
    
  • Switch to OSPI NOR BOOT MODE and power on the EVM.
Attention
As the wake-up R5 is the device manager, it needs to be started by the SBL. So it can not be loaded through CCS. It should be flashed and booted through SBL.

See Also

DSS

Sample Output

Sciserver Testapp Built On: Dec 7 2023 14:12:00
Sciserver Version: v2023.11.0.0REL.MCUSDK.MM.NN.PP.bb
RM_PM_HAL Version: vMM.NN.PP
Starting Sciserver..... PASSED
DispApp_init() - DONE !!!
DSS display application started...
Display create complete!!
Starting display ... !!!
Display in progress ... DO NOT HALT !!!
Underflow did not occur
Underflow did not occur
Sync Lost did not occur
Display delete complete!!
DispApp_deInit() - DONE !!!
****************************************************
Safety Data Log Region : 0
Safety Data VP ID: VP1
Safety Check Interupt Trigger: TRUE
Safety Check Mode: FRAME_FREEZE_DETECT
Safety Data Frame count: 13
Safety Data Captured Signature: 0xCCFA10E0
****************************************************
Safety Data Log Region : 1
Safety Data VP ID: VP1
Safety Check Interupt Trigger: TRUE
Safety Check Mode: FRAME_FREEZE_DETECT
Safety Data Frame count: 33
Safety Data Captured Signature: 0x7FE99F52
****************************************************
Safety Data Log Region : 2
Safety Data VP ID: VP1
Safety Check Interupt Trigger: TRUE
Safety Check Mode: DATA_INTEGRITY
Safety Data Frame count: 73
Safety Data Captured Signature: 0x5576A020
****************************************************
Safety Data Log Region : 3
Safety Data VP ID: VP1
Safety Check Interupt Trigger: TRUE
Safety Check Mode: DATA_INTEGRITY
Safety Data Frame count: 73
Safety Data Captured Signature: 0xCD822043
****************************************************
Safety Data Pipeline ID: VID1
Safety Check Interupt Trigger: TRUE
Safety Check Mode: FRAME_FREEZE_DETECT
Safety Data Frame count: 53
Safety Data Captured Signature: 0xF6BA4989
****************************************************
Safety Data Pipeline ID: VIDL1
Safety Check Interupt Trigger: TRUE
Safety Check Mode: DATA_INTEGRITY
Safety Data Frame count: 73
Safety Data Captured Signature: 0xC948AD61
DSS Safety Test Passed!!