The Release package consists of MCAL Drivers & Applications for J722S device. The MCAL modules are compliant to AUTOSAR specification versioned 4.3.1.
Refer to MCUSW_MCAL_10.00.00_manifest.html at top level.
The[Link] for User Guide provides the documentation and references necessary to begin development on TI's platforms using J722S.
User shall refer MCU+SDK from below links provided.
|
Variant |
Link |
|
J722S |
Refer to following documentation for further details:
|
J722S
MCAL User Guide |
This
document details Supported driver, Installation, Dependencies, Build
instructions, Steps to run example applications, Module Specific User Guides
and others |
|
|
MCAL
Configurator User Guide |
Refer
this before attempting to reconfigure MCAL modules. This includes steps to
Install Configurator (EB), Configurator Licensing, Generation of MCAL
Configurations and others |
|
|
MCAL
Compliance Support Package |
Refer
to this for Safety Compliance collateral such as Design Documents, Test
Reports, Static Analysis Reports, Dynamic Analysis Reports. |
This
can be found at {mcusw/csp/Common/SoC
Integration Package/SOC_NAME/} |
Configurator package name is
MCUSW_10_00_00_06_CONFIG-windows-installer.exe, and contains following items:
Please refer to J722S MCAL User Guide for further instructions on access to this configurator.
|
Modules/Topic |
Compatibility |
Remarks |
|
TI Arm Clang Compiler |
V3.2.2 |
NA |
|
EB Tresos
Studio |
V24.0.0 |
NA |
|
Build |
gmake |
NA |
|
MCU+ SDK |
mcu_plus_sdk_10_00_00_25 |
The MCAL examples are built
and validated on mcu_plus_sdk_10_00_00_25 version. Refer to respective
version of MCU+SDK User Guide to setup the EVM. |
IMPORTANT NOTE: User should
ensure to use below modules version for MCUSW_J7AEN_10.00.00.01 release. User should take care to not mis-match
or mix-and-match the versions with various MCUSW releases. Bundle Version of
all plugins is 10.0.0.
|
Module |
Previous Module
Version |
Current Module
Version |
Remarks |
|
CAN |
9.1.0 |
10.0.0 |
User should generate Configuration again |
|
CDD IPC |
10.0.1 |
11.0.0 |
User should generate Configuration again |
|
DIO |
10.0.0 |
10.1.0 |
Minor Bug Fix . Refer to "Fixed Defects" |
|
GPT |
9.0.1 |
9.0.1 |
None |
|
MCU |
9.1.1 |
10.0.0 |
User should generate Configuration again |
|
SPI |
9.0.1 |
9.0.1 |
None |
|
FLS |
10.1.0 |
10.1.0 |
None |
|
WDG |
9.0.0 |
9.1.0 |
Minor version Update |
|
ETH |
9.2.0 |
10.0.0 |
Bug fixes, errata i2443 workaround. |
|
ETH TRCV |
9.2.0 |
10.0.0 |
Minor Bug Fix . Refer to
"Fixed Defects" |
|
OS |
9.0.1 |
9.0.1 |
None |
|
EcuM |
9.0.0 |
9.0.0 |
None. |
|
DEM |
9.0.0 |
9.0.0 |
None. |
|
SoC |
HOST (OS) |
Test Platform |
|
J722S |
Windows / Linux, EB
configurator only on Windows |
J722S |
|
ID |
Issue Summary |
|
Errata
i2443: CPSW: Ethernet to Host Timestamp Issue |
|
|
Am62x:
Eth freertos app crash with latest sdk |
|
|
ETh apps build errors |
|
|
CanSetBaudrateApi given as list in MCAL Plugins instead of parameter |
|
|
EthTrcv: Dem Error STD_ON/OFF should be added in all template |
|
|
Eth:
Dem Error STD_ON/OFF should be added in all template |
|
|
Fls : Fls_Brd_Nor
file contain Fee_Cbk.h included |
|
|
Eth : EthIf_TxConfirmation API is not
called under ETH_WRAPPER_ENABLED flag. |
|
|
Eth : Eth_setDemEventStatus Private Api should be under check and enabled only if DEM is
enabled. |
|
|
"Mcu_SetMode" API not implemented as per Autosar |
|
|
CAN
driver does not include 'CanSetBaudrateApi' to
enable/disable Can_SetBaudRate() API |
|
|
Debug
binaries not working on latest mcusw master tag : MCAL_SitaraMPU_09.02.00.03 |
|
|
Fls_App_Indac and FLS_App_Dac examples are
failing for SDR mode |
|
|
Cdd_Ipc : When DEM error generation
is enabled then build fails |
|
|
Mcu : In Mcu
configuration for McuClockSettingConfig , ModuleName and ModuleClockId
have missing modules |
|
|
Wdg: SetTrigger condition not
reloading the WDT down counter |
|
|
Build
issue in ETH in case of IqrType selected as CAT1 |
|
|
Cdd_Ipc : CddIrqType
as the configurable parameter don't contain option to select CAT1/VOID |
|
|
"CAN_ISR_TEXT_SECTION"
is being added before ISR API definition |
|
|
In
Can_PBcfg.c file CAN_START_SEC_ISR_CODE defined
prior to CAN_STOP_SEC_CONFIG_DATA |
|
|
MCU
Get reset reason for POR is not supported due to the recommended Reset
sequence is not followed. |
|
|
IPC-CDD:
Validation of DM R5 is pending due to issue in core communication |
|
ID |
Variant |
Severity |
Summary |
Comments |
|
MCAL-25355 |
J722S |
S3-Minor |
EthTrcv: App Half Duplex Manual Mode Fail |
eth_trcv_test_app currently will run test in loopback mode regardless of configurations, which will cause the test to fail if the user sets the configuration in manual mode with half duplex. Example application issue, no functionality affected. |
|
MCAL-25830 |
J722S |
S3-Minor |
SPI
logging feature not usable with Vector Microsar OS |
User
Shall disable logging feature in SPI Configuration. |
|
MCAL-25451 |
J722S |
S3-Minor |
Warning
Observed in MCU module while loading plugins in EB Tresos |
These warning are observed
for mcu clock src id in
the XDM. These do not impact functionality. |
|
MCAL-24838 |
J722S |
S3-Minor |
Mcu API Mcu_GetPllStatus always
returns MCU_PLL_STATUS_UNDEFINED |
- |
|
ID |
Description |
Workaround |
Comments |
|
None |
|
|
|
For technical support and
additional assistance, visit E2E or contact local TI Field Application
Engineer.
@Copyright 1995-2024, Texas Instruments Incorporated.
All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale