MCUSW
Can_RegisterReadbackType Struct Reference

Detailed Description

Register Readback Structure.

Structure to read back key CAN control registers.

The Safety API to readback CAN register vales will populate this structure

Data Fields

uint32 CanReadBackRegPID
 
uint32 CanReadBackRegSTAT
 
uint32 CanReadBackRegCREL
 
uint32 CanReadBackRegENDN
 
uint32 CanReadBackRegCTRL
 
uint32 CanReadBackRegRWD
 
uint32 CanReadBackRegCCCR
 
uint32 CanReadBackRegTDCR
 
uint32 CanReadBackRegGFC
 
uint32 CanReadBackRegSIDFC
 
uint32 CanReadBackRegXIDFC
 
uint32 CanReadBackRegRXF0C
 
uint32 CanReadBackRegRXBC
 
uint32 CanReadBackRegRXF1C
 
uint32 CanReadBackRegTXBC
 
uint32 CanReadBackRegTXESC
 
uint32 CanReadBackRegTXEFC
 
uint32 CanReadBackRegRXESC
 
uint32 CanReadBackRegXIDAM