![]() |
MCUSW
|
ADC log structure per group entry.
Data Fields | |
| uint32 | timeStamp |
| Adc_GroupType | groupId |
| Adc_HWUnitType | hwUnitId |
| uint32 | isReScheduled |
| uint32 Adc_GroupLogEntryType::timeStamp |
Timestamp based on 32-kHz Synchronized Timer (COUNTER_32K) at which the group is scheduled
| Adc_GroupType Adc_GroupLogEntryType::groupId |
Group ID of the scheduled group
| Adc_HWUnitType Adc_GroupLogEntryType::hwUnitId |
HWUnit associated with the group
| uint32 Adc_GroupLogEntryType::isReScheduled |
This will be set to TRUE is a group is rescheduled when a higher priority task pre-empts this group