![]() |
MCUSW
|
Structure containing parameters for ADC MCAL channel configuration. In term of ADC hardware, this represents the step configuration. There are ADC_NUM_CHANNEL steps in the ADC hardware and each step could be mapped to an actual hardware input channel.
Data Fields | |
| uint32 | hwChannelId |
| uint32 | openDelay |
| uint32 | sampleDelay |
| uint32 | rangeCheckEnable |
| Adc_AveragingMode | averagingMode |