![]() |
MCUSW
|
AUTOSAR (AUTomotive Open System ARchitecture) is an open and standardized automotive software architecture jointly developed by automobile manufacturers, suppliers, and tool developers. AUTOSAR focuses on strategic targets such as modularity, configurability, and transferability of software modules, and the standardization of their interfaces.
AUTOSAR is based on the concept of separation between infrastructure and application. AUTOSAR software component implementation is independent from the infrastructure.
Autosar infrastructure consists of the following layers:
MicroController Abstraction Layer (MCAL) is a software module enabling direct access to on-chip MCU peripheral modules and making the upper software layer independent of the MCU.
The Microcontroller Abstraction Layer (MCAL) is the lowest layer of the AUTOSAR Basic Software architecture. MCAL contains drivers with direct access to the microcontroller internal peripherals and memory-mapped microcontroller external devices. MCAL is hardware-specific, ensuring a standard interface to the Basic Software. It manages the microcontroller peripherals and provides the components of the Basic Software with microcontroller-independent values. MCAL also implements notification mechanisms to support the distribution of commands, responses, and information to processes.
Fig. 1.1: AUTOSAR MCAL Layer
MCAL software (part of the package that includes the hardware platform) must be configured for the specific automotive application. For example, a CAN BUS (MCAL) driver needs to be configured for in-vehicle networking; similarly, drivers like LIN BUS, FlexRay, PWM, SPI, and Ethernet must be configured based on the application’s needs.
Configuration of these drivers is carried out by specialized code generation and configuration tools (for example, EB Tresos). The source files generated by such tools contain structures with elements like configuration values, based on the Parameter Definition File. These values are then fed to peripheral registers, address pointers, macro definitions, etc.
The MCAL drivers implement the software specification from AUTOSAR 4.3.1. Additionally, examples demonstrating MCAL driver usage have been included.
CDD stands for Complex Device Drivers. A Complex Driver is a software entity that provides for the integration of special-purpose functionality/drivers not defined in AUTOSAR. A CDD resides in the Complex Drivers Layer of the Basic Software and interacts with standard BSW modules or the RTE.

Fig. 1.2: CDD in Layered Software Architecture
The main goal of the CDD is to implement complex sensor evaluation and actuator control with direct access to the microcontroller (via specific interrupts or complex microcontroller peripherals, external devices, etc.) to fulfill special functional and timing requirements. In addition, it might be used to implement enhanced services / protocols or to encapsulate legacy functionality of a non-AUTOSAR system.
CDD implementation may be application-, microcontroller-, and ECU-dependent. Lastly, the CDD can serve as a mechanism of migration to introduce existing or new concepts into the AUTOSAR Software Architecture.
Refer to AUTOSAR_EXP_LayeredSoftwareArchitecture for more details on CDD-related configurations.
MCAL is a collective package of Safety Certified Driver Modules (ASIL D/B depending on the device), developed with a process certified for ISO 26262 compliance.
Drivers implement hardware safety mechanisms (as listed in the HW Safety Manual) to address random faults.
The Software Compliance Support Package (CSP) is the collection of documentation that TI offers to help customers with their certification processes for the integrated system. CSP will be made available in mySecure SW as an independent package two weeks after the official MCAL release.
The CSP helps customers qualify MCAL in their system context. This is necessary if the software is modified or the tooling changed such that TI’s functional safety assessment of MCAL is invalidated.
Each HW IP Module MCAL driver has its own CSP for customers.
TI offers MCAL and CDD drivers (source code) for MCU devices, along with a licensed Configurator Package. The rest of the AUTOSAR Basic Software is provided by various AUTOSAR vendors (Vector, Elektrobit, ETAS, etc.).

Fig. 1.3: Software Offering
Customers receive:
The customer then integrates these deliverables based on integration guides from the AUTOSAR vendor and TI. Back To Top