MCUSW
ADC Handler and Driver API

Introduction

The ADC Driver MCAL provides low level access to ADC peripheral present on Device.
The ADC Driver implements a standardized interface specified in the AUTOSAR_SWS_ADCDriver document.

Only the following combinations of modes are supported:

Following combinations of modes are not supported:

See also
ADC Configuration

Sub Modules

 ADC Configuration
 

Data Structures

struct  Adc_GroupLogEntryType
 ADC log structure per group entry. More...
 

ADC Driver Module SW Version Info

Defines for ADC Driver version used for compatibility checks

#define ADC_SW_MAJOR_VERSION   (9U)
 Driver Implementation Major Version. More...
 
#define ADC_SW_MINOR_VERSION   (2U)
 Driver Implementation Minor Version. More...
 
#define ADC_SW_PATCH_VERSION   (0U)
 Driver Implementation Patch Version. More...
 

ADC Driver Module AUTOSAR Version Info

Defines for ADC Driver AUTOSAR version used for compatibility checks

#define ADC_AR_RELEASE_MAJOR_VERSION   (4U)
 AUTOSAR Major version specification implemented by ADC Driver. More...
 
#define ADC_AR_RELEASE_MINOR_VERSION   (3U)
 AUTOSAR Minor version specification implemented by ADC Driver. More...
 
#define ADC_AR_RELEASE_REVISION_VERSION   (1U)
 AUTOSAR Patch version specification implemented by ADC Driver. More...
 

ADC Driver ID Info

#define ADC_VENDOR_ID   ((uint16) 44U)
 Texas Instruments Vendor ID. More...
 
#define ADC_MODULE_ID   ((uint16) 123U)
 ADC Driver Module ID. More...
 
#define ADC_INSTANCE_ID   ((uint8) 0U)
 ADC Driver Instance ID. More...
 
#define ADC_DEF_CHANNEL_RESOLUTION   ((Adc_ResolutionType) 12U)
 The default channel resolution supported by the current ADC hardware. No other value is supported by the hardware. More...
 
#define ADC_NUM_CHANNEL   (10U)
 Number of MCAL channels - in terms of ADC HW, this represents the number of hardware steps. Note: In terms of ADC IP number of steps is 16. Due to AUTOSAR specification, the channel ID's should be unique i.e each channel Id and actual HW channel should have one to one mapping. So ADC_NUM_CHANNEL is fixed to 9 as number of actual HW channels available is also 9. More...
 
#define ADC_MIN_CHANNEL_ID   (0U)
 Minimum value of channel ID. More...
 
#define ADC_MAX_CHANNEL_ID   (ADC_NUM_CHANNEL - 1U)
 Maximum value of channel ID. More...
 
#define ADC_NUM_HW_CHANNEL   (10U)
 Number of actual HW channels - in terms of ADC HW, this represents the actual channel input to the ADC module. Note: This is a fixed value as per the ADC module and can't be changed. More...
 
#define ADC_MIN_HW_CHANNEL_ID   (0U)
 Minimum value of HW channel ID. More...
 
#define ADC_MAX_HW_CHANNEL_ID   (ADC_NUM_HW_CHANNEL - 1U)
 Maximum value of HW channel ID. More...
 
#define ADC_MIN_OPEN_DELAY   (0x00U)
 Minimum value of open delay. More...
 
#define ADC_MAX_OPEN_DELAY   (0x3FFFFU)
 Maximum value of open delay. More...
 
#define ADC_MIN_SAMPLE_DELAY   (0x00U)
 Minimum value of sample delay. More...
 
#define ADC_MAX_SAMPLE_DELAY   (0xFFU)
 Maximum value of sample delay. More...
 
#define ADC_MIN_RANGE   (0x00U)
 Minimum value of range. More...
 
#define ADC_MAX_RANGE   (0xFFFU)
 Maximum value of range. More...
 

ADC Error Codes

Error codes returned by ADC functions

typedef uint8 Adc_ChannelType
 Numeric ID of an ADC channel. More...
 
typedef uint8 Adc_GroupType
 Numeric ID of an ADC channel group. More...
 
typedef uint32 Adc_ValueGroupType
 Type for reading the converted values of a channel group (raw, without further scaling, right aligned). More...
 
typedef uint32 Adc_PrescaleType
 Type of clock prescaler factor. More...
 
typedef uint16 Adc_ConversionTimeType
 Type of conversion time, i.e. the time during which the sampled analogue value is converted into digital representation. More...
 
typedef uint16 Adc_SamplingTimeType
 Type of sampling time, i.e. the time during which the value is sampled (in clockcycles). More...
 
typedef uint8 Adc_ResolutionType
 Type of channel resolution in number of bits. More...
 
typedef uint8 Adc_GroupPriorityType
 Priority level of the channel. Lowest priority is 0. More...
 
typedef uint32 Adc_GroupDefType
 Type of assignment of channels to a channel group. More...
 
typedef uint16 Adc_StreamNumSampleType
 Type for configuring the number of group conversions in streaming access mode (in single access mode, parameter is 1). More...
 
typedef uint8 Adc_HwTriggerTimerType
 Type for the value of the ADC module embedded timer. More...
 
typedef uint8 Adc_HWUnitType
 Specifies the identification (ID) for a ADC Hardware microcontroller peripheral (unit) More...
 
typedef uint8 Adc_RefSelType
 Specifies the Reference select for functional internal diagnostic debug mode. More...
 
#define ADC_E_UNINIT   ((uint8) 0x0AU)
 API service used without module initiali-zation. More...
 
#define ADC_E_BUSY   ((uint8) 0x0BU)
 API service called during ongoing process. More...
 
#define ADC_E_IDLE   ((uint8) 0x0CU)
 API service called while no conversion is ongoing. More...
 
#define ADC_E_ALREADY_INITIALIZED   ((uint8) 0x0DU)
 API Adc_Init service called while the ADC driver has already been initialized. More...
 
#define ADC_E_PARAM_CONFIG   ((uint8) 0x0EU)
 API service called with incorrect configuration parameter. More...
 
#define ADC_E_PARAM_POINTER   ((uint8) 0x14U)
 API servcie called with invalid data buffer pointer. More...
 
#define ADC_E_PARAM_GROUP   ((uint8) 0x15U)
 API servcie called with invalid group ID. More...
 
#define ADC_E_WRONG_CONV_MODE   ((uint8) 0x16U)
 API servcie called on a group with conversion mode configured as continuous. More...
 
#define ADC_E_WRONG_TRIGG_SRC   ((uint8) 0x17U)
 API servcie called for group with wrong trigger source. More...
 
#define ADC_E_NOTIF_CAPABILITY   ((uint8) 0x18U)
 Enable/disable notification function for a group whose configuration set has no notification available. More...
 
#define ADC_E_BUFFER_UNINIT   ((uint8) 0x19U)
 Conversion started and result buffer pointer is not initialized. More...
 
#define ADC_E_NOT_DISENGAGED   ((uint8) 0x1AU)
 One or more ADC group/channel not in IDLE state. More...
 
#define ADC_E_POWER_STATE_NOT_SUPPORTED   ((uint8) 0x1BU)
 Unsupported power state request. More...
 
#define ADC_E_TRANSITION_NOT_POSSIBLE   ((uint8) 0x1CU)
 Requested power state can not be reached directly. More...
 
#define ADC_E_PERIPHERAL_NOT_PREPARED   ((uint8) 0x1DU)
 ADC not prepared for target power state. More...
 

ADC Service Ids

The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error

typedef P2FUNC (void, ADC_APPL_CODE, Adc_GroupEndNotifyType)(void)
 Typedef for group end notification function pointer. More...
 
 FUNC (void, ADC_CODE) Adc_Init(P2CONST(Adc_ConfigType
 Service for ADC initialization. More...
 
 FUNC (Std_ReturnType, ADC_CODE) Adc_SetupResultBuffer(Adc_GroupType Group
 This service initializes ADC driver with the group specific result buffer start address where the conversion results will be stored. More...
 
 FUNC (Adc_StatusType, ADC_CODE) Adc_GetGroupStatus(Adc_GroupType Group)
 Returns the conversion status of the requested ADC Channel group. More...
 
 FUNC (Adc_StreamNumSampleType, ADC_CODE) Adc_GetStreamLastPointer(Adc_GroupType Group
 Returns the number of valid samples per channel, stored in the result buffer. More...
 
 P2VAR (Adc_RegisterReadbackType, AUTOMATIC, ADC_APPL_DATA) RegRbPtr)
 
#define ADC_SID_INIT   ((uint8) 0x00U)
 Adc_Init() API Service ID. More...
 
#define ADC_SID_DEINIT   ((uint8) 0x01U)
 Adc_DeInit() API Service ID. More...
 
#define ADC_SID_START_GROUP_CONVERSION   ((uint8) 0x02U)
 Adc_StartGroupConversion() API Service ID. More...
 
#define ADC_SID_STOP_GROUP_CONVERSION   ((uint8) 0x03U)
 Adc_StopGroupConversion() API Service ID. More...
 
#define ADC_SID_READ_GROUP   ((uint8) 0x04U)
 Adc_ReadGroup() API Service ID. More...
 
#define ADC_SID_ENABLE_HARDWARE_TRIGGER   ((uint8) 0x05U)
 Adc_EnableHardwareTrigger() API Service ID. More...
 
#define ADC_SID_DISABLE_HARDWARE_TRIGGER   ((uint8) 0x06U)
 Adc_DisableHardwareTrigger() API Service ID. More...
 
#define ADC_SID_ENABLE_GROUP_NOTIFICATION   ((uint8) 0x07U)
 Adc_EnableGroupNotification() API Service ID. More...
 
#define ADC_SID_DISABLE_GROUP_NOTIFICATION   ((uint8) 0x08U)
 Adc_DisableGroupNotification() API Service ID. More...
 
#define ADC_SID_GET_GROUP_STATUS   ((uint8) 0x09U)
 Adc_GetGroupStatus() API Service ID. More...
 
#define ADC_SID_GET_VERSION_INFO   ((uint8) 0x0AU)
 Adc_GetVersionInfo() API Service ID. More...
 
#define ADC_SID_GET_STREAM_LAST_POINTER   ((uint8) 0x0BU)
 Adc_GetStreamLastPointer() API Service ID. More...
 
#define ADC_SID_SETUP_RESULT_BUFFER   ((uint8) 0x0CU)
 Adc_SetupResultBuffer() API Service ID. More...
 
#define ADC_SID_SET_POWER_STATE   ((uint8) 0x10U)
 Adc_SetPowerState() API Service ID. More...
 
#define ADC_SID_GET_CURRENT_POWER_STATE   ((uint8) 0x11U)
 Adc_GetCurrentPowerState() API Service ID. More...
 
#define ADC_SID_GET_TARGET_POWER_STATE   ((uint8) 0x12U)
 Adc_GetTargetPowerState() API Service ID. More...
 
#define ADC_SID_PREPARE_POWER_STATE   ((uint8) 0x13U)
 Adc_PreparePowerState() API Service ID. More...
 
#define ADC_SID_MAIN_POWER_TRANSITION_MANAGER   ((uint8) 0x14U)
 Adc_Main_PowerTransitionManager() API Service ID. More...
 
#define ADC_SID_IOHWAB_NOTIFICATION   ((uint8) 0x20U)
 IoHwAb_AdcNotification() API Service ID. More...
 
#define ADC_SID_IOHWAB_NOTIFY_READY_FOR_POWER_STATE   ((uint8) 0x70U)
 IoHwAb_Adc_NotifyReadyForPowerState() API Service ID. More...
 
enum  Adc_StatusType { ADC_IDLE, ADC_BUSY, ADC_COMPLETED, ADC_STREAM_COMPLETED }
 Current status of the conversion of the requested ADC Channel group. More...
 
enum  Adc_TriggerSourceType { ADC_TRIGG_SRC_SW, ADC_TRIGG_SRC_HW }
 Type for configuring the trigger source for an ADC Channel group. More...
 
enum  Adc_GroupConvModeType { ADC_CONV_MODE_ONESHOT, ADC_CONV_MODE_CONTINUOUS }
 Type for configuring the conversion mode of an ADC Channel group. More...
 
enum  Adc_StreamBufferModeType { ADC_STREAM_BUFFER_LINEAR, ADC_STREAM_BUFFER_CIRCULAR }
 Type for configuring the streaming access mode buffer type. More...
 
enum  Adc_GroupAccessModeType { ADC_ACCESS_MODE_SINGLE, ADC_ACCESS_MODE_STREAMING }
 Type for configuring the access mode to group conversion results. More...
 
enum  Adc_HwTriggerSignalType { ADC_HW_TRIG_RISING_EDGE, ADC_HW_TRIG_FALLING_EDGE, ADC_HW_TRIG_BOTH_EDGES }
 Type for configuring on which edge of the hardware trigger signal the driver should react, i.e. start the conversion. More...
 
enum  Adc_PriorityImplementationType { ADC_PRIORITY_NONE, ADC_PRIORITY_HW, ADC_PRIORITY_HW_SW }
 Type for configuring the prioritization mechanism. More...
 
enum  Adc_GroupReplacementType { ADC_GROUP_REPL_ABORT_RESTART, ADC_GROUP_REPL_SUSPEND_RESUME }
 Replacement mechanism, which is used on ADC group level, if a group conversion is interrupted by a group which has a higher priority. More...
 
enum  Adc_ChannelRangeSelectType {
  ADC_RANGE_UNDER_LOW, ADC_RANGE_BETWEEN, ADC_RANGE_OVER_HIGH, ADC_RANGE_ALWAYS,
  ADC_RANGE_NOT_UNDER_LOW, ADC_RANGE_NOT_BETWEEN, ADC_RANGE_NOT_OVER_HIGH
}
 In case of active limit checking: defines which conversion values are taken into account related to the boardes defined with AdcChannelLowLimit and AdcChannelHighLimit. More...
 
enum  Adc_ResultAlignmentType { ADC_ALIGN_LEFT, ADC_ALIGN_RIGHT }
 Type for alignment of ADC raw results in ADC result buffer (left/right alignment). More...
 
enum  Adc_PowerStateType { ADC_FULL_POWER, ADC_ZERO_POWER }
 Power state currently active or set as target power state. More...
 
enum  Adc_PowerStateRequestResultType {
  ADC_SERVICE_ACCEPTED, ADC_NOT_INIT, ADC_SEQUENCE_ERROR, ADC_HW_FAILURE,
  ADC_POWER_STATE_NOT_SUPP, ADC_TRANS_NOT_POSSIBLE
}
 Result of the requests related to power state transitions. More...
 
enum  Adc_AveragingMode {
  ADC_AVERAGING_MODE_NONE, ADC_AVERAGING_MODE_2_SAMPLES, ADC_AVERAGING_MODE_4_SAMPLES, ADC_AVERAGING_MODE_8_SAMPLES,
  ADC_AVERAGING_MODE_16_SAMPLES
}
 Enum to number of samplings to average. ADC allows user to program the number of samplings to average. More...
 
 AUTOMATIC
 
ADC_PBCFG CfgPtr
 
const Adc_ValueGroupTypeDataBufferPtr
 
Adc_ValueGroupType ** PtrToSamplePtr
 
ADC_APPL_DATA versioninfo
 
Adc_RefSelType RefSelect
 
 FUNC (void, ADC_CODE_FAST) Adc_IntISR_Fun(Adc_ChannelType AdcChannel)
 ADC ISR. More...
 

Macro Definition Documentation

◆ ADC_SW_MAJOR_VERSION

#define ADC_SW_MAJOR_VERSION   (9U)

Driver Implementation Major Version.

◆ ADC_SW_MINOR_VERSION

#define ADC_SW_MINOR_VERSION   (2U)

Driver Implementation Minor Version.

◆ ADC_SW_PATCH_VERSION

#define ADC_SW_PATCH_VERSION   (0U)

Driver Implementation Patch Version.

◆ ADC_AR_RELEASE_MAJOR_VERSION

#define ADC_AR_RELEASE_MAJOR_VERSION   (4U)

AUTOSAR Major version specification implemented by ADC Driver.

◆ ADC_AR_RELEASE_MINOR_VERSION

#define ADC_AR_RELEASE_MINOR_VERSION   (3U)

AUTOSAR Minor version specification implemented by ADC Driver.

◆ ADC_AR_RELEASE_REVISION_VERSION

#define ADC_AR_RELEASE_REVISION_VERSION   (1U)

AUTOSAR Patch version specification implemented by ADC Driver.

◆ ADC_VENDOR_ID

#define ADC_VENDOR_ID   ((uint16) 44U)

Texas Instruments Vendor ID.

◆ ADC_MODULE_ID

#define ADC_MODULE_ID   ((uint16) 123U)

ADC Driver Module ID.

◆ ADC_INSTANCE_ID

#define ADC_INSTANCE_ID   ((uint8) 0U)

ADC Driver Instance ID.

◆ ADC_DEF_CHANNEL_RESOLUTION

#define ADC_DEF_CHANNEL_RESOLUTION   ((Adc_ResolutionType) 12U)

The default channel resolution supported by the current ADC hardware. No other value is supported by the hardware.

◆ ADC_NUM_CHANNEL

#define ADC_NUM_CHANNEL   (10U)

Number of MCAL channels - in terms of ADC HW, this represents the number of hardware steps. Note: In terms of ADC IP number of steps is 16. Due to AUTOSAR specification, the channel ID's should be unique i.e each channel Id and actual HW channel should have one to one mapping. So ADC_NUM_CHANNEL is fixed to 9 as number of actual HW channels available is also 9.

◆ ADC_MIN_CHANNEL_ID

#define ADC_MIN_CHANNEL_ID   (0U)

Minimum value of channel ID.

◆ ADC_MAX_CHANNEL_ID

#define ADC_MAX_CHANNEL_ID   (ADC_NUM_CHANNEL - 1U)

Maximum value of channel ID.

◆ ADC_NUM_HW_CHANNEL

#define ADC_NUM_HW_CHANNEL   (10U)

Number of actual HW channels - in terms of ADC HW, this represents the actual channel input to the ADC module. Note: This is a fixed value as per the ADC module and can't be changed.

◆ ADC_MIN_HW_CHANNEL_ID

#define ADC_MIN_HW_CHANNEL_ID   (0U)

Minimum value of HW channel ID.

◆ ADC_MAX_HW_CHANNEL_ID

#define ADC_MAX_HW_CHANNEL_ID   (ADC_NUM_HW_CHANNEL - 1U)

Maximum value of HW channel ID.

◆ ADC_MIN_OPEN_DELAY

#define ADC_MIN_OPEN_DELAY   (0x00U)

Minimum value of open delay.

◆ ADC_MAX_OPEN_DELAY

#define ADC_MAX_OPEN_DELAY   (0x3FFFFU)

Maximum value of open delay.

◆ ADC_MIN_SAMPLE_DELAY

#define ADC_MIN_SAMPLE_DELAY   (0x00U)

Minimum value of sample delay.

◆ ADC_MAX_SAMPLE_DELAY

#define ADC_MAX_SAMPLE_DELAY   (0xFFU)

Maximum value of sample delay.

◆ ADC_MIN_RANGE

#define ADC_MIN_RANGE   (0x00U)

Minimum value of range.

◆ ADC_MAX_RANGE

#define ADC_MAX_RANGE   (0xFFFU)

Maximum value of range.

◆ ADC_E_UNINIT

#define ADC_E_UNINIT   ((uint8) 0x0AU)

API service used without module initiali-zation.

◆ ADC_E_BUSY

#define ADC_E_BUSY   ((uint8) 0x0BU)

API service called during ongoing process.

◆ ADC_E_IDLE

#define ADC_E_IDLE   ((uint8) 0x0CU)

API service called while no conversion is ongoing.

◆ ADC_E_ALREADY_INITIALIZED

#define ADC_E_ALREADY_INITIALIZED   ((uint8) 0x0DU)

API Adc_Init service called while the ADC driver has already been initialized.

◆ ADC_E_PARAM_CONFIG

#define ADC_E_PARAM_CONFIG   ((uint8) 0x0EU)

API service called with incorrect configuration parameter.

◆ ADC_E_PARAM_POINTER

#define ADC_E_PARAM_POINTER   ((uint8) 0x14U)

API servcie called with invalid data buffer pointer.

◆ ADC_E_PARAM_GROUP

#define ADC_E_PARAM_GROUP   ((uint8) 0x15U)

API servcie called with invalid group ID.

◆ ADC_E_WRONG_CONV_MODE

#define ADC_E_WRONG_CONV_MODE   ((uint8) 0x16U)

API servcie called on a group with conversion mode configured as continuous.

◆ ADC_E_WRONG_TRIGG_SRC

#define ADC_E_WRONG_TRIGG_SRC   ((uint8) 0x17U)

API servcie called for group with wrong trigger source.

◆ ADC_E_NOTIF_CAPABILITY

#define ADC_E_NOTIF_CAPABILITY   ((uint8) 0x18U)

Enable/disable notification function for a group whose configuration set has no notification available.

◆ ADC_E_BUFFER_UNINIT

#define ADC_E_BUFFER_UNINIT   ((uint8) 0x19U)

Conversion started and result buffer pointer is not initialized.

◆ ADC_E_NOT_DISENGAGED

#define ADC_E_NOT_DISENGAGED   ((uint8) 0x1AU)

One or more ADC group/channel not in IDLE state.

◆ ADC_E_POWER_STATE_NOT_SUPPORTED

#define ADC_E_POWER_STATE_NOT_SUPPORTED   ((uint8) 0x1BU)

Unsupported power state request.

◆ ADC_E_TRANSITION_NOT_POSSIBLE

#define ADC_E_TRANSITION_NOT_POSSIBLE   ((uint8) 0x1CU)

Requested power state can not be reached directly.

◆ ADC_E_PERIPHERAL_NOT_PREPARED

#define ADC_E_PERIPHERAL_NOT_PREPARED   ((uint8) 0x1DU)

ADC not prepared for target power state.

◆ ADC_SID_INIT

#define ADC_SID_INIT   ((uint8) 0x00U)

Adc_Init() API Service ID.

◆ ADC_SID_DEINIT

#define ADC_SID_DEINIT   ((uint8) 0x01U)

Adc_DeInit() API Service ID.

◆ ADC_SID_START_GROUP_CONVERSION

#define ADC_SID_START_GROUP_CONVERSION   ((uint8) 0x02U)

Adc_StartGroupConversion() API Service ID.

◆ ADC_SID_STOP_GROUP_CONVERSION

#define ADC_SID_STOP_GROUP_CONVERSION   ((uint8) 0x03U)

Adc_StopGroupConversion() API Service ID.

◆ ADC_SID_READ_GROUP

#define ADC_SID_READ_GROUP   ((uint8) 0x04U)

Adc_ReadGroup() API Service ID.

◆ ADC_SID_ENABLE_HARDWARE_TRIGGER

#define ADC_SID_ENABLE_HARDWARE_TRIGGER   ((uint8) 0x05U)

Adc_EnableHardwareTrigger() API Service ID.

◆ ADC_SID_DISABLE_HARDWARE_TRIGGER

#define ADC_SID_DISABLE_HARDWARE_TRIGGER   ((uint8) 0x06U)

Adc_DisableHardwareTrigger() API Service ID.

◆ ADC_SID_ENABLE_GROUP_NOTIFICATION

#define ADC_SID_ENABLE_GROUP_NOTIFICATION   ((uint8) 0x07U)

Adc_EnableGroupNotification() API Service ID.

◆ ADC_SID_DISABLE_GROUP_NOTIFICATION

#define ADC_SID_DISABLE_GROUP_NOTIFICATION   ((uint8) 0x08U)

Adc_DisableGroupNotification() API Service ID.

◆ ADC_SID_GET_GROUP_STATUS

#define ADC_SID_GET_GROUP_STATUS   ((uint8) 0x09U)

Adc_GetGroupStatus() API Service ID.

◆ ADC_SID_GET_VERSION_INFO

#define ADC_SID_GET_VERSION_INFO   ((uint8) 0x0AU)

Adc_GetVersionInfo() API Service ID.

◆ ADC_SID_GET_STREAM_LAST_POINTER

#define ADC_SID_GET_STREAM_LAST_POINTER   ((uint8) 0x0BU)

Adc_GetStreamLastPointer() API Service ID.

◆ ADC_SID_SETUP_RESULT_BUFFER

#define ADC_SID_SETUP_RESULT_BUFFER   ((uint8) 0x0CU)

Adc_SetupResultBuffer() API Service ID.

◆ ADC_SID_SET_POWER_STATE

#define ADC_SID_SET_POWER_STATE   ((uint8) 0x10U)

Adc_SetPowerState() API Service ID.

◆ ADC_SID_GET_CURRENT_POWER_STATE

#define ADC_SID_GET_CURRENT_POWER_STATE   ((uint8) 0x11U)

Adc_GetCurrentPowerState() API Service ID.

◆ ADC_SID_GET_TARGET_POWER_STATE

#define ADC_SID_GET_TARGET_POWER_STATE   ((uint8) 0x12U)

Adc_GetTargetPowerState() API Service ID.

◆ ADC_SID_PREPARE_POWER_STATE

#define ADC_SID_PREPARE_POWER_STATE   ((uint8) 0x13U)

Adc_PreparePowerState() API Service ID.

◆ ADC_SID_MAIN_POWER_TRANSITION_MANAGER

#define ADC_SID_MAIN_POWER_TRANSITION_MANAGER   ((uint8) 0x14U)

Adc_Main_PowerTransitionManager() API Service ID.

◆ ADC_SID_IOHWAB_NOTIFICATION

#define ADC_SID_IOHWAB_NOTIFICATION   ((uint8) 0x20U)

IoHwAb_AdcNotification() API Service ID.

◆ ADC_SID_IOHWAB_NOTIFY_READY_FOR_POWER_STATE

#define ADC_SID_IOHWAB_NOTIFY_READY_FOR_POWER_STATE   ((uint8) 0x70U)

IoHwAb_Adc_NotifyReadyForPowerState() API Service ID.

Typedef Documentation

◆ Adc_ChannelType

typedef uint8 Adc_ChannelType

Numeric ID of an ADC channel.

◆ Adc_GroupType

typedef uint8 Adc_GroupType

Numeric ID of an ADC channel group.

◆ Adc_ValueGroupType

typedef uint32 Adc_ValueGroupType

Type for reading the converted values of a channel group (raw, without further scaling, right aligned).

Note: Even though the resolution for this ADC HW is 10-bit, we set this to 32-bit integer as the register read access is 32-bit.

◆ Adc_PrescaleType

typedef uint32 Adc_PrescaleType

Type of clock prescaler factor.

◆ Adc_ConversionTimeType

typedef uint16 Adc_ConversionTimeType

Type of conversion time, i.e. the time during which the sampled analogue value is converted into digital representation.

◆ Adc_SamplingTimeType

typedef uint16 Adc_SamplingTimeType

Type of sampling time, i.e. the time during which the value is sampled (in clockcycles).

◆ Adc_ResolutionType

typedef uint8 Adc_ResolutionType

Type of channel resolution in number of bits.

◆ Adc_GroupPriorityType

typedef uint8 Adc_GroupPriorityType

Priority level of the channel. Lowest priority is 0.

◆ Adc_GroupDefType

typedef uint32 Adc_GroupDefType

Type of assignment of channels to a channel group.

◆ Adc_StreamNumSampleType

typedef uint16 Adc_StreamNumSampleType

Type for configuring the number of group conversions in streaming access mode (in single access mode, parameter is 1).

◆ Adc_HwTriggerTimerType

typedef uint8 Adc_HwTriggerTimerType

Type for the value of the ADC module embedded timer.

◆ Adc_HWUnitType

typedef uint8 Adc_HWUnitType

Specifies the identification (ID) for a ADC Hardware microcontroller peripheral (unit)

◆ Adc_RefSelType

typedef uint8 Adc_RefSelType

Specifies the Reference select for functional internal diagnostic debug mode.

Enumeration Type Documentation

◆ Adc_StatusType

Current status of the conversion of the requested ADC Channel group.

Enumerator
ADC_IDLE 

The conversion of the specified group has not been started. No result is available

ADC_BUSY 

The conversion of the specified group has been started and is still going on. So far no result is available

ADC_COMPLETED 

A conversion round (which is not the final one) of the specified group has been finished. A result is available for all channels of the group

ADC_STREAM_COMPLETED 

The result buffer is completely filled. For each channel of the selected group the number of samples to be acquired is available

◆ Adc_TriggerSourceType

Type for configuring the trigger source for an ADC Channel group.

Enumerator
ADC_TRIGG_SRC_SW 

Group is triggered by a software API call

ADC_TRIGG_SRC_HW 

Group is triggered by a hardware event Note: This feature is not supported in this driver

◆ Adc_GroupConvModeType

Type for configuring the conversion mode of an ADC Channel group.

Enumerator
ADC_CONV_MODE_ONESHOT 

Exactly one conversion of each channel in an ADC channel group is performed after the configured trigger event

ADC_CONV_MODE_CONTINUOUS 

Repeated conversions of each ADC channel in an ADC channel group are performed

◆ Adc_StreamBufferModeType

Type for configuring the streaming access mode buffer type.

Enumerator
ADC_STREAM_BUFFER_LINEAR 

The ADC Driver stops the conversion as soon as the stream buffer is full (number of samples reached)

ADC_STREAM_BUFFER_CIRCULAR 

The ADC Driver continues the conversion even if the stream buffer is full (number of samples reached) by wrapping around the stream buffer itself

◆ Adc_GroupAccessModeType

Type for configuring the access mode to group conversion results.

Enumerator
ADC_ACCESS_MODE_SINGLE 

Single value access mode

ADC_ACCESS_MODE_STREAMING 

Streaming access mode

◆ Adc_HwTriggerSignalType

Type for configuring on which edge of the hardware trigger signal the driver should react, i.e. start the conversion.

Note: This feature is not supported in this driver

Enumerator
ADC_HW_TRIG_RISING_EDGE 

React on the rising edge of the hardware trigger signal

ADC_HW_TRIG_FALLING_EDGE 

React on the falling edge of the hardware trigger signal

ADC_HW_TRIG_BOTH_EDGES 

React on both edges of the hardware trigger signal

◆ Adc_PriorityImplementationType

Type for configuring the prioritization mechanism.

Enumerator
ADC_PRIORITY_NONE 

Priority mechanism is not available

ADC_PRIORITY_HW 

Hardware priority mechanism is available only

ADC_PRIORITY_HW_SW 

Hardware and software priority mechanism is available

◆ Adc_GroupReplacementType

Replacement mechanism, which is used on ADC group level, if a group conversion is interrupted by a group which has a higher priority.

Enumerator
ADC_GROUP_REPL_ABORT_RESTART 

Abort/Restart mechanism is used on group level, if a group is interrupted by a higher priority group

ADC_GROUP_REPL_SUSPEND_RESUME 

Suspend/Resume mechanism is used on group level, if a group is interrupted by a higher priority group. Note: The implementation is same as abort/restart i.e. when a group is started again, previous intermediate results are discarded and the driver always starts from first channel of the group

◆ Adc_ChannelRangeSelectType

In case of active limit checking: defines which conversion values are taken into account related to the boardes defined with AdcChannelLowLimit and AdcChannelHighLimit.

Note: This feature is not supported yet.

Enumerator
ADC_RANGE_UNDER_LOW 

Range below low limit - low limit value included

ADC_RANGE_BETWEEN 

Range between low limit and high limit - high limit value included

ADC_RANGE_OVER_HIGH 

Range above high limit

ADC_RANGE_ALWAYS 

Complete range - independent from channel limit settings

ADC_RANGE_NOT_UNDER_LOW 

Range above low limit

ADC_RANGE_NOT_BETWEEN 

Range above high limit or below low limit - low limit value included

ADC_RANGE_NOT_OVER_HIGH 

Range below high limit - high limit value included

◆ Adc_ResultAlignmentType

Type for alignment of ADC raw results in ADC result buffer (left/right alignment).

Enumerator
ADC_ALIGN_LEFT 

Left alignment. Note: This feature is not supported in the ADC hardware

ADC_ALIGN_RIGHT 

Right alignment

◆ Adc_PowerStateType

Power state currently active or set as target power state.

Enumerator
ADC_FULL_POWER 

Full Power (0)

ADC_ZERO_POWER 

Power modes with decreasing power consumptions

◆ Adc_PowerStateRequestResultType

Result of the requests related to power state transitions.

Enumerator
ADC_SERVICE_ACCEPTED 

Power state change executed

ADC_NOT_INIT 

ADC Module not initialized

ADC_SEQUENCE_ERROR 

Wrong API call sequence

ADC_HW_FAILURE 

The HW module has a failure which prevents it to enter the required power state

ADC_POWER_STATE_NOT_SUPP 

ADC Module does not support the requested power state

ADC_TRANS_NOT_POSSIBLE 

ADC Module cannot transition directly from the current power state to the requested power state or the HW peripheral is still busy

◆ Adc_AveragingMode

Enum to number of samplings to average. ADC allows user to program the number of samplings to average.

Enumerator
ADC_AVERAGING_MODE_NONE 

Disable averaging

ADC_AVERAGING_MODE_2_SAMPLES 

Set number of samplings to average to 2

ADC_AVERAGING_MODE_4_SAMPLES 

Set number of samplings to average to 4

ADC_AVERAGING_MODE_8_SAMPLES 

Set number of samplings to average to 8

ADC_AVERAGING_MODE_16_SAMPLES 

Set number of samplings to average to 16

Function Documentation

◆ FUNC() [1/5]

FUNC ( void  ,
ADC_CODE_FAST   
)

ADC ISR.

◆ P2FUNC()

typedef P2FUNC ( void  ,
ADC_APPL_CODE  ,
Adc_GroupEndNotifyType   
)

Typedef for group end notification function pointer.

◆ FUNC() [2/5]

FUNC ( void  ,
ADC_CODE   
)

Service for ADC initialization.

This service returns the version information of this module.

Disables the notification mechanism for the requested ADC Channel group.

Enables the notification mechanism for the requested ADC Channel group.

Stops the conversion of the requested ADC Channel group.

Starts the conversion of all channels of the requested ADC Channel group.

This service sets all ADC HW Units to a state comparable to their power on reset state.

*  Service name        : Adc_Init
*  Syntax              : void Adc_Init( const Adc_ConfigType* CfgPtr )
*  Mode                : Supervisor Mode (Privileged Mode)
*  Service ID[hex]     : 0x00
*  Sync/Async          : Synchronous
*  Reentrancy          : Non Reentrant
*  Parameters (in)     : Pointer to configuration set in Variant PB
*                        (Variant PC requires a NULL_PTR).
*  Parameters (inout)  : None
*  Parameters (out)    : None
*  Return value        : None
*  Description         : Initializes the ADC hardware units and driver
*  
*  Service name        : Adc_DeInit
*  Syntax              : void Adc_DeInit(void)
*  Mode                : Supervisor Mode (Privileged Mode)
*  Service ID[hex]     : 0x01
*  Sync/Async          : Synchronous
*  Reentrancy          : Non Reentrant
*  Parameters (in)     : None
*  Parameters (inout)  : None
*  Parameters (out)    : None
*  Return value        : None
*  Description         : Returns all ADC HW Units to a state comparable to
*                        their power on reset state
*  
*  Service name        : Adc_StartGroupConversion
*  Syntax              : void Adc_StartGroupConversion( Adc_GroupType Group )
*  Mode                : Supervisor Mode (Privileged Mode)
*  Service ID[hex]     : 0x02
*  Sync/Async          : Asynchronous
*  Reentrancy          : Reentrant
*  Parameters (in)     : Group - Numeric ID of requested ADC Channel group.
*  Parameters (inout)  : None
*  Parameters (out)    : None
*  Return value        : None
*  Description         : Starts the conversion of all channels of the
*                        requested ADC Channel group.
*  
*  Service name        : Adc_StopGroupConversion
*  Syntax              : void Adc_StopGroupConversion( Adc_GroupType Group )
*  Mode                : Supervisor Mode (Privileged Mode)
*  Service ID[hex]     : 0x03
*  Sync/Async          : Synchronous
*  Reentrancy          : Reentrant
*  Parameters (in)     : Group - Numeric ID of requested ADC Channel group.
*  Parameters (inout)  : None
*  Parameters (out)    : None
*  Return value        : None
*  Description         : Stops the conversion of the requested ADC Channel
*                        group.
*  
*  Service name        : Adc_EnableGroupNotification
*  Syntax              : void Adc_EnableGroupNotification( Adc_GroupType Group )
*  Mode                : User Mode (Non-Privileged Mode)
*  Service ID[hex]     : 0x07
*  Sync/Async          : Synchronous
*  Reentrancy          : Reentrant
*  Parameters (in)     : Group - Numeric ID of requested ADC channel group.
*  Parameters (inout)  : None
*  Parameters (out)    : None
*  Return value        : None
*  Description         : Enables the notification mechanism for the requested
*                        ADC Channel group.
*  
*  Service name        : Adc_DisableGroupNotification
*  Syntax              : void Adc_DisableGroupNotification( Adc_GroupType Group )
*  Mode                : User Mode (Non-Privileged Mode)
*  Service ID[hex]     : 0x08
*  Sync/Async          : Synchronous
*  Reentrancy          : Reentrant
*  Parameters (in)     : Group - Numeric ID of requested ADC channel group.
*  Parameters (inout)  : None
*  Parameters (out)    : None
*  Return value        : None
*  Description         : Disables the notification mechanism for the requested
*                        ADC Channel group.
*  
*  Service name        : Adc_GetVersionInfo
*  Syntax              : void Adc_GetVersionInfo( Std_VersionInfoType* versioninfo )
*  Mode                : User Mode (Non-Privileged Mode)
*  Service ID[hex]     : 0x0A
*  Sync/Async          : Synchronous
*  Reentrancy          : Reentrant
*  Parameters (in)     : None
*  Parameters (inout)  : None
*  Parameters (out)    : versioninfo - Pointer to where to store the version
*                        information of this module
*  Return value        : None
*  Description         : Returns the version information of this module
*  

◆ FUNC() [3/5]

FUNC ( Std_ReturnType  ,
ADC_CODE   
)

This service initializes ADC driver with the group specific result buffer start address where the conversion results will be stored.

This function disables the Functional Internal Diagnostic Debug mode.

This function enables the Functional Internal Diagnostic Debug mode and selects a known voltage source(REFP or VMID) that connects to the AFE.

This function reads the important registers of the hardware unit and returns the value in the structure.

Reads the group conversion result of the last completed conversion round of the requested group and stores the channel values starting at the DataBufferPtr address.

*  Service name        : Adc_SetupResultBuffer
*  Syntax              : Std_ReturnType Adc_SetupResultBuffer(
*                                          Adc_GroupType Group,
*                                          Adc_ValueGroupType* DataBufferPtr)
*  Mode                : User Mode (Non-Privileged Mode)
*  Service ID[hex]     : 0x0C
*  Sync/Async          : Synchronous
*  Reentrancy          : Reentrant
*  Parameters (in)     : Group - Numeric ID of requested ADC channel group.
*                        DataBufferPtr - pointer to result data buffer
*  Parameters (inout)  : None
*  Parameters (out)    : None
*  Return value        : Std_ReturnType
*                        E_OK: result buffer pointer initialized correctly
*                        E_NOT_OK: operation failed or development error occured
*  Description         : Initializes ADC driver with the group specific result
*                        buffer start address where the conversion results
*                        will be stored. The application has to ensure that
*                        the application buffer, where DataBufferPtr points
*                        to, can hold all the conversion results of the
*                        specified group. The initialization with
*                        Adc_SetupResultBuffer is required after reset,
*                        before a group conversion can be started.
*  
*  Service name        : Adc_ReadGroup
*  Syntax              : Std_ReturnType Adc_ReadGroup(
*                              Adc_GroupType Group,
*                              Adc_ValueGroupType* DataBufferPtr )
*  Mode                : User Mode (Non-Privileged Mode)
*  Service ID[hex]     : 0x04
*  Sync/Async          : Synchronous
*  Reentrancy          : Reentrant
*  Parameters (in)     : Group - Numeric ID of requested ADC channel group.
*                        DataBufferPtr - ADC results of all channels of the
*                        selected group are stored in the data buffer
*                        addressed with the pointer
*  Parameters (inout)  : None
*  Parameters (out)    : None
*  Return value        : Std_ReturnType
*                        E_OK: results are available and written to the data buffer
*                        E_NOT_OK: no results are available or development error occured
*  Description         : Reads the group conversion result of the last
*                        completed conversion round of the requested group
*                        and stores the channel values starting at the
*                        DataBufferPtr address. The group channel values are
*                        stored in ascending channel number order (in contrast
*                        to the storage layout of the result buffer if
*                        streaming access is configured).
*  

This API should be called after Adc_Init is called. Otherwise this API will return E_NOT_OK.

This API could be used to readback the register contents after Adc_Init and then the readback value could be compared during ADC execution to check the correctness of the HW unit. Since this API is used for this purpose, the register returned are the ones which doesn't change after init based on conv or channel config.

*  Service name        : Adc_RegisterReadback
*  Mode                : Supervisor Mode (Privileged Mode)
*  Sync/Async          : Synchronous
*  Reentrancy          : Reentrant
*  Parameters (in)     : HWUnit - ADC Hardware microcontroller peripheral
*                        unit ID. If this is invalid, then the API will
*                        return E_NOT_OK.
*  Parameters (inout)  : RegRbPtr - Pointer to where to store the readback
*                        values. If this pointer is NULL_PTR, then the API
*                        will return E_NOT_OK.
*  Return value        : Std_ReturnType
*                        E_OK: Register read back has been done
*                        E_NOT_OK: Register read back failed
*  
*  Service name        : Adc_EnableInternalDiagnostic
*  Mode                : Supervisor Mode (Privileged Mode)
*  Sync/Async          : Synchronous
*  Reentrancy          : Reentrant
*  Parameters (in)     : Group - Numeric ID of requested ADC channel group.
*                        If this is invalid, then the API will return E_NOT_OK.
*                        RefSelect - Reference select for functional internal
*                        diagnostic debug mode.
*                        0 = VMID
*                        1 = REFP
*  Parameters (inout)  : None
*  Return value        : Std_ReturnType
*                        E_OK: Functional Internal Diagnostic Debug Mode
*                        has been enabled Successfully.
*                        E_NOT_OK: Functional Internal Diagnostic Debug Mode
*                        enable failed.
*  
*  Service name        : Adc_DisableInternalDiagnostic
*  Mode                : Supervisor Mode (Privileged Mode)
*  Sync/Async          : Synchronous
*  Reentrancy          : Reentrant
*  Parameters (in)     : Group - Numeric ID of requested ADC channel group.
*                        If this is invalid, then the API will return E_NOT_OK.
*  Parameters (inout)  : None
*  Return value        : Std_ReturnType
*                        E_OK: Functional Internal Diagnostic Debug Mode
*                        has been disabled Successfully.
*                        E_NOT_OK: Functional Internal Diagnostic Debug Mode
*                        disable failed.
*  

◆ FUNC() [4/5]

FUNC ( Adc_StatusType  ,
ADC_CODE   
)

Returns the conversion status of the requested ADC Channel group.

*  Service name        : Adc_GetGroupStatus
*  Syntax              : Adc_StatusType Adc_GetGroupStatus( Adc_GroupType Group )
*  Mode                : User Mode (Non-Privileged Mode)
*  Service ID[hex]     : 0x09
*  Sync/Async          : Synchronous
*  Reentrancy          : Reentrant
*  Parameters (in)     : Group - Numeric ID of requested ADC channel group.
*  Parameters (inout)  : None
*  Parameters (out)    : None
*  Return value        : Adc_StatusType - Conversion status for the requested
*                        group
*  Description         : Returns the conversion status of the requested ADC
*                        Channel group.
*  

◆ FUNC() [5/5]

FUNC ( Adc_StreamNumSampleType  ,
ADC_CODE   
)

Returns the number of valid samples per channel, stored in the result buffer.

*  Service name        : Adc_GetStreamLastPointer
*  Syntax              : Adc_StreamNumSampleType Adc_GetStreamLastPointer(
*                              Adc_GroupType Group,
*                              Adc_ValueGroupType** PtrToSamplePtr )
*  Mode                : User Mode (Non-Privileged Mode)
*  Service ID[hex]     : 0x0B
*  Sync/Async          : Synchronous
*  Reentrancy          : Reentrant
*  Parameters (in)     : Group - Numeric ID of requested ADC channel group.
*  Parameters (inout)  : None
*  Parameters (out)    : PtrToSamplePtr - Pointer to result buffer pointer.
*  Return value        : Adc_StreamNumSampleType - Number of valid samples
*                        per channel
*  Description         : Returns the number of valid samples per channel,
*                        stored in the result buffer. Reads a pointer,
*                        pointing to a position in the group result buffer.
*                        With the pointer position, the results of all group
*                        channels of the last completed conversion round can
*                        be accessed. With the pointer and the return value,
*                        all valid group conversion results can be accessed
*                        (the user has to take the layout of the result buffer
*                        into account).
*  

◆ P2VAR()

P2VAR ( Adc_RegisterReadbackType  ,
AUTOMATIC  ,
ADC_APPL_DATA   
)

Variable Documentation

◆ AUTOMATIC

AUTOMATIC

◆ CfgPtr

ADC_PBCFG CfgPtr

◆ DataBufferPtr

Adc_ValueGroupType * DataBufferPtr

◆ PtrToSamplePtr

Adc_ValueGroupType** PtrToSamplePtr

◆ versioninfo

ADC_APPL_DATA versioninfo

◆ RefSelect

Adc_RefSelType RefSelect