MCUSW
Spi.h File Reference

Introduction

This file contains interface header for SPI MCAL driver.

Go to the source code of this file.

SPI Buffer Definition

#define SPI_IB   (0U)
 Buffer definitions IB - internal buffers. More...
 
#define SPI_EB   (1U)
 Buffer definitions EB - external buffers. Only this is supported. More...
 
#define SPI_IB_EB   (2U)
 Buffer definitions IB/EB - internal/external buffers. More...
 
typedef uint8 Spi_DataBufferType
 Type of application data buffer elements. More...
 
typedef uint16 Spi_NumberOfDataType
 Type for defining the number of data elements of the type Spi_DataBufferType to send and / or receive by Channel. More...
 
typedef uint8 Spi_ChannelType
 Specifies the identification (ID) for a Channel. More...
 
typedef uint16 Spi_JobType
 Specifies the identification (ID) for a Job. More...
 
typedef uint8 Spi_SequenceType
 Specifies the identification (ID) for a sequence of jobs. More...
 
typedef uint8 Spi_HWUnitType
 Specifies the identification (ID) for a SPI Hardware micro controller peripheral (unit) More...
 

SPI Config Ids

The Config Ids used for different SPI Configuration builds

#define SPI_CFG_ID_0   (0x01U)
 Config 0 (All configurations ON), Scaleability level 2) More...
 
#define SPI_CFG_ID_1   (0x02U)
 Config 1 (All configurations OFF). SPI_CFG_ID_1 is used only for compile check. More...
 
#define SPI_CFG_ID_2   (0x04U)
 Config 2 (All configurations ON except DET OFF) More...
 
#define SPI_CFG_ID_3   (0x08U)
 Config 3 (Configurator auto generated file) More...
 
#define SPI_CFG_ID_4   (0x10U)
 Config 4 (Config is used only by Unit Test, Scaleability level 0) More...
 
#define SPI_CFG_ID_5   (0x20U)
 Config 5 (Config is used only by Unit Test for DMA
More...
 
#define SPI_CFG_ID_6   (0x40U)
 Config 6 (Config is used only by Unit Test for DMA. More...
 
#define SPI_CFG_ID_7   (0x80U)
 Config 7 (Performance testing only, level 2, asynch, no DMA) More...
 
#define SPI_CFG_ID_8   (0x100U)
 Config 8 (Loopback test on different data sizes, level 1, asynch, no DMA) More...
 
enum  Spi_StatusType { SPI_UNINIT = 0U, SPI_IDLE = 1U, SPI_BUSY = 2U }
 This type defines a range of specific status for SPI Handler/Driver. More...
 
enum  Spi_JobResultType { SPI_JOB_OK = 0U, SPI_JOB_PENDING = 1U, SPI_JOB_FAILED = 2U, SPI_JOB_QUEUED = 3U }
 This type defines a range of specific Jobs status for SPI Handler/Driver. More...
 
enum  Spi_SeqResultType { SPI_SEQ_OK = 0U, SPI_SEQ_PENDING = 1U, SPI_SEQ_FAILED = 2U, SPI_SEQ_CANCELLED = 3U }
 This type defines a range of specific Sequences status for SPI Handler/Driver. More...
 
enum  Spi_HwUnitResultType { SPI_HW_UNIT_OK = 0U, SPI_HW_UNIT_PENDING = 1U, SPI_HW_UNIT_FAILED = 2U }
 This type defines a range of specific HW unit status for SPI Handler/Driver. More...
 
enum  Spi_AsyncModeType { SPI_POLLING_MODE = 0U, SPI_INTERRUPT_MODE = 1U }
 Specifies the asynchronous mechanism mode for SPI busses handled asynchronously in LEVEL 2. More...
 
enum  Spi_TransferType { SPI_MSB = 0U, SPI_LSB = 1U }
 Word transfer order - MSB first or LSB first. More...
 
enum  Spi_LevelType { SPI_LOW = STD_LOW, SPI_HIGH }
 Type for SPI Chip Select Polarity and Clock Idle Level. More...
 
enum  Spi_CsPinType { SPI_CS0 = 0U, SPI_CS1, SPI_CS2, SPI_CS3 }
 SPI Chip Select Pin. More...
 
enum  Spi_ClkMode { SPI_CLK_MODE_0 = 0x00U, SPI_CLK_MODE_1 = 0x01U, SPI_CLK_MODE_2 = 0x02U, SPI_CLK_MODE_3 = 0x03U }
 SPI Clock Mode - sets the clock polarity and phase. Note: These values are a direct register mapping. So don't change value. More...
 
enum  Spi_TxRxMode { SPI_TX_RX_MODE_BOTH = 0x00U, SPI_TX_RX_MODE_TX_ONLY = 0x02U }
 SPI TX/RX Mode. More...
 
enum  Spi_JobPriorityType { SPI_JOB_PRIORITY_0 = 0U, SPI_JOB_PRIORITY_1, SPI_JOB_PRIORITY_2, SPI_JOB_PRIORITY_3 }
 SPI Job Priority. More...
 
enum  Spi_CsModeType { SPI_SINGLE = 0U, SPI_CONTINUOUS = 1U }
 SPI Chip Select Mode. More...
 
enum  Spi_DataDelayType { SPI_DATADELAY_0 = 0U, SPI_DATADELAY_1 = 1U, SPI_DATADELAY_2 = 2U, SPI_DATADELAY_3 = 3U }
 Spi_DataDelayType defines the number of interface clock cycles between CS toggling and first or last edge of MCSPI clock. More...
 
enum  Spi_DataLineReceiveType { DATA_LINE_0_RECEPTION = 0U, DATA_LINE_1_RECEPTION = 1U }
 Spi_DataLineReceiveType defines the lines selected for reception. More...
 
enum  Spi_DataLineTransmitType { DATA_LINE_NO_TRANSMISSION = 0x3U, DATA_LINE_0_TRANSMISSION = 0x2U, DATA_LINE_1_TRANSMISSION = 0x1U, DATA_LINE_BOTH_TRANSMISSION = 0x0U }
 Spi_DataLineTransmitType defines the lines selected for transmission. More...
 
enum  Mcspi_IrqStatusType { SPI_NO_EVENT = 0U, SPI_EVENT_PENDING = 1U, SPI_STATUS_READ_FAIL = 2U }
 Irq status and std return type. More...
 
typedef void(* Spi_CacheWbInv) (uint8 *BufPtr, uint16 LenByte)
 Cache write-back invalidate function. More...
 
typedef void(* Spi_CacheWb) (uint8 *BufPtr, uint16 LenByte)
 Cache write-back function. More...
 
typedef void(* Spi_CacheInv) (uint8 *BufPtr, uint16 LenByte)
 Cache invalidate function. More...
 
 AUTOMATIC
 
SPI_CONFIG_DATA CfgPtr
 
SPI_APPL_DATA versioninfo
 
 FUNC (void, SPI_CODE) Spi_Init(P2CONST(Spi_ConfigType
 Service for SPI initialization. More...
 
 FUNC (Std_ReturnType, SPI_CODE) Spi_DeInit(void)
 Service for SPI de-initialization. More...
 
 FUNC (Spi_StatusType, SPI_CODE) Spi_GetStatus(void)
 Service returns the SPI Handler/Driver software module status. More...
 
 FUNC (Spi_JobResultType, SPI_CODE) Spi_GetJobResult(Spi_JobType Job)
 This service returns the last transmission result of the specified Job. More...
 
 FUNC (Spi_SeqResultType, SPI_CODE) Spi_GetSequenceResult(Spi_SequenceType Sequence)
 This service returns the last transmission result of the specified Sequence. More...
 
 P2CONST (Spi_DataBufferType, AUTOMATIC, SPI_APPL_DATA) DataBufferPtr)
 
 P2VAR (Spi_DataBufferType, AUTOMATIC, SPI_APPL_DATA) DataBufferPointer)
 
 P2VAR (Spi_RegisterReadbackType, AUTOMATIC, SPI_APPL_DATA) RegRbPtr)
 

Data Structures

struct  Spi_ChannelConfigType
 SPI Channel configuration structure. More...
 
struct  Spi_McspiExternalDeviceConfigType
 SPI Job configuration structure specific to McSPI peripheral. More...
 
struct  Spi_ExternalDeviceConfigType
 SPI external device specific configuration structure . More...
 
struct  Spi_JobConfigType
 SPI Job configuration structure. More...
 
struct  Spi_SeqConfigType
 SPI Sequence configuration structure. More...
 
struct  Spi_HwUnitConfigType
 SPI Hardware unit configuration structure. More...
 
struct  Spi_ConfigType
 SPI config structure. More...
 
struct  Spi_ChannelConfigType_PC
 SPI channel config structure parameters Pre-Compile only. More...
 
struct  Spi_JobConfigType_PC
 SPI job config structure parameters Pre-Compile only. More...
 
struct  Spi_SeqConfigType_PC
 SPI sequence config structure parameters Pre-Compile only. More...
 
struct  Spi_RegisterReadbackType
 SPI register readback structure. More...
 

Macros

SPI Driver Module SW Version Info

Defines for SPI Driver version used for compatibility checks

#define SPI_SW_MAJOR_VERSION   (9U)
 Driver Implementation Major Version. More...
 
#define SPI_SW_MINOR_VERSION   (2U)
 Driver Implementation Minor Version. More...
 
#define SPI_SW_PATCH_VERSION   (1U)
 Driver Implementation Patch Version. More...
 
SPI Driver Module AUTOSAR Version Info

Defines for SPI Driver AUTOSAR version used for compatibility checks

#define SPI_AR_RELEASE_MAJOR_VERSION   (4U)
 AUTOSAR Major version specification implemented by SPI Driver. More...
 
#define SPI_AR_RELEASE_MINOR_VERSION   (3U)
 AUTOSAR Minor version specification implemented by SPI Driver. More...
 
#define SPI_AR_RELEASE_REVISION_VERSION   (1U)
 AUTOSAR Patch version specification implemented by SPI Driver. More...
 
SPI Driver ID Info
#define SPI_VENDOR_ID   ((uint16) 44U)
 Texas Instruments Vendor ID. More...
 
#define SPI_MODULE_ID   ((uint16) 83U)
 SPI Driver Module ID. More...
 
#define SPI_INSTANCE_ID   ((uint8) 0U)
 SPI Driver Instance ID. More...
 
SPI Error Codes

Error codes returned by SPI functions

#define SPI_E_PARAM_CHANNEL   ((uint8) 0x0AU)
 API service called with wrong parameter. More...
 
#define SPI_E_PARAM_JOB   ((uint8) 0x0BU)
 API service called with wrong parameter. More...
 
#define SPI_E_PARAM_SEQ   ((uint8) 0x0CU)
 API service called with wrong parameter. More...
 
#define SPI_E_PARAM_LENGTH   ((uint8) 0x0DU)
 API service called with wrong parameter. More...
 
#define SPI_E_PARAM_UNIT   ((uint8) 0x0EU)
 API service called with wrong parameter. More...
 
#define SPI_E_PARAM_POINTER   ((uint8) 0x10U)
 APIs called with a Null Pointer. More...
 
#define SPI_E_UNINIT   ((uint8) 0x1AU)
 API service used without module initiali-zation. More...
 
#define SPI_E_SEQ_PENDING   ((uint8) 0x2AU)
 Services called in a wrong sequence. More...
 
#define SPI_E_SEQ_IN_PROCESS   ((uint8) 0x3AU)
 Synchronous transmission service called at wrong time. More...
 
#define SPI_E_ALREADY_INITIALIZED   ((uint8) 0x4AU)
 API Spi_Init service called while the SPI driver has already been initialized. More...
 
#define SPI_E_SEQUENCE_NOT_OK   ((uint8) 0x5AU)
 Sequence did not complete successfully. More...
 
SPI Service Ids

The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error

#define SPI_SID_INIT   ((uint8) 0x00U)
 Spi_Init() API Service ID. More...
 
#define SPI_SID_DEINIT   ((uint8) 0x01U)
 Spi_DeInit() API Service ID. More...
 
#define SPI_SID_WRITE_IB   ((uint8) 0x02U)
 Spi_WriteIB() API Service ID. More...
 
#define SPI_SID_ASYNC_TRANSMIT   ((uint8) 0x03U)
 Spi_AsyncTransmit() API Service ID. More...
 
#define SPI_SID_READ_IB   ((uint8) 0x04U)
 Spi_ReadIB() API Service ID. More...
 
#define SPI_SID_SETUP_EB   ((uint8) 0x05U)
 Spi_SetupEB() API Service ID. More...
 
#define SPI_SID_GET_STATUS   ((uint8) 0x06U)
 Spi_GetStatus() API Service ID. More...
 
#define SPI_SID_GET_JOB_RESULT   ((uint8) 0x07U)
 Spi_GetJobResult() API Service ID. More...
 
#define SPI_SID_GET_SEQ_RESULT   ((uint8) 0x08U)
 Spi_GetSequenceResult() API Service ID. More...
 
#define SPI_SID_GET_VERSION_INFO   ((uint8) 0x09U)
 Spi_GetVersionInfo() API Service ID. More...
 
#define SPI_SID_SYNC_TRANSMIT   ((uint8) 0x0AU)
 Spi_SyncTransmit() API Service ID. More...
 
#define SPI_SID_GET_HW_UNIT_STATUS   ((uint8) 0x0BU)
 Spi_GetHWUnitStatus() API Service ID. More...
 
#define SPI_SID_CANCEL   ((uint8) 0x0CU)
 Spi_Cancel() API Service ID. More...
 
#define SPI_SID_SET_ASYNC_MODE   ((uint8) 0x0DU)
 Spi_SetAsyncMode() API Service ID. More...
 
#define SPI_SID_MAINFUNCTION_HANDLING   ((uint8) 0x10U)
 Spi_MainFunction_Handling() API Service ID. More...
 
#define SPI_SID_DMA_INIT   ((uint8) 0x20U)
 Spi_GetDmaHandle() API Service ID. More...
 
#define SPI_MCSPI_FCLK   (48000000U)
 MCSPI functional clock input in Hz. This clock is used to generate the serial clock output after the divider. More...