MCUSW
Mcu.h File Reference

Introduction

This file contains interface header for MCU MCAL driver.

Go to the source code of this file.

MCU Reset Modes

Reset mode enum which can be used in Mcu_PerformReset()

#define MCU_PERFORM_RESET_MODE_COLD   ((uint8) 0U)
 Initiate SW COLD RESET sequence. More...
 
#define MCU_PERFORM_RESET_MODE_WARM   ((uint8) 1U)
 Initiate SW WARM RESET sequence. More...
 
#define MCU_E_MODE_FAILURE   0U
 
typedef uint8 Mcu_ClockType
 This type specifies the identification (ID) for a ClockType status used by Mcu_InitClock() More...
 
typedef uint32 Mcu_RawResetType
 This type specifies the identification (ID) for a RAW MCU reset status returned by Mcu_GetResetRawValue() More...
 
typedef uint8 Mcu_RamSectionType
 This type specifies the identification (ID) for a RAM section used in Mcu_InitRamSection() More...
 
typedef uint8 Mcu_ModeType
 This type specifies the identification (ID) for a MCU mode used in Mcu_SetMode() More...
 
const struct Mcu_ConfigType_s McuModuleConfiguration_0
 MCU Configuration struct declaration. More...
 
 AUTOMATIC
 
MCU_PBCFG ConfigPtr
 
MCU_APPL_DATA versioninfo
 
typedef P2CONST (Mcu_ClockConfigType, AUTOMATIC, MCU_PBCFG) Mcu_ClockConfigPtrType
 Pointer to Clock Config structure. More...
 
 FUNC (void, MCU_CODE) Mcu_Init(P2CONST(Mcu_ConfigType
 This service initializes the MCU driver. More...
 
 FUNC (Std_ReturnType, MCU_CODE) Mcu_InitClock(Mcu_ClockType ClockSetting)
 This service initializes the PLL and other MCU specific clock options. More...
 
 FUNC (Mcu_PllStatusType, MCU_CODE) Mcu_GetPllStatus(void)
 This service provides the lock status of the PLL. More...
 
 FUNC (Mcu_ResetType, MCU_CODE) Mcu_GetResetReason(void)
 The service reads the reset type from the hardware, if supported. More...
 
 FUNC (Mcu_RawResetType, MCU_CODE) Mcu_GetResetRawValue(void)
 The service reads the reset type from the hardware register, if supported. More...
 
 FUNC (Mcu_RamStateType, MCU_CODE) Mcu_GetRamState(void)
 This service provides the actual status of the microcontroller Ram. (if supported) More...
 

Data Structures

struct  Mcu_ClockConfigType
 Structure for module clock setting. More...
 
struct  Mcu_ConfigType
 MCU CONFIG ROOT structure. More...
 

Macros

#define ARRAYSIZE(array)
 
MCU Driver Module SW Version Info

Defines for MCU Driver version used for compatibility checks

#define MCU_SW_MAJOR_VERSION   (10U)
 Driver Implementation Major Version. More...
 
#define MCU_SW_MINOR_VERSION   (1U)
 Driver Implementation Minor Version. More...
 
#define MCU_SW_PATCH_VERSION   (1U)
 Driver Implementation Patch Version. More...
 
MCU Driver Module AUTOSAR Version Info

Defines for MCU Driver AUTOSAR version used for compatibility checks

#define MCU_AR_RELEASE_MAJOR_VERSION   (4U)
 AUTOSAR Major version specification implemented by MCU Driver. More...
 
#define MCU_AR_RELEASE_MINOR_VERSION   (3U)
 AUTOSAR Minor version specification implemented by MCU Driver. More...
 
#define MCU_AR_RELEASE_REVISION_VERSION   (1U)
 AUTOSAR Patch version specification implemented by MCU Driver. More...
 
MCU Driver ID Info
#define MCU_VENDOR_ID   ((uint16) 44U)
 Texas Instruments Vendor ID. More...
 
#define MCU_MODULE_ID   ((uint16) 101U)
 MCU Driver Module ID. More...
 
#define MCU_INSTANCE_ID   ((uint8) 0U)
 MCU Driver Instance ID. More...
 
MCU Error Codes

Error codes returned by MCU functions

#define MCU_E_PARAM_CONFIG   (0x0AU)
 ERROR Description: API service called with wrong configuration parameter. More...
 
#define MCU_E_PARAM_CLOCK   (0x0BU)
 ERROR Description: API service used with wrong clock value. More...
 
#define MCU_E_PARAM_MODE   (0x0CU)
 ERROR Description: API service used with wrong mode. More...
 
#define MCU_E_PARAM_RAMSECTION   (0x0DU)
 ERROR Description: API service called with invalid/wrong RAM section. More...
 
#define MCU_E_PLL_NOT_LOCKED   (0x0EU)
 ERROR Description: API service is called while PLL is not locked. More...
 
#define MCU_E_UNINIT   (0x0FU)
 ERROR Description: Mcu Driver API service is called before initialization of MCU Driver. More...
 
#define MCU_E_PARAM_POINTER   (0x10U)
 ERROR Description: API service is called with NULL/Wrong pointer. More...
 
#define MCU_E_INIT_FAILED   (0x11U)
 ERROR Description: Initialization of the MCU Driver Failed. More...
 
MCU Driver State Values

The MCU Driver State Values

#define MCU_STATUS_UNINIT   ((uint8)(0U))
 MCU driver Status uninitialized. More...
 
#define MCU_STATUS_INIT   ((uint8)(1U))
 MCU driver Status Initialized. More...
 
MCU Service Ids

The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error

#define MCU_SID_INIT   (0x00U)
 Mcu_Init() API Service ID. More...
 
#define MCU_SID_INIT_RAM_SECTION   (0x01U)
 Mcu_InitRamSection() API Service ID. More...
 
#define MCU_SID_INIT_CLOCK   (0x02U)
 Mcu_InitClock() API Service ID. More...
 
#define MCU_SID_DISTRIBUTE_PLL_CLOCK   (0x03U)
 Mcu_DistributePllClock() API Service ID. More...
 
#define MCU_SID_GET_PLL_STATUS   (0x04U)
 Mcu_GetPllStatus() API Service ID. More...
 
#define MCU_SID_GET_RESET_REASON   (0x05U)
 Mcu_GetResetReason() API Service ID. More...
 
#define MCU_SID_GET_RESET_RAW_VALUE   (0x06U)
 Mcu_GetResetRawValue() API Service ID. More...
 
#define MCU_SID_PERFORM_RESET   (0x07U)
 Mcu_PerformReset() API Service ID. More...
 
#define MCU_SID_SETMODE   (0x08U)
 Mcu_SetMode() API Service ID. More...
 
#define MCU_SID_GET_VERSION_INFO   (0x09U)
 Mcu_GetVersionInfo() API Service ID. More...
 
#define MCU_SID_GET_RAM_STATE   (0x0AU)
 Mcu_GetRamState() API Service ID. More...