![]() |
MCUSW
|
This file contains interface header for GPT MCAL driver.
Go to the source code of this file.
GPT Service Ids | |
The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error | |
| #define | GPT_SID_GET_VERSION_INFO (0x00U) |
| Gpt_GetVersionInfo() API Service ID. More... | |
| #define | GPT_SID_INIT (0x01U) |
| Gpt_Init() API Service ID. More... | |
| #define | GPT_SID_DEINIT (0x02U) |
| Gpt_DeInit() API Service ID. More... | |
| #define | GPT_SID_GET_TIME_ELAPSED (0x03U) |
| Gpt_GetTimeElapsed() API Service ID. More... | |
| #define | GPT_SID_GET_TIME_REMAINING (0x04U) |
| Gpt_GetTimeRemaining() API Service ID. More... | |
| #define | GPT_SID_START_TIMER (0x05U) |
| Gpt_StartTimer() API Service ID. More... | |
| #define | GPT_SID_STOP_TIMER (0x06U) |
| Gpt_StopTimer() API Service ID. More... | |
| #define | GPT_SID_ENABLE_NOTIFY (0x07U) |
| Gpt_EnableNotification() API Service ID. More... | |
| #define | GPT_SID_DISABLE_NOTIFY (0x08U) |
| Gpt_DisableNotification() API Service ID. More... | |
| #define | GPT_SID_SET_MODE (0x09U) |
| Gpt_SetMode() API Service ID. More... | |
| #define | GPT_SID_DISABLE_WAKEUP (0x0AU) |
| Gpt_DisableWakeup() API Service ID. More... | |
| #define | GPT_SID_ENABLE_WAKEUP (0x0BU) |
| Gpt_EnableWakeup() API Service ID. More... | |
| #define | GPT_SID_CHECK_WAKEUP (0x0CU) |
| Gpt_CheckWakeup() API Service ID. More... | |
| #define | GPT_SID_GET_PREDEFTIMERVALUE (0x0DU) |
| Gpt_GetPredefTimerValue() API Service ID. More... | |
| #define | GPT_SID_GET_GETHWUNITOBJ (0x0EU) |
| GPT Get Hw Unit Obj API Service ID. More... | |
| #define | GPT_SID_REGISTER_READBACK (0x0FU) |
| GPT Critical register read back API Service ID. More... | |
| enum | Gpt_ModeType { GPT_MODE_NORMAL = 0U, GPT_MODE_SLEEP = 1U, GPT_MODE_INVALID = 0xFFU } |
| List of process modes More... | |
| enum | Gpt_PredefTimerType { GPT_PREDEF_TIMER_1US_16BIT = 0U, GPT_PREDEF_TIMER_1US_24BIT = 1U, GPT_PREDEF_TIMER_1US_32BIT = 2U, GPT_PREDEF_TIMER_100US_32BIT = 3U } |
| Type for GPT Predef Timers. More... | |
| enum | Gpt_PrescaleValueType { GPT_PRESCALER_CLK_DIV_BY_2 = 0x0U, GPT_PRESCALER_CLK_DIV_BY_4 = 0x1U, GPT_PRESCALER_CLK_DIV_BY_8 = 0x2U, GPT_PRESCALER_CLK_DIV_BY_16 = 0x3U, GPT_PRESCALER_CLK_DIV_BY_32 = 0x4U, GPT_PRESCALER_CLK_DIV_BY_64 = 0x5U, GPT_PRESCALER_CLK_DIV_BY_128 = 0x6U, GPT_PRESCALER_CLK_DIV_BY_256 = 0x7U, GPT_PRESCALER_NO_PRESCALE = 0xFFU } |
| List of Prescale values for General purpose timer channels The timer counter is prescaled with the value 2^(PTV+1). Example: PTV = 3, counter increases value (if started) after 16 functional clock periods Note: Not applicable to GPT Predef timers. More... | |
| enum | Gpt_ChannelMode { GPT_CH_MODE_CONTINUOUS = 0U, GPT_CH_MODE_ONESHOT } |
| GPT channel mode macros. More... | |
| enum | Gpt_ChannelStateType { GPT_UNINITIALIZED = 0U, GPT_INITIALIZED, GPT_RUNNING, GPT_STOPPED, GPT_EXPIRED } |
| GPT channel state GPT will be in one of this state during its lifetime. More... | |
| typedef uint32 | Gpt_ChannelType |
| Type describing the Gpt channel. More... | |
| typedef uint32 | Gpt_ValueType |
| Type describing the timeout value More... | |
| typedef void(* | Gpt_NotifyType) (void) |
| Notification callback function pointer More... | |
| AUTOMATIC | |
| GPT_APPL_DATA | VersionInfoPtr |
| GPT_CONST | CfgPtr |
| Gpt_ValueType | Value |
| uint32 * | TimeValuePtr |
| FUNC (void, GPT_CODE) Gpt_GetVersionInfo(P2VAR(Std_VersionInfoType | |
| This service returns the version information of this module. More... | |
| FUNC (Gpt_ValueType, GPT_CODE) Gpt_GetTimeElapsed(Gpt_ChannelType Channel) | |
| Gpt_GetTimeElapsed will return the time elapsed for channel which is referenced. The user can configure the channel in two modes, One-shot and Continuous mode. In one shot mode, if the timer is in stopped state, the function will return time value at the moment of stopping. If the timer is expired, the function will return the target time configured for the channel. In Continuous Mode - The elapsed time value will be the value relative to last occurrence. More... | |
| FUNC (Std_ReturnType, GPT_CODE) Gpt_RegisterReadback(Gpt_ChannelType GptChannel | |
| This function reads the important registers of the hardware unit and returns the value in the structure. More... | |
| P2VAR (Gpt_RegisterReadbackType, AUTOMATIC, GPT_APPL_DATA) RegRbPtr) | |
Data Structures | |
| struct | Gpt_ChannelConfigType |
| Configuration per channel. More... | |
| struct | Gpt_ChannelConfigType_PC |
| SPI sequence config structure parameters Pre-Compile only. More... | |
| struct | Gpt_ConfigType |
| global configuration of the driver More... | |
| struct | Gpt_RegisterReadbackType |
| GPT register readback structure. More... | |
Macros | |
GPT Driver Module SW Version Info | |
Defines for GPT Driver version used for compatibility checks | |
| #define | GPT_SW_MAJOR_VERSION (9U) |
| Driver Implementation Major Version. More... | |
| #define | GPT_SW_MINOR_VERSION (2U) |
| Driver Implementation Minor Version. More... | |
| #define | GPT_SW_PATCH_VERSION (1U) |
| Driver Implementation Patch Version. More... | |
GPT Driver Module AUTOSAR Version Info | |
Defines for GPT Driver AUTOSAR version used for compatibility checks | |
| #define | GPT_AR_RELEASE_MAJOR_VERSION (4U) |
| AUTOSAR Major version specification implemented by GPT Driver. More... | |
| #define | GPT_AR_RELEASE_MINOR_VERSION (3U) |
| AUTOSAR Minor version specification implemented by GPT Driver. More... | |
| #define | GPT_AR_RELEASE_REVISION_VERSION (1U) |
| AUTOSAR Patch version specification implemented by GPT Driver. More... | |
GPT Driver ID Info | |
| #define | GPT_VENDOR_ID ((uint16) 44U) |
| Texas Instruments Vendor ID. More... | |
| #define | GPT_MODULE_ID ((uint16) 100U) |
| GPT Driver Module ID. More... | |
| #define | GPT_INSTANCE_ID ((uint8) 0U) |
| GPT Driver Instance ID. More... | |
| #define | GPT_CH_ISR_MODE_CONTINUOUS (0U) |
| GPT continuous mode index. More... | |
| #define | GPT_CH_ISR_MODE_ONESHOT (1U) |
| GPT oneshot mode index. More... | |
| #define | GPT_CH_ISR_MODE_CONT_WAKEUP (2U) |
| GPT continuous wakeup mode index. More... | |
| #define | GPT_CH_ISR_MODE_ONESHOT_WAKEUP (3U) |
| GPT oneshot wakeup mode index. More... | |
GPT Error Codes | |
Error codes returned by GPT functions | |
| #define | GPT_E_UNINIT (0x0AU) |
| API service used without module initialization. More... | |
| #define | GPT_E_BUSY (0x0BU) |
| API service called during ongoing process (Timer is already running) More... | |
| #define | GPT_E_MODE (0x0CU) |
| API service called when driver is in wrong mode. Used primarily when PreDef Timers are used. Since PreDef Timer are not supported in this implementation, this error code is not used. More... | |
| #define | GPT_E_ALREADY_INITIALIZED (0x0DU) |
| API Gpt_Init is called but the module is already initialized. More... | |
| #define | GPT_E_INIT_FAILED (0x0EU) |
| API Gpt_Init is called but the module is already initialized. More... | |
| #define | GPT_E_PARAM_CHANNEL (0x14U) |
| API called with invalid channel. More... | |
| #define | GPT_E_PARAM_VALUE (0x15U) |
| API service called with invalid start timer parameter. More... | |
| #define | GPT_E_PARAM_POINTER (0x16U) |
| API service called with invalid(Null_Ptr) data buffer pointer. More... | |
| #define | GPT_E_PARAM_PREDEF_TIMER (0x17U) |
| API service called with invalid Predef Timer. Not supported in this implementation. More... | |
| #define | GPT_E_PARAM_MODE (0x1FU) |
| Gpt_SetMode is called with wrong mode parameter. More... | |
| #define | GPT_E_INVALID_ISR (0x80U) |
| Invalid entry to ISR. More... | |