![]() |
MCUSW
|
This file contains the interface of the Virtual Mac Ethernet driver.
Go to the source code of this file.
Functions | |
| FUNC (Std_ReturnType, ETH_CODE) Eth_VirtMacRpcInit(P2CONST(Eth_ConfigType | |
| This function initializes Eth Virtual MAC driver's Remote Procedure Call. More... | |
| FUNC (void, ETH_CODE) Eth_VirtMac_MainFunction(uint8 ctrlIdx) | |
| This function initializes the driver. More... | |
Variables | |
| AUTOMATIC | |
| ETH_PBCFG | CfgPtr |
| uint8 * | macAddress |
| uint8 * | ipv4Address |
| uint8 uint32 | vlanId |