MCUSW
Cdd_IpcIrq.h File Reference

Introduction

This file contains ISR function declaration for CDD IPC Driver.

Go to the source code of this file.

Functions

 FUNC (void, CDD_IPC_CODE_FAST) Cdd_IpcIrq_Fun(uint32 srcProcId)
 A Mailbox can raise multiple interrupts. In this implementation, the Mailbox new message interrupt is used determine presence of data from the remote core in the vring. More...