MCUSW
Can_Irq.h File Reference

Introduction

This file contains cover page for generating doxygen API documentation.

Go to the source code of this file.

Functions

 FUNC (void, CAN_CODE) Can_IntISR_Function(Can_ControllerInstance CanInstanceID
 This function is the ISR for CAN controller 0/INT 0. More...
 

Variables

uint32 baseAddr
 

Function Documentation

◆ FUNC()

FUNC ( void  ,
CAN_CODE   
)

This function is the ISR for CAN controller 0/INT 0.

*
*  Function name     : Can_IntISR_Fun
*  Syntax            : void Can_IntISR_Fun(Can_ControllerInstance CanInstanceID)
*  Mode              : Supervisor Mode (Privileged Mode)
*  Service ID[hex]   : N/A
*  Sync/Async        : Synchronous
*  Reentrancy        : Non-Reentrant
*  Parameters (in)   : None
*  Parameters (inout): None
*  Parameters (out)  : None
*  Return value      : None
*  Description       : This function is the ISR for CAN controller 0/INT 0 <br>
*                      This function should be invoked either by OS Interrupt
*                      frame handler <br>
*                      CAN Interrupt frame handler for Category 1 ISR
* 

Variable Documentation

◆ baseAddr

uint32 baseAddr