SimpleLink™ SDK Edge AI Plugin 9.12.00.00 Release Notes

Table of Contents

Introduction

The SimpleLink™ SDK EdgeAI Plugin (EDGEAI) from Texas Instruments is a plugin for enabling EdgeAI development on TI’s Wireless MUCs leveraging the TI’s Edge AIs Studio.

Documentation

The following documentation is provided with this release.

What’s New

This is the initial release of the Plugin. The main features that have been developed are:

Fixed Issues

This is the initial release of the Plugin.

Known Issues and Limitations

Operating System Support

Dependencies

EDGEAI requires the following dependency versions (or compatible):

Device Support

This SDK supports the following SimpleLink™ wireless MCUs:

Device Orderable Part Number (OPN) LaunchPad Product Page Migrate from these examples
CC2755R10 CC2755R105E0WRHAR N/A CC2755R10 LP-EM-CC2745R10-Q1
CC2755P10 CC2755P105E0WRHA N/A CC2755P10 N/A
CC2745R10-Q1 CC2745R10E0WRHARQ1 LP-EM-CC2745R10-Q1 CC2745R10-Q1 LP-EM-CC2745R10-Q1
CC2745R10-Q1 CC2745R10E1WRHARQ1 LP-EM-CC2745R10-Q1 CC2745R10-Q1 LP-EM-CC2745R10-Q1

Versioning

All releases have 4 segment versions (M.mm.pp.bb). This includes GA and pre-releases (engineering, alpha/EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 1.00.00.00_eng).

This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and bb is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory.

Subsequent releases of patch upgrades will be identified by the patch number. Typically, these patches only include critical bug fixes.

Technical Support

Last updated: 2025-11-28