EDGEAI API
Macros | Enumerations | Functions | Variables
feature_extract.h File Reference

Detailed Description

PRELIMINARY Feature Extraction for EdgeAI


WARNING These set of functions are PRELIMINARY, and subject to change in the next few months.

To use the Feature Extraction library, include this header file in the application as follows:

Overview

This library will serve as a pre-processing stage where raw signal inputs will be fed to the feature extraction library and the resulting output will be fed into the pre-compiled NN model. The function that have been implemented so far are the following:


Usage

To use the Feature Extraction Library call the previous APIs accordingly.

#include <stddef.h>
#include <stdint.h>
Include dependency graph for feature_extract.h:

Go to the source code of this file.

Macros

#define ADCSAMPLESIZE   125
 
#define SAMPLING_FREQ   25
 
#define PADDING_SIZE_LEFT   4
 
#define PADDING_SIZE_RIGHT   3
 
#define PADDED_INPUT_SIZE   (ADCSAMPLESIZE + PADDING_SIZE_LEFT + PADDING_SIZE_RIGHT)
 
#define WINDOW_SIZE   32
 
#define WINDOW_STRIDE_SIZE   4
 
#define NUM_WINDOWS   25
 
#define FFT_SIZE   64
 
#define NUM_BINS   (FFT_SIZE / 2)
 
#define POOLED_BINS   (NUM_BINS / 2)
 
#define TOP_N_FREQ   2
 
#define KURTOSIS_CHUNK_SIZE   8
 
#define KURTOSIS_STRIDE_SIZE   8
 
#define NUM_FEAT_FFT   16
 
#define NUM_FEAT_TOPFREQ   TOP_N_FREQ
 
#define NUM_FEAT_KURTOSIS   4
 
#define NUM_FEAT_ZCR   1
 
#define NUM_FEAT_SLOPE   1
 
#define NUM_FEAT_PW_SPEC   1
 
#define NUM_TOTAL_FEATURES   25
 

Enumerations

enum  fe_status_t {
  FE_OK = 0x00,
  FE_ERR_NULLPTR = 0x01,
  FE_ERR_BAD_PARAM = 0x02,
  FE_ERR_DSP = 0x03
}
 Specifies the FE status codes. More...
 

Functions

fe_status_t FE_applyWindow (const uint8_t *data_stream, uint8_t output_windows[25][32])
 Builds padded/sliding windows from an input stream considering a stride size. More...
 
fe_status_t FE_zeroCrossingRate (const uint8_t *input_window, float *zcr_out)
 Measures of how often a signal crosses the zero axis, indicating the frequency or noisiness of a signal. More...
 
fe_status_t FE_slopeChanges (const uint8_t *input_window, float *slope_changes)
 Counts the sign changes of signal differences. More...
 
fe_status_t FE_fftPool (const uint8_t *input_window, float *fft_output_pool_mag)
 calculate FFT magnitudes and pooling (averaging) to produce NUM_FEAT_FFT features. More...
 
fe_status_t FE_topFrequencies (const uint8_t *input_window, float *top_freqs)
 Extract the index of the dominant frequencies (Hz) per window. More...
 
fe_status_t FE_spectralEntropy (const uint8_t *input_window, float *entropy_out)
 Calculates the Shannon spectral entropy. The Spectral Entropy acts as an indicator of how spread out the power is. More...
 
fe_status_t FE_kurtosis (const uint8_t *input_window, float *kurtosis_output)
 Calculates the fisher or excess kurtosis without bias for each segment of a given series. Kurtosis describes the "peakedness" of a probability distribution. More...
 
fe_status_t FE_concatenateFeatures (const float *fft_output_pool_mag, uint32_t window_index, const float *kurtosis_output, const float *zcr, const float *slope_changes, const float *top_dominant_freq, const float *power_spectrum, float *concatenated_features)
 Concatenate many feature arrays into a big feature vector. The offsets are determined by NUM_FEAT_X and NUM_WINDOWS macros. More...
 

Variables

uint32_t samplingfreq
 

Macro Definition Documentation

§ ADCSAMPLESIZE

#define ADCSAMPLESIZE   125

§ SAMPLING_FREQ

#define SAMPLING_FREQ   25

§ PADDING_SIZE_LEFT

#define PADDING_SIZE_LEFT   4

§ PADDING_SIZE_RIGHT

#define PADDING_SIZE_RIGHT   3

§ PADDED_INPUT_SIZE

#define PADDED_INPUT_SIZE   (ADCSAMPLESIZE + PADDING_SIZE_LEFT + PADDING_SIZE_RIGHT)

§ WINDOW_SIZE

#define WINDOW_SIZE   32

§ WINDOW_STRIDE_SIZE

#define WINDOW_STRIDE_SIZE   4

§ NUM_WINDOWS

#define NUM_WINDOWS   25

§ FFT_SIZE

#define FFT_SIZE   64

§ NUM_BINS

#define NUM_BINS   (FFT_SIZE / 2)

§ POOLED_BINS

#define POOLED_BINS   (NUM_BINS / 2)

§ TOP_N_FREQ

#define TOP_N_FREQ   2

§ KURTOSIS_CHUNK_SIZE

#define KURTOSIS_CHUNK_SIZE   8

§ KURTOSIS_STRIDE_SIZE

#define KURTOSIS_STRIDE_SIZE   8

§ NUM_FEAT_FFT

#define NUM_FEAT_FFT   16

§ NUM_FEAT_TOPFREQ

#define NUM_FEAT_TOPFREQ   TOP_N_FREQ

§ NUM_FEAT_KURTOSIS

#define NUM_FEAT_KURTOSIS   4

§ NUM_FEAT_ZCR

#define NUM_FEAT_ZCR   1

§ NUM_FEAT_SLOPE

#define NUM_FEAT_SLOPE   1

§ NUM_FEAT_PW_SPEC

#define NUM_FEAT_PW_SPEC   1

§ NUM_TOTAL_FEATURES

#define NUM_TOTAL_FEATURES   25

Enumeration Type Documentation

§ fe_status_t

Specifies the FE status codes.

This enum defines the return states of the FE functions.

Enumerator
FE_OK 

Process ended successfully. The pointer to one of the function arguments has a NULL value.

FE_ERR_NULLPTR 

One of the Feature Extraction configuration parameters is incorrect or not supported.

FE_ERR_BAD_PARAM 

DSP operation has failed.

FE_ERR_DSP 

Function Documentation

§ FE_applyWindow()

fe_status_t FE_applyWindow ( const uint8_t *  data_stream,
uint8_t  output_windows[25][32] 
)

Builds padded/sliding windows from an input stream considering a stride size.

Parameters
[in]data_streampointer to input data stream [ADCSAMPLESIZE] for time series.
[out]output_windowspreallocated 2D-array [NUM_WINDOWS][WINDOW_SIZE].
Return values
FE_OKProcess ended successfully.
FE_ERR_NULLPTRThe pointer to one of the function arguments has a NULL value.
FE_ERR_BAD_PARAMOne of the Feature Extraction configuration parameters is incorrect or not supported.
FE_ERR_DSPDSP operation has failed.

§ FE_zeroCrossingRate()

fe_status_t FE_zeroCrossingRate ( const uint8_t *  input_window,
float *  zcr_out 
)

Measures of how often a signal crosses the zero axis, indicating the frequency or noisiness of a signal.

Parameters
[in]input_windowinput window uint8.
[out]zcr_outpointer to result float32.
Return values
FE_OKProcess ended successfully.
FE_ERR_NULLPTRThe pointer to one of the function arguments has a NULL value.
FE_ERR_BAD_PARAMOne of the Feature Extraction configuration parameters is incorrect or not supported.
FE_ERR_DSPDSP operation has failed.

§ FE_slopeChanges()

fe_status_t FE_slopeChanges ( const uint8_t *  input_window,
float *  slope_changes 
)

Counts the sign changes of signal differences.

Parameters
[in]input_windowinput window uint8.
[out]slope_changespointer to result float32.
Return values
FE_OKProcess ended successfully.
FE_ERR_NULLPTRThe pointer to one of the function arguments has a NULL value.
FE_ERR_BAD_PARAMOne of the Feature Extraction configuration parameters is incorrect or not supported.
FE_ERR_DSPDSP operation has failed.

§ FE_fftPool()

fe_status_t FE_fftPool ( const uint8_t *  input_window,
float *  fft_output_pool_mag 
)

calculate FFT magnitudes and pooling (averaging) to produce NUM_FEAT_FFT features.

Parameters
[in]input_windowinput window uint8.
[out]fft_output_pool_magpreallocated array of NUM_FEAT_FFT float32.
Return values
FE_OKProcess ended successfully.
FE_ERR_NULLPTRThe pointer to one of the function arguments has a NULL value.
FE_ERR_BAD_PARAMOne of the Feature Extraction configuration parameters is incorrect or not supported.
FE_ERR_DSPDSP operation has failed.

§ FE_topFrequencies()

fe_status_t FE_topFrequencies ( const uint8_t *  input_window,
float *  top_freqs 
)

Extract the index of the dominant frequencies (Hz) per window.

Parameters
[in]input_windowinput window uint8.
[out]top_freqspreallocated array of length TOP_N_FREQ.
Return values
FE_OKProcess ended successfully.
FE_ERR_NULLPTRThe pointer to one of the function arguments has a NULL value.
FE_ERR_BAD_PARAMOne of the Feature Extraction configuration parameters is incorrect or not supported.
FE_ERR_DSPDSP operation has failed.

§ FE_spectralEntropy()

fe_status_t FE_spectralEntropy ( const uint8_t *  input_window,
float *  entropy_out 
)

Calculates the Shannon spectral entropy. The Spectral Entropy acts as an indicator of how spread out the power is.

Parameters
[in]input_windowinput window uint8.
[out]entropy_outpointer to float32 result.
Return values
FE_OKProcess ended successfully.
FE_ERR_NULLPTRThe pointer to one of the function arguments has a NULL value.
FE_ERR_BAD_PARAMOne of the Feature Extraction configuration parameters is incorrect or not supported.
FE_ERR_DSPDSP operation has failed.

§ FE_kurtosis()

fe_status_t FE_kurtosis ( const uint8_t *  input_window,
float *  kurtosis_output 
)

Calculates the fisher or excess kurtosis without bias for each segment of a given series. Kurtosis describes the "peakedness" of a probability distribution.

Parameters
[in]input_windowinput window uint8.
[out]kurtosis_outputpreallocated array of NUM_FEAT_KURTOSIS float32.
Return values
FE_OKProcess ended successfully.
FE_ERR_NULLPTRThe pointer to one of the function arguments has a NULL value.
FE_ERR_BAD_PARAMOne of the Feature Extraction configuration parameters is incorrect or not supported.
FE_ERR_DSPDSP operation has failed.

§ FE_concatenateFeatures()

fe_status_t FE_concatenateFeatures ( const float *  fft_output_pool_mag,
uint32_t  window_index,
const float *  kurtosis_output,
const float *  zcr,
const float *  slope_changes,
const float *  top_dominant_freq,
const float *  power_spectrum,
float *  concatenated_features 
)

Concatenate many feature arrays into a big feature vector. The offsets are determined by NUM_FEAT_X and NUM_WINDOWS macros.

Parameters
[in]fft_output_pool_magpointer to FFT features (NUM_FEAT_FFT)
[in]window_indexwhich window this belongs to (0 .. NUM_WINDOWS-1)
[in]kurtosis_outputpointer to NUM_FEAT_KURTOSIS values
[in]zcrpointer to zcr value (scalar)
[in]slope_changespointer to slope_changes value (scalar)
[in]top_dominant_freqpointer to TOP_N_FREQ values
[in]power_spectrumpointer to spectral entropy (scalar)
[out]concatenated_featurespreallocated feature vector of size NUM_TOTAL_FEATURES * NUM_WINDOWS
Return values
FE_OKProcess ended successfully.
FE_ERR_NULLPTRThe pointer to one of the function arguments has a NULL value.
FE_ERR_BAD_PARAMOne of the Feature Extraction configuration parameters is incorrect or not supported.
FE_ERR_DSPDSP operation has failed.

Variable Documentation

§ samplingfreq

uint32_t samplingfreq
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale