![]() |
![]() |
|
EDGEAI API
|
#include <ti/ai/edge_ai/dap/core/DAP_core.h>
Go to the source code of this file.
Variables | |
| const char | Device_name [] |
| const uint8_t | SDK_version [2] |
| const uint8_t | availableSensorsCount |
| const char * | sensorInformation [] |
| uint8_t | availableModelsCount |
| const char * | modelInformation [] |
| uint8_t | inferencesCount |
| const DAP_Inference | inferences [] |
| uint16_t | propertiesCount |
| DAP_Property | properties [] |
| const char Device_name[] |
| const uint8_t SDK_version[2] |
| const uint8_t availableSensorsCount |
| const char* sensorInformation[] |
| uint8_t availableModelsCount |
| const char* modelInformation[] |
| uint8_t inferencesCount |
| const DAP_Inference inferences[] |
| uint16_t propertiesCount |
| DAP_Property properties[] |