33 #ifndef ti_edgeai_DAP_core__include 34 #define ti_edgeai_DAP_core__include 46 #define DAP_MAX_FRAME_SIZE_BYTES (200) Definition: DAP_core.h:204
Definition: DAP_core.h:113
Definition: DAP_core.h:139
Definition: DAP_core.h:68
Data Types for the inferences and properties.
Definition: DAP_core.h:224
uint16_t u16
Definition: DAP_core.h:231
void DAP_sendError(DAP_Handle *dapHandle, DAP_CommandType command, const char errorMessage[])
Send error to host.
DAP_CommandPayloadFixedLength
Minimum payload length of commands sent from the host to the target.
Definition: DAP_core.h:126
Definition: DAP_core.h:133
DAP_DataTypes dataFormat
Definition: DAP_core.h:245
DAP configuration.
Definition: DAP.h:156
Definition: DAP_core.h:145
Definition: DAP_core.h:216
Definition: DAP_core.h:206
Definition: DAP_core.h:108
Definition: DAP_core.h:111
Definition: DAP_core.h:165
Definition: DAP_core.h:129
Definition: DAP_core.h:173
Definition: DAP_core.h:189
Definition: DAP_core.h:98
Definition: DAP_core.h:72
Definition: DAP_core.h:208
DAP_SendDataType
Definition: DAP.h:171
uint8_t index
Definition: DAP_core.h:57
Definition: DAP_core.h:115
DAP_CommandType
DAP command types.
Definition: DAP_core.h:85
Definition: DAP_core.h:70
Definition: DAP_core.h:193
Definition: DAP_core.h:153
Definition: DAP_core.h:141
DAP_ErrorType
DAP error types.
Definition: DAP_core.h:63
DAP_ErrorType DAP_verifyFrame(DAP_Frame *frame)
Verify a frame.
int8_t i8
Definition: DAP_core.h:233
Definition: DAP_core.h:175
DAP_ResponsePayloadFixedLength
Minimum payload length of commands sent from the target to the host.
Definition: DAP_core.h:162
Definition: DAP_core.h:90
Definition: DAP_core.h:185
Definition: DAP_core.h:92
Definition: DAP_core.h:191
float f32
Definition: DAP_core.h:237
const char * name
Definition: DAP_core.h:226
Definition: DAP_core.h:151
double f64
Definition: DAP_core.h:238
size_t length
Definition: DAP_core.h:54
int16_t i16
Definition: DAP_core.h:234
uint8_t u8
Definition: DAP_core.h:230
#define DAP_MAX_FRAME_SIZE_BYTES
Definition: DAP_core.h:46
Definition: DAP_core.h:242
Definition: DAP_core.h:96
Definition: DAP_core.h:171
Definition: DAP_core.h:106
Definition: DAP_core.h:187
Definition: DAP_core.h:218
Definition: DAP_core.h:137
PRELIMINARY DAP for EdgeAI
Definition: DAP_core.h:104
Definition: DAP_core.h:177
Definition: DAP_core.h:210
float f16
Definition: DAP_core.h:236
Definition: DAP_core.h:155
Definition: DAP_core.h:214
Definition: DAP_core.h:48
Definition: DAP_core.h:179
Definition: DAP_core.h:167
void DAP_serviceCommand(DAP_Handle *dapHandle, DAP_Frame *commandFrame)
Service a command sent by the host.
void DAP_receiveDataCommand(DAP_Handle *dapHandle, DAP_SendDataType sendDataType, void *data, size_t dataSize)
Send data to host.
int32_t i32
Definition: DAP_core.h:235
const char * info
Definition: DAP_core.h:244
Definition: DAP_core.h:149
Definition: DAP_core.h:131
Definition: DAP_core.h:74
DAP_DataTypes dataFormat
Definition: DAP_core.h:227
Definition: DAP_core.h:102
Definition: DAP_core.h:202
Definition: DAP_core.h:212
Definition: DAP_core.h:183
Definition: DAP_core.h:100
Definition: DAP_core.h:119
Definition: DAP_core.h:117
Definition: DAP_core.h:88
Definition: DAP_core.h:66
Definition: DAP_core.h:181
Definition: DAP_core.h:169
DAP_DataTypes
Data Types for the inferences and properties.
Definition: DAP_core.h:199
Definition: DAP_core.h:147
Definition: DAP_core.h:143
Definition: DAP_core.h:135
uint32_t u32
Definition: DAP_core.h:232
Definition: DAP_core.h:94
Definition: DAP_core.h:76