EDGEAI API
Data Structures | Macros | Enumerations | Functions
DAP_core.h File Reference
#include <stdint.h>
#include <stdbool.h>
#include <string.h>
#include <ti/ai/edge_ai/dap/DAP.h>
Include dependency graph for DAP_core.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  DAP_Frame
 
struct  DAP_Property
 Data Types for the inferences and properties. More...
 
struct  DAP_Inference
 

Macros

#define DAP_MAX_FRAME_SIZE_BYTES   (200)
 

Enumerations

enum  DAP_ErrorType {
  DAP_ERROR_TYPE_NONE = 0x00,
  DAP_ERROR_TYPE_MISMATCH_START_BYTE = 0xE1,
  DAP_ERROR_TYPE_MISMATCH_END_BYTE = 0xE2,
  DAP_ERROR_TYPE_ADDR_RANGE = 0xE3,
  DAP_ERROR_TYPE_MISMATCH_CRC = 0xE4,
  DAP_ERROR_TYPE_MISMATCH_TARGET_ADDR = 0xE5
}
 DAP error types. More...
 
enum  DAP_CommandType {
  DAP_ERROR_COMMAND = 0x00,
  DAP_GET_CAPABILITIES_COMMAND = 0x01,
  DAP_LIST_SENSORS_COMMAND = 0x02,
  DAP_CONFIGURE_PIPELINE_COMMAND = 0x03,
  DAP_LIST_MODELS_COMMAND = 0x04,
  DAP_REMOVE_MODEL_COMMAND = 0x05,
  DAP_START_MODEL_UPLOAD_COMMAND = 0x06,
  DAP_END_MODEL_UPLOAD_COMMAND = 0x07,
  DAP_START_STREAMING_COMMAND = 0x08,
  DAP_STOP_STREAMING_COMMAND = 0x09,
  DAP_LIST_INFERENCING_VALUES_COMMAND = 0x0a,
  DAP_READ_PROPERTY_COMMAND = 0x0c,
  DAP_WRITE_PROPERTY_COMMAND = 0x0d,
  DAP_LIST_PROPERTIES_COMMAND = 0x0e,
  DAP_SEND_DATA_COMMAND = 0x10,
  DAP_RECEIVE_DATA_COMMAND = 0x10
}
 DAP command types. More...
 
enum  DAP_CommandPayloadFixedLength {
  DAP_GET_CAPABILITIES_CMD_FIXED_LENGHT = 0,
  DAP_LIST_SENSORS_FIXED_CMD_LENGHT = 0,
  DAP_CONFIGURE_PIPELINE_CMD_FIXED_LENGHT = 2,
  DAP_LIST_MODELS_CMD_FIXED_LENGHT = 0,
  DAP_REMOVE_MODEL_CMD_FIXED_LENGTH = 1,
  DAP_START_MODEL_UPLOAD_CMD_FIXED_LENGTH = 0,
  DAP_END_MODEL_UPLOAD_CMD_FIXED_LENGTH = 4,
  DAP_START_STREAMING_CMD_FIXED_LENGHT = 0,
  DAP_STOP_STREAMING_CMD_FIXED_LENGHT = 0,
  DAP_LIST_INFERENCING_VALUES_CMD_FIXED_LENGTH = 0,
  DAP_READ_PROPERTY_CMD_FIXED_LENGHT = 1,
  DAP_WRITE_PROPERTY_CMD_FIXED_LENGHT = 1,
  DAP_LIST_PROPERTIES_CMD_FIXED_LENGHT = 0,
  DAP_DATA_CMD_FIXED_LENGTH = 0
}
 Minimum payload length of commands sent from the host to the target. More...
 
enum  DAP_ResponsePayloadFixedLength {
  DAP_ERROR_FIXED_LENGHT = 2,
  DAP_GET_CAPABILITIES_FIXED_LENGHT = 4,
  DAP_LIST_SENSORS_FIXED_LENGHT = 2,
  DAP_CONFIGURE_PIPELINE_FIXED_LENGHT = 0,
  DAP_LIST_MODELS_FIXED_LENGHT = 2,
  DAP_REMOVE_MODEL_FIXED_LENGTH = 0,
  DAP_START_MODEL_UPLOAD_FIXED_LENGTH = 0,
  DAP_END_MODEL_UPLOAD_FIXED_LENGTH = 0,
  DAP_START_STREAMING_FIXED_LENGHT = 0,
  DAP_STOP_STREAMING_FIXED_LENGHT = 0,
  DAP_LIST_INFERENCING_VALUES_FIXED_LENGTH = 3,
  DAP_READ_PROPERTY_FIXED_LENGHT = 1,
  DAP_WRITE_PROPERTY_FIXED_LENGHT = 1,
  DAP_LIST_PROPERTIES_FIXED_LENGHT = 3,
  DAP_DATA_FIXED_LENGTH = 0
}
 Minimum payload length of commands sent from the target to the host. More...
 
enum  DAP_DataTypes {
  DAP_DATA_TYPE_INT8 = 0x01,
  DAP_DATA_TYPE_INT16 = 0x02,
  DAP_DATA_TYPE_INT32 = 0x03,
  DAP_DATA_TYPE_UINT8 = 0x04,
  DAP_DATA_TYPE_UINT16 = 0x05,
  DAP_DATA_TYPE_UINT32 = 0x06,
  DAP_DATA_TYPE_FLOAT16 = 0x07,
  DAP_DATA_TYPE_FLOAT32 = 0x08,
  DAP_DATA_TYPE_FLOAT64 = 0x09
}
 Data Types for the inferences and properties. More...
 

Functions

DAP_ErrorType DAP_verifyFrame (DAP_Frame *frame)
 Verify a frame. More...
 
void DAP_serviceCommand (DAP_Handle *dapHandle, DAP_Frame *commandFrame)
 Service a command sent by the host. More...
 
void DAP_sendError (DAP_Handle *dapHandle, DAP_CommandType command, const char errorMessage[])
 Send error to host. More...
 
void DAP_receiveDataCommand (DAP_Handle *dapHandle, DAP_SendDataType sendDataType, void *data, size_t dataSize)
 Send data to host. More...
 

Macro Definition Documentation

§ DAP_MAX_FRAME_SIZE_BYTES

#define DAP_MAX_FRAME_SIZE_BYTES   (200)

Enumeration Type Documentation

§ DAP_ErrorType

DAP error types.

Enumerator
DAP_ERROR_TYPE_NONE 

No error

DAP_ERROR_TYPE_MISMATCH_START_BYTE 

Mismatch Start byte error

DAP_ERROR_TYPE_MISMATCH_END_BYTE 

Mismatch end byte error

DAP_ERROR_TYPE_ADDR_RANGE 

Error in Address range

DAP_ERROR_TYPE_MISMATCH_CRC 

Mismatch CRC error

DAP_ERROR_TYPE_MISMATCH_TARGET_ADDR 

Mismatch target address error

§ DAP_CommandType

DAP command types.

This enum defines the commands that can be sent between the host and the target.

Enumerator
DAP_ERROR_COMMAND 

Sent from target to host to indicate there has been an error.

DAP_GET_CAPABILITIES_COMMAND 

Get software capabilities and metadata.

DAP_LIST_SENSORS_COMMAND 

List all available sensors.

DAP_CONFIGURE_PIPELINE_COMMAND 

Configure the application.

DAP_LIST_MODELS_COMMAND 

List all available models.

DAP_REMOVE_MODEL_COMMAND 

Remove one of the models.

DAP_START_MODEL_UPLOAD_COMMAND 

Signal the target that the host will start sending data.

DAP_END_MODEL_UPLOAD_COMMAND 

Signal the target that the host is done sending data.

DAP_START_STREAMING_COMMAND 

Signal the target to start sending data to the host.

DAP_STOP_STREAMING_COMMAND 

Signal the target to stop sending data to the host.

DAP_LIST_INFERENCING_VALUES_COMMAND 

List all inference values.

DAP_READ_PROPERTY_COMMAND 

Read a sampling property.

DAP_WRITE_PROPERTY_COMMAND 

Write to a sampling property,

DAP_LIST_PROPERTIES_COMMAND 

List all sampling properties.

DAP_SEND_DATA_COMMAND 

Data comming from the host to the target (model upload).

DAP_RECEIVE_DATA_COMMAND 

Data comming from the target to the host (streaming).

§ DAP_CommandPayloadFixedLength

Minimum payload length of commands sent from the host to the target.

Enumerator
DAP_GET_CAPABILITIES_CMD_FIXED_LENGHT 

No fixed payload

DAP_LIST_SENSORS_FIXED_CMD_LENGHT 

No fixed payload

DAP_CONFIGURE_PIPELINE_CMD_FIXED_LENGHT 

Mode, Model Index

DAP_LIST_MODELS_CMD_FIXED_LENGHT 

No fixed payload

DAP_REMOVE_MODEL_CMD_FIXED_LENGTH 

Model Index

DAP_START_MODEL_UPLOAD_CMD_FIXED_LENGTH 

No fixed payload

DAP_END_MODEL_UPLOAD_CMD_FIXED_LENGTH 

Checksum

DAP_START_STREAMING_CMD_FIXED_LENGHT 

No fixed payload

DAP_STOP_STREAMING_CMD_FIXED_LENGHT 

No fixed payload

DAP_LIST_INFERENCING_VALUES_CMD_FIXED_LENGTH 

No fixed payload

DAP_READ_PROPERTY_CMD_FIXED_LENGHT 

Property Index

DAP_WRITE_PROPERTY_CMD_FIXED_LENGHT 

Property Index

DAP_LIST_PROPERTIES_CMD_FIXED_LENGHT 

No fixed payload

DAP_DATA_CMD_FIXED_LENGTH 

No fixed payload

§ DAP_ResponsePayloadFixedLength

Minimum payload length of commands sent from the target to the host.

Enumerator
DAP_ERROR_FIXED_LENGHT 

Command, Error Number

DAP_GET_CAPABILITIES_FIXED_LENGHT 

API Versio, Capability Flag, SDK Major Version, SDK Minor Version

DAP_LIST_SENSORS_FIXED_LENGHT 

Sensor Count, Sensor Index

DAP_CONFIGURE_PIPELINE_FIXED_LENGHT 

No fixed payload

DAP_LIST_MODELS_FIXED_LENGHT 

Model Count, Model Index

DAP_REMOVE_MODEL_FIXED_LENGTH 

No fixed payload

DAP_START_MODEL_UPLOAD_FIXED_LENGTH 

No fixed payload

DAP_END_MODEL_UPLOAD_FIXED_LENGTH 

No fixed payload

DAP_START_STREAMING_FIXED_LENGHT 

No fixed payload

DAP_STOP_STREAMING_FIXED_LENGHT 

No fixed payload

DAP_LIST_INFERENCING_VALUES_FIXED_LENGTH 

Inference Count, Inference Index, Inference Data Format

DAP_READ_PROPERTY_FIXED_LENGHT 

Property Index

DAP_WRITE_PROPERTY_FIXED_LENGHT 

Property Index

DAP_LIST_PROPERTIES_FIXED_LENGHT 

Property Count, Property Index, Property Data Format

DAP_DATA_FIXED_LENGTH 

No fixed payload

§ DAP_DataTypes

Data Types for the inferences and properties.

Enumerator
DAP_DATA_TYPE_INT8 

8-bit signed integer

DAP_DATA_TYPE_INT16 

16-bit signed integer

DAP_DATA_TYPE_INT32 

32-bit signed integer

DAP_DATA_TYPE_UINT8 

8-bit unsigned integer

DAP_DATA_TYPE_UINT16 

16-bit unsigned integer

DAP_DATA_TYPE_UINT32 

32-bit unsigned integer

DAP_DATA_TYPE_FLOAT16 

16-bit half precision floating point value

DAP_DATA_TYPE_FLOAT32 

32-bit normal precision floating point value

DAP_DATA_TYPE_FLOAT64 

64-bit double precision floating point value

Function Documentation

§ DAP_verifyFrame()

DAP_ErrorType DAP_verifyFrame ( DAP_Frame frame)

Verify a frame.

This function verify if a frame is well constructed

Parameters
[in]framepointer to a frame
Returns
Returns if there is an error in the frame.

§ DAP_serviceCommand()

void DAP_serviceCommand ( DAP_Handle dapHandle,
DAP_Frame commandFrame 
)

Service a command sent by the host.

This function decodes the command sent by the host and generates a response packet based on the command received.

Parameters
[in]dapHandlepointer
[in]commandFramepointer to the received packet.

§ DAP_sendError()

void DAP_sendError ( DAP_Handle dapHandle,
DAP_CommandType  command,
const char  errorMessage[] 
)

Send error to host.

This function sends an error packet to the host. Errors can be synchronous, in response to a command, or asynchronous, errors that are not sent in response to any specific command, such as, errors during streaming operations.

Parameters
[in]dapHandlepointer
[in]commanderror type
[in]errorMessagestring with the error message

§ DAP_receiveDataCommand()

void DAP_receiveDataCommand ( DAP_Handle dapHandle,
DAP_SendDataType  sendDataType,
void *  data,
size_t  dataSize 
)

Send data to host.

This function sends a buffer of data to the DAP

Parameters
[in]dapHandlepointer
[in]sendDataTypeType of the data sent
[in]datapointer to a buffer with the data
[in]dataSizesize of the data buffer in bytes
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale