EDGEAI API
Data Fields
DAP_Frame Struct Reference

#include <ti/ai/edge_ai/dap/core/DAP_core.h>

Collaboration diagram for DAP_Frame:
Collaboration graph

Data Fields

uint8_t buffer [(200)]
 
size_t length
 
uint8_t index
 

Field Documentation

§ buffer

uint8_t DAP_Frame::buffer[(200)]

Pointer to buffer

§ length

size_t DAP_Frame::length

Length in bytes

§ index

uint8_t DAP_Frame::index

Buffer Index


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale