EDGEAI API
Variables
DAP_interface.h File Reference
#include <ti/ai/edge_ai/dap/core/DAP_core.h>
Include dependency graph for DAP_interface.h:

Go to the source code of this file.

Variables

const char Device_name []
 
const uint8_t SDK_version [2]
 
const uint8_t availableSensorsCount
 
const char * sensorInformation []
 
uint8_t availableModelsCount
 
const char * modelInformation []
 
uint8_t inferencesCount
 
const DAP_Inference inferences []
 
uint16_t propertiesCount
 
DAP_Property properties []
 

Variable Documentation

§ Device_name

const char Device_name[]

§ SDK_version

const uint8_t SDK_version[2]

§ availableSensorsCount

const uint8_t availableSensorsCount

§ sensorInformation

const char* sensorInformation[]

§ availableModelsCount

uint8_t availableModelsCount

§ modelInformation

const char* modelInformation[]

§ inferencesCount

uint8_t inferencesCount

§ inferences

const DAP_Inference inferences[]

§ propertiesCount

uint16_t propertiesCount

§ properties

DAP_Property properties[]
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale