Sensor Controller Studio CLI for Linux Manifest
06-19-2019
Manifest ID - SRAS00006359
Legend
(explanation of the fields in the Manifest Table below)
|
Software Name
|
The name of the application or file
|
|
Version
|
Version of the application or file
|
|
License Type
|
Type of license(s) under which TI will be providing
software to the licensee (e.g. BSD-3-Clause, GPL-2.0, TI Text File License, TI
Commercial License). The license could be under Commercial terms or Open Source. See Open Source Reference License Disclaimer in
the Disclaimers Section. Whenever possible, TI will use an SPDX Short Identifier for an Open Source
License. TI Commercial license terms are not usually included in the manifest and are conveyed through a variety
of means such as a clickwrap license upon install,
a signed license agreement and so forth.
|
|
Location
|
The directory name and path on the media or a specific file where the Software is located. Typically fully qualified path names
are not used and instead the relevant top level directory of the application is given.
A notation often used in the manifests is [as installed]/directory/*. Note that the asterisk implies that all
files under that directory are licensed as the License Type field denotes. Any exceptions to this will
generally be denoted as [as installed]/directory/* except as noted below which means as shown in subsequent rows of
the manifest.
|
|
Delivered As
|
This field will either be “Source”, “Binary” or “Source
and Binary” and is the primary form the content of the Software is delivered
in. If the Software is delivered in an archive format, this field
applies to the contents of the archive. If the word Limited is used
with Source, as in “Limited Source” or “Limited Source and Binary” then
only portions of the Source for the application are provided.
|
|
Modified by TI
|
This field will either be “Yes” or “No”. A “Yes” means
TI has made changes to the Software. A “No” means TI has not made any
changes. Note: This field is not applicable for Software “Obtained
from” TI.
|
|
Obtained from
|
This field specifies from where or from whom TI obtained
the Software. It may be a URL to an Open Source site, a 3rd
party licensor, or TI. See Links Disclaimer in the Disclaimers
Section.
|
Disclaimers
Export Control Classification Number (ECCN)
Any use of ECCNs listed in the Manifest is at the user’s risk
and without recourse to TI. Your
company, as the exporter of record, is responsible for determining the
correct classification of any item at
the time of export. Any export classification by TI of Software is for
TI’s internal use only and shall not be construed as a representation
or warranty
regarding the proper export classification for such Software or whether
an export
license or other documentation is required for exporting such Software
Links in the Manifest
Any
links appearing on this Manifest
(for example in the “Obtained from” field) were verified at the time
the Manifest was created. TI makes no guarantee that any listed links
will
remain active in the future.
Open Source License References
Your company is responsible for confirming the
applicable license terms for any open source Software
listed in this Manifest that was not “Obtained from” TI. Any open
source license
specified in this Manifest for Software that was
not “Obtained from” TI is for TI’s internal use only and shall not be
construed as a representation or warranty regarding the proper open
source license terms
for such Software.
Export Information
ECCN for Software included in this release:
EAR99
Sensor Controller Studio CLI for Linux Manifest Table
See the Legend above for a description of these columns.
| Software Name |
Version |
License Type |
Delivered As |
Modified by TI |
|
|
|
Sensor Controller Studio CLI for Linux
|
2.5.0
|
TI Commercial
|
Binary
|
N/A
|
Location |
[installed path]/bin
|
| Obtained from |
TI
|
|
Qt(1)
|
5.9.2
|
LGPL-3.0
|
Binary and Source
|
No
|
Location |
Binaries: [installed path]/lib,Source: http://software-dl.ti.com/manifest/esd/exports/qt-everywhere-opensource-src-5.9.2.tar.xz
|
| Obtained from |
https://download.qt.io/archive/qt/5.9/5.9.2/qt-opensource-linux-x64-5.9.2.run Downloaded: December 4, 2012
|
1) The Qt source and binaries are distributed subject to the LGPL v3.0 license. A copy of the LGPL v3.0 license can be found in this document. Please refer to http://qt-project.org/doc/qt-5/licensing.html for information about Qt's licenses and the licenses of third party components used in Qt.
Credits
Licenses
Sensor Controller Studio CLI for Linux Licenses
LGPL-3.0 License
GNU LESSER GENERAL PUBLIC LICENSE
Version 3, 29 June 2007
Copyright (C) 2007 Free Software Foundation, Inc. http://fsf.org/
Everyone is permitted to copy and distribute verbatim copies of this license document, but changing it is not allowed.
This version of the GNU Lesser General Public License incorporates the terms and conditions of version 3 of the GNU General Public License, supplemented by the additional permissions listed below.
0. Additional Definitions.
As used herein, "this License" refers to version 3 of the GNU Lesser General Public License, and the "GNU GPL" refers to version 3 of the GNU General Public License.
"The Library" refers to a covered work governed by this License, other than an Application or a Combined Work as defined below.
An "Application" is any work that makes use of an interface provided by the Library, but which is not otherwise based on the Library. Defining a subclass of a class defined by the Library is deemed a mode of using an interface provided by the Library.
A "Combined Work" is a work produced by combining or linking an Application with the Library. The particular version of the Library with which the Combined Work was made is also called the "Linked Version".
The "Minimal Corresponding Source" for a Combined Work means the Corresponding Source for the Combined Work, excluding any source code for portions of the Combined Work that, considered in isolation, are based on the Application, and not on the Linked Version.
The "Corresponding Application Code" for a Combined Work means the object code and/or source code for the Application, including any data and utility programs needed for reproducing the Combined Work from the Application, but excluding the System Libraries of the Combined Work.
1. Exception to Section 3 of the GNU GPL.
You may convey a covered work under sections 3 and 4 of this License without being bound by section 3 of the GNU GPL.
2. Conveying Modified Versions.
If you modify a copy of the Library, and, in your modifications, a facility refers to a function or data to be supplied by an Application that uses the facility (other than as an argument passed when the facility is invoked), then you may convey a copy of the modified version:
a) under this License, provided that you make a good faith effort to ensure that, in the event an Application does not supply the function or data, the facility still operates, and performs whatever part of its purpose remains meaningful, or
b) under the GNU GPL, with none of the additional permissions of this License applicable to that copy.
3. Object Code Incorporating Material from Library Header Files.
The object code form of an Application may incorporate material from a header file that is part of the Library. You may convey such object code under terms of your choice, provided that, if the incorporated material is not limited to numerical parameters, data structure layouts and accessors, or small macros, inline functions and templates (ten or fewer lines in length), you do both of the following:
a) Give prominent notice with each copy of the object code that the Library is used in it and that the Library and its use are covered by this License.
b) Accompany the object code with a copy of the GNU GPL and this license document.
4. Combined Works.
You may convey a Combined Work under terms of your choice that, taken together, effectively do not restrict modification of the portions of the Library contained in the Combined Work and reverse engineering for debugging such modifications, if you also do each of the following:
a) Give prominent notice with each copy of the Combined Work that the Library is used in it and that the Library and its use are covered by this License.
b) Accompany the Combined Work with a copy of the GNU GPL and this license document.
c) For a Combined Work that displays copyright notices during execution, include the copyright notice for the Library among these notices, as well as a reference directing the user to the copies of the GNU GPL and this license document.
d) Do one of the following:
0) Convey the Minimal Corresponding Source under the terms of this License, and the Corresponding Application Code in a form suitable for, and under terms that permit, the user to recombine or relink the Application with a modified version of the Linked Version to produce a modified Combined Work, in the manner specified by section 6 of the GNU GPL for conveying Corresponding Source.
1) Use a suitable shared library mechanism for linking with the Library. A suitable mechanism is one that (a) uses at run time a copy of the Library already present on the user's computer system, and (b) will operate properly with a modified version of the Library that is interface-compatible with the Linked Version.
e) Provide Installation Information, but only if you would otherwise be required to provide such information under section 6 of the GNU GPL, and only to the extent that such information is necessary to install and execute a modified version of the Combined Work produced by recombining or relinking the Application with a modified version of the Linked Version. (If you use option 4d0, the Installation Information must accompany the Minimal Corresponding Source and Corresponding Application Code. If you use option 4d1, you must provide the Installation Information in the manner specified by section 6 of the GNU GPL for conveying Corresponding Source.)
5. Combined Libraries.
You may place library facilities that are a work based on the Library side by side in a single library together with other library facilities that are not Applications and are not covered by this License, and convey such a combined library under terms of your choice, if you do both of the following:
a) Accompany the combined library with a copy of the same work based on the Library, uncombined with any other library facilities, conveyed under the terms of this License.
b) Give prominent notice with the combined library that part of it is a work based on the Library, and explaining where to find the accompanying uncombined form of the same work.
6. Revised Versions of the GNU Lesser General Public License.
The Free Software Foundation may publish revised and/or new versions of the GNU Lesser General Public License from time to time. Such new versions will be similar in spirit to the present version, but may differ in detail to address new problems or concerns.
Each version is given a distinguishing version number. If the Library as you received it specifies that a certain numbered version of the GNU Lesser General Public License "or any later version" applies to it, you have the option of following the terms and conditions either of that published version or of any later version published by the Free Software Foundation. If the Library as you received it does not specify a version number of the GNU Lesser General Public License, you may choose any version of the GNU Lesser General Public License ever published by the Free Software Foundation.
If the Library as you received it specifies that a proxy can decide whether future versions of the GNU Lesser General Public License shall
apply, that proxy's public statement of acceptance of any version is permanent authorization for you to choose that version for the Library.