Release Notes for Code Composer Studio™ Theia v1.4.0
These release notes contain valuable information which may not be included in other product documentation. This information will assist you in the use of Code Composer Studio™ Theia.The release notes are divided into five sections:
Contents
CCS Theia is a new Integrated Development Environment (IDE) based on Theia IDE framework. CCS Theia v1.4.0 uses a modified version of Theia-IDE. ( https://theia-ide.org/ )
CCS Theia has a more limited set of features and limited set of devices. Each release will add support for new features and new devices.
For additional information and support, please go to:
https://software-dl.ti.com/ccs/esd/documents/users_guide_ccs_theia/index.html
Please note that Code Composer Studio Theia v1.4.0 is recommended for production development with MSPM0, and MSP430 devices. CCS Theia includes optional support for Wireless connectivity (not WiFi), Sitara, and mmWave devices. Evaluation support for C2000 devices is included.
Please note that Code Composer Studio Theia is a 64bit application and thus will not run on 32bit operating systems.
Supported distributions include:
Code Composer Studio Theia will run on other distributions but those are the officially supported and tested distributions. For more details on installation instructions as well as debug probe and device support please see this article on Linux Host Support.
Versions Supported
Each Code Composer Studio Theia release is validated against a set of macOS releases. This release was validated with:
Debug Probe Support
Details of the macOS releases, debug probes and devices supported is available here.
Please note that use of anti-virus software or a firewall may cause issues during installation.
McAfee software in particular has been especially troublesome.
If possible, disable anti-virus and firewall software during installation.
If not, use of the Offline Installer is strongly recommended.On Windows:
If you are using an Offline CCS Theia Installer, the zip file in which it is
distributed must first be extracted:1. Right-click on CCSTheia1.x.x.xxxxx_win64.zip and select "Extract All...".
2. Enter the directory where you wish to extract the files.
3. Click on Extract.Once extraction has successfully completed, proceed with the installation steps below.
To install Code Composer Studio Theia:1. Run ccs_theia_setup_1.x.x.xxxxx.exe.
2. Choose where you want to install.
3. Select the components you wish to install.On OS X:
Please visit https://software-dl.ti.com/ccs/esd/documents/ccs_macos_host_support.html
The offline installer is now distributed as disk images (.dmg files)
1. Right-click on CCSTheia1.x.x.xxxxx_osx.dmg and select "Open”. This will open the disk image and mount it.
To install Code Composer Studio Theia:1. Run ccs_theia_setup_1.x.x.xxxxx by clicking on the application in the Finder
2. Choose where you want to install.
3. Select the components you wish to install.On Linux:
Please visit https://software-dl.ti.com/ccs/esd/documents/ccs_linux_host_support.html
before installing CCS Theia on Linux. It contains important information on
installing CCS Theia on different Linux distributions, including CCS Theia dependencies that may need to be installed first.
Before installing CCS Theia, the tarball file in which the CCS Theia Installer is distributed must first be extracted:untar CCSTheia1.x.x.xxxxx_linux-x64.tar.gz and extract all files.
e.g. tar xfz CCSTheia1.x.x.xxxxx_linux-x64.tar.gz
Once extraction has successfully completed, proceed with the installation steps below.
Note: To facilitate the installation of emulation drivers, it is necessary to run part of the installation process as root.
You may if you wish install all of CCS Theia as root. However, it is preferred that you first install CCS Theia as a normal user and then install the drivers as root.
To install Code Composer Studio Theia as a normal user and emulation drivers as root:1. Run ccs_theia_setup_1.x.x.xxxxx.run as a normal user.
2. Choose where you want to install.
3. Select the components you wish to install.
4. Navigate to directory <Install-Folder>/ccs/install_scripts.
5. As root, execute script "install_drivers.sh".To install all of Code Composer Studio Theia as root:
1. Run ccs_theia_setup_1.x.x.xxxxx.run as root.
2. Choose where you want to install.
3. Select the components you wish to install.
· V1.4.0 is an incremental update to the CCS Theia product with many new updates and improvements. The changes included:
o Update to Theia v1.46 baseline
o Improvements in trace support
o Energy Trace ++ support for MSP430
o System Project debug with OptiShare
o Breakpoint view improvements
o Register view improvements
o Real time view updates
o MSPM0 WIR support
o ARM Core Trace
· XDS110 serial number could be corrupted on a split launchpad
· Many build and project system related improvements.
· Trace decoding may take up to 20 seconds for large captures.
· PC Hibernation affects CCS Theia inter-process communication with Resource Explorer opened. You may see a message “Error communicating with Cloud Agent “. Also, a notification panel in bottom right will be shown indicating that CCS Theia has gone offline. Please choose Restart option to restart CCS Theia and re-establish IPC communication.
· New Theia-based IDE:
· Compilers
o TI CLANG 3.2.2 LTS, C2800 Compiler Tools v22.6.1 and MSP430 Compiler Tools v21.6.1.LTS compilers are bundled
· Device Support
o MSPM0: Recommended for production development.
o MSP430: Recommended for production development
o Wireless connectivity (not WiFi): Optional
o C2000: Evaluation, not recommended for production development.
Name
Version
ARM Clang Compiler Tools
v3.2.2.LTS
BlackHawk Emulator Drivers
v9.0.0.002
C2000 Device Support
v6.20.0.0
C2000 Emulation Flash
v1.0.0.5
C2000_FEATURE_METADATA
v6.20.0.0
C2800 Compiler Tools
v22.6.1.A23259
C6000 Compiler Tools
v8.3.12
CC26xx Device Support
v3.19.0.12
CC3220 Device Support
v1.0.5
CC323X Device Support
v1.0.5
CC32xx Device Support
v1.0.8
CC32xx Driver Support
v1.0.8
Debug Server
v12.7.0.3382
Debug Server Flash
v12.7.0.3382
MSP430 Build Header Support
v11.1.0.20211104
MSP430 Compiler Tools
v21.6.1.LTS
MSP430 Debug Support
v11.1.0.20211104
MSP430 Device Support
v11.1.0.20211104
MSP430 GCC Build Header Support
v11.1.0.20211104
MSP432 Debug Support
v8.2.3.0
MSVC 2015+ Redistributable
v14.34.31938
Mmwave Radar Device Support
v1.7.9
Node.js
v18.16.0
SEGGER J-Link
v7.96.0
SEGGER J-Link USB Driver
v1.0.1.0
Shared Device Support
v1.1.7
Sys Config
v1.20.0.3587
TI Cloud Agent
v0.5.4757
TIREX Desktop
v4.16.0.202401192252
Eclipse
v1.4.0.202404221345
MSPM0 Support
v1.09.01.01
Main CCS Theia Installer
v1.4.0.20240419092215
Sitara Device Support
v1.6.7
Sitara MCU Device Support
v1.3.2
TI Emulators
v12.7.0.00130
Theia
v1.4.0.20240424230213
MSPM0 Support
v1.09.01.01
Windows 10 and Windows 11 are all trademarks and/or registered trademarks of Microsoft Corporation.
OSX, macOS are trademarks of Apple.
MSPM0, MSP430, GUI Composer, C2000, Code Composer Studio, XDS110 are trademarks
of Texas Instruments.
Ubuntu is a trademark of Canonical.
J-Link is a trademark of Segger.
© Copyright 2024