Release Notes for Code Composer Studio™ Theia v1.3.1
These release notes contain valuable information which may not be included in other product documentation. This information will assist you in the use of Code Composer Studio™ Theia.The release notes are divided into five sections:
Contents
CCS Theia is a new Integrated Development Environment (IDE) based on Theia IDE framework. CCS Theia v1.3.1 uses a modified version of Theia-IDE. ( https://theia-ide.org/ )
CCS Theia has a more limited set of features and limited set of devices. Each release will add support for new features and new devices.
For additional information and support, please go to:
https://software-dl.ti.com/ccs/esd/documents/users_guide_ccs_theia/index.html
Please note that Code Composer Studio Theia v1.3.1 is recommended for production development with MSPM0, MSP430 devices. CCS Theia includes optional support for Wireless connectivity (not WiFi) devices and evaluation support for C2000 devices.
Please note that Code Composer Studio Theia is a 64bit application and thus will not run on 32bit operating systems.
Supported distributions include:
Code Composer Studio Theia will run on other distributions but those are the officially supported and tested distributions. For more details on installation instructions as well as debug probe and device support please see this article on Linux Host Support.
Versions Supported
Each Code Composer Studio Theia release is validated against a set of macOS releases. This release was validated with:
Debug Probe Support
Details of the macOS releases, debug probes and devices supported is available here.
Please note that use of anti-virus software or a firewall may cause issues during installation.
McAfee software in particular has been especially troublesome.
If possible, disable anti-virus and firewall software during installation.
If not, use of the Offline Installer is strongly recommended.On Windows:
If you are using an Offline CCS Theia Installer, the zip file in which it is
distributed must first be extracted:1. Right-click on CCSTheia1.x.x.xxxxx_win64.zip and select "Extract All...".
2. Enter the directory where you wish to extract the files.
3. Click on Extract.Once extraction has successfully completed, proceed with the installation steps below.
To install Code Composer Studio Theia:1. Run ccs_theia_setup_1.x.x.xxxxx.exe.
2. Choose where you want to install.
3. Select the components you wish to install.On OS X:
Please visit https://software-dl.ti.com/ccs/esd/documents/ccs_macos_host_support.html
The offline installer is now distributed as disk images (.dmg files)
1. Right-click on CCSTheia1.x.x.xxxxx_osx.dmg and select "Open”. This will open the disk image and mount it.
To install Code Composer Studio Theia:1. Run ccs_theia_setup_1.x.x.xxxxx by clicking on the application in the Finder
2. Choose where you want to install.
3. Select the components you wish to install.On Linux:
Please visit https://software-dl.ti.com/ccs/esd/documents/ccs_linux_host_support.html
before installing CCS Theia on Linux. It contains important information on
installing CCS Theia on different Linux distributions, including CCS Theia dependencies that may need to be installed first.
Before installing CCS Theia, the tarball file in which the CCS Theia Installer is distributed must first be extracted:untar CCSTheia1.x.x.xxxxx_linux-x64.tar.gz and extract all files.
e.g. tar xfz CCSTheia1.x.x.xxxxx_linux-x64.tar.gz
Once extraction has successfully completed, proceed with the installation steps below.
Note: To facilitate the installation of emulation drivers, it is necessary to run part of the installation process as root.
You may if you wish install all of CCS Theia as root. However, it is preferred that you first install CCS Theia as a normal user and then install the drivers as root.
To install Code Composer Studio Theia as a normal user and emulation drivers as root:1. Run ccs_theia_setup_1.x.x.xxxxx.run as a normal user.
2. Choose where you want to install.
3. Select the components you wish to install.
4. Navigate to directory <Install-Folder>/ccs/install_scripts.
5. As root, execute script "install_drivers.sh".To install all of Code Composer Studio Theia as root:
1. Run ccs_theia_setup_1.x.x.xxxxx.run as root.
2. Choose where you want to install.
3. Select the components you wish to install.
· V1.3.1 is a maintenance release to address issues related to multi-core debug and C2x core trace. No new features are included.
· Prevent the selected debug context from unexpectedly changing on a multi-core device.
· The trace view may become blank when switching cores on a multi-core device.
· It may not be possible to start a debug session on older MacOS versions (v11 and earlier).
· For devices that support “fake standby”, it may not be possible to run the target once this mode is entered.
· Updated MSPM0 device support package.
· PC Hibernation affects CCS Theia inter-process communication with Resource Explorer opened. You may see a message “Error communicating with Cloud Agent “. Also, a notification panel in bottom right will be shown indicating that CCS Theia has gone offline. Please choose Restart option to restart CCS Theia and re-establish IPC communication.
· New Theia-IDE based IDE:
· Compilers
o TI CLANG 3.2.1 LTS, C2800 Compiler Tools v22.6.1 and MSP430 Compiler Tools v21.6.1.LTS compilers are bundled
· Device Support
o MSPM0: Recommended for production development.
o MSP430: Recommended for production development
o Wireless connectivity (not WiFi): Optional
o C2000: Evaluation, not recommended for production development.
name
version
ARM Clang Compiler Tools (linux64/osx/win64)
V3.2.1.LTS
C2800 Compiler Tools (linux64/osx/win64)
v22.6.1.LTS
CCS Certificate (win64)
vmaster
CCS Installer (linux64/osx/win64)
v1.3.0.20240125125742
CCS Installer Dependencies (win64)
v1.0.0.20170130000000
CCS Installer Dependencies (linux64/osx)
v1.0.0.20180710000000
CCS Utilities (win64/linux64/osx)
v1.0.0.20221028
Debug Server (linux64/osx/win64)
v12.7.0.3313
Debug Server Flash (linux64/osx/win64)
v12.7.0.3313
Eclipse (linux64/osx/win64)
v4.23.0.0
Theia-ide (linux64/osx/win64)
V1.40
IDE GUI Composer (linux64/osx/win64)
v3.3.0
InstallBuilder (linux64/osx/win64)
v21.9.0
JRE (linux64/osx/win64)
v17.0.2
MSP430 Compiler Tools (linux64/osx/win64)
v21.6.1.LTS
MSP430 Support (linux64/osx/win64)
v11.1.0.20211104
MSPM0 Support (linux64/osx/win64)
v1.07.00.02
MSVC 2017 Redistributable (x64) (win64)
v14.34.31938
Node.js (linux64/osx/win64)
V18.16.0
Shared Device Support (linux64/win64)
v1.1.7
Segger J Link
V7.94.0
Sys Config (linux64/osx/win64)
v1.19.0.3426
TI Cloud Agent (linux64/osx/win64)
V0.5.4671
TI Emulators (linux64/osx/win64)
v12.7.0.00062
TIREX4 Desktop (linux64/osx/win64)
v4.16.0.202401192252
Windows 10 and Windows 11 are all trademarks and/or registered trademarks of Microsoft Corporation.
OSX, macOS are trademarks of Apple.
MSPM0, MSP430, GUI Composer, C2000, Code Composer Studio, XDS110 are trademarks
of Texas Instruments.
Ubuntu is a trademark of Canonical.
J-Link is a trademark of Segger.
© Copyright 2024