UCD Power Sequencer Studio Release Notes

Table of Contents

Introduction

The UCD Power Sequencer Studio communicates with the UCD91xxx device via an I2C electrical interface using the PMBus™ command protocol. Users will be able to interact with the graphical user interface (GUI) provided to both send these commands to the device and also recieve data on the device status, displayed on the GUI.

This is version 1.01.00 of the UCD Power Sequencer Studio.

Documentation

What’s New

This release includes the following updates.

Known Limitations