Code Composer Studio for Linux README
-----------------------------------------

If you are using an Offline CCS Installer, the zip file in which it is
distributed must first be extracted:

    1. unzip CCSxx.x.x.xxxxx_linux.zip 
    2. cd CCS_xx.x.x.xxxxx_linux

Once extraction has successfully completed, proceed with the installation
steps below.
To install Code Composer Studio:

    1. Execute ccs_setup_xx.x.x.xxxxx.run
    2. Choose where you want to install.
    3. Select the components you wish to install.

In order to complete the installation, please run the script 
${ccsinstalldir}/install_scripts/install_drivers.sh as administrator.