--
Manifest template 1.0
This template is used to generate A PLAIN TEXT Uploadable manifest for SRAS.
Table Instructions:
Define what you are delivering by filling in the table below. Tables start with the start keyword
end with the end keyword,
and may also contain footnotes specific to that table.
You can have as many “Public” tables as you like in your manifest and can name them. You can have one and only one “Private” table.
To create additional tables copy everything starting with and then paste it after the table below.
The field “attribute =” can be set to Public (the default) or Private to define the type of table it is. If the table is Public then
everything in the table will appear on your manifest. If the table is Private then none of the entries will appear on your manifest
but they will be stored in the SRAS. Private tables are useful for documenting third party code, that requires Legal review, but does
not need to be acknowledged on the manifest you ship; e.g. it may be covered by our TI license.
The field “name = “ is used to put a heading over the table on the manifest you ship.
The field “description =” is used to put a description under the Table name on the manifest you ship.
To learn how to document software in the table read the instructions here. A brief explanation of the table columns follows.
License Type - If its an SPDX defined license use their short name identifier. You can see a list here: http://spdx.org/licenses/ . If
it’s not on the list and not a commercial or TSPA license then use the application name as the license.
Delivered As - This field will either be “Source”, “Binary” or “Source and Binary” and is the form the content of the Software is
delivered in. If the Software is delivered in an archive format, this field applies to the contents of the archive. If the word
Limited is used with Source, as in “Limited Source” or “Limited Source and Binary” then only portions of the Source for the
application are provided.
Modified by TI - This field will either be “Yes” or “No”. A “Yes” means TI has made changes to the Software. A “No” means TI
has not made any changes. Note: This field is not applicable for Software “Obtained from” TI.
Location - The directory name and path on the media, e.g. drive, (or in an archive) where the Software is located after
installing or extracting.
Obtained From - This field specifies from where or from whom TI obtained the Software. It may be a URL to an Open Source site,
a 3rd party licensor, or TI (if TI developed the software). See Links Disclaimer in the Disclaimers Section.
-->
Version = “1.0”
Sep = “|”
Tool=”Hand”
<-- ** Do not edit or remove anything above this line **
-->
<--
Instructions:
DO NOT Alter the column headings below. The order is extremely important; if you change the order or add or
remove a column the upload will not work. When adding a row to the table below you must account for each column.
If a column does not have a value add it, but leave it blank. Each column should appear on its own line and start
with the | character.
Here is an example row for a BSD application written by TI:
| TI application
| 1.0
| BSD-3-Clause
| Source
| N/A
| [as installed]/*
| Texas Instruments
-->
attribute = “Public”
name = “DRV7308EVM SENSORLESS SOFTWARE Manifest Table”
description = “See the Legend above for a description of these columns.”
| DRV7308EVM SENSORLESS SOFTWARE
| 1.0.0
| TI Commercial
| Source
| N/A
| [installed path]/*
| Texas Instruments
| Boot ROM for f28p55x
| Rev 1
| TI Commercial
| Source
| N/A
| [installed path]/src_device/boot_rom/*
| Texas Instruments
| F28P55x Device Support
| 5.02.00.00
| BSD-3-Clause
| Source
| N/A
| [installed path]/src_device/device_support/*
| Texas Instruments
| F28P55x Driver Library
| 5.02.00.00
| BSD-3-Clause
| Source
| N/A
| [installed path]/src_device/driverlib/*, [installed path]/src_device/driverlib.lib
| Texas Instruments
| IQMath
| 1.68.00.00
| TI Text File
| Binary
| N/A
| [installed path]/src_device/boot_rom/source/iqmath/*
| Texas Instruments
| Scale Factor Optimization (SFO) Library
| 8.00.00.00
| TI Text File
| Binary
| N/A
| [installed path]/src_sta/hrpwm/*
| Texas Instruments
| C2000Ware MotorControl SDK Libraries
| 5.01.00.00
| BSD-3-Clause
| Source and Binary
| N/A
| [installed path]/libraries/*
| Texas Instruments
<-- Instructions: Use this section to place footnotes you may have for the table above or just any notes in general. To do a footnote DO NOT use the Microsoft word footnote capability. Instead use an old fashioned (number), e.g. (1) in the table above. All notes must between the Footnotes … footnotes block. Anything outside of this will not work. Do not remove this text. It will not appear on your manifest..-->
<-- Instructions: Some open source licenses may require a specific credit or attribution in product documentation. Those credits should be listed here and all credits should fit between the Credits … credit block. Anything outside of this will not work. Do not remove this text. It will not appear on your manifest. -->
<-- Instructions: Place a unique copy of each Open Source license referenced in the table above here and any OSS licenses that require attribution. All license text should fit between the Licenses …licenses block. Anything outside of this will not work. Do not remove this text. It will not appear on your manifest. -->
-------------------------------------------------------------------------------------
C2000 Device Support, Driver Library, C2000Ware MotorControl SDK Libraries Licenses
-------------------------------------------------------------------------------------
Texas Instruments BSD-3-Clause
Copyright (C) 2023 Texas Instruments Incorporated - http://www.ti.com/
Redistribution and use in source and binary forms, with or without
modification, are permitted provided that the following conditions
are met:
Redistributions of source code must retain the above copyright
notice, this list of conditions and the following disclaimer.
Redistributions in binary form must reproduce the above copyright
notice, this list of conditions and the following disclaimer in the
documentation and/or other materials provided with the
distribution.
Neither the name of Texas Instruments Incorporated nor the names of
its contributors may be used to endorse or promote products derived
from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
"AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
(INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
-------------------------------------------------------------------------------------
C2000 Scale Factor Optimization (SFO) Libraries License
-------------------------------------------------------------------------------------
Copyright: Copyright (C) 2023 Texas Instruments Incorporated -
All rights reserved not granted herein.
Limited License.
Texas Instruments Incorporated grants a world-wide, royalty-free,
non-exclusive license under copyrights and patents it now or hereafter
owns or controls to make, have made, use, import, offer to sell and sell
("Utilize") this software subject to the terms herein. With respect to the
foregoing patent license, such license is granted solely to the extent that
any such patent is necessary to Utilize the software alone. The patent
license shall not apply to any combinations which include this software,
other than combinations with devices manufactured by or for TI
("TI Devices").
No hardware patent is licensed hereunder.
Redistributions must preserve existing copyright notices and reproduce this
license (including the above copyright notice and the disclaimer and
(if applicable) source code license limitations below) in the documentation
and/or other materials provided with the distribution.
Redistribution and use in binary form, without modification, are permitted
provided that the following conditions are met:
* No reverse engineering, decompilation, or disassembly of this software is
permitted with respect to any software provided in binary form.
* Any redistribution and use are licensed by TI for use only
with TI Devices.
* Nothing shall obligate TI to provide you with source code for the
software licensed and provided to you in object code.
If software source code is provided to you, modification and redistribution
of the source code are permitted provided that the following conditions
are met:
* any redistribution and use of the source code, including any resulting
derivative works, are licensed by TI for use only with TI Devices.
* any redistribution and use of any object code compiled from the source
code and any resulting derivative works, are licensed by TI for use
only with TI Devices.
Neither the name of Texas Instruments Incorporated nor the names of its
suppliers may be used to endorse or promote products derived from this
software without specific prior written permission.