Understanding the Ultrasonic Sensing Solution Library
=====================================================

Software Architecture
---------------------

The USS SW Library is split into three main components:

-  **Precompiled code** - Enables running the pre-define set of algorithms developed by Texas Instruments to calculate DtoF, AToF and volume flow rate.
-  **Source code** -
-  Enables configuration of USS and USS\_A module for ultrasonic firing and capture sequences

   -  If running the library on `EVM430-FR6043 <http://www.ti.com/tool/evm430-fr6043>`__ it allows users to control external circuitry on the EVM.

-  **USS SW Library Configuration files** - The following files allows configuration of the library in addition to calibration files. For more information regarding modifying the library configuration file please refer to `Modifying USS SW Library Configuration files <#modify>`__

The image below shows the software architecture of the library.

.. figure:: images/USS_SW_Library_Arquitecture.png
   :alt: USS SW Library Architecture

   USS SW Library Architecture

Folder Structure
----------------

From the root directory, the following folders are available:

-  **docs/** - Contains all documentation related to the USS SW Library plugin
-  **examples/** - Contains all of the code examples and their IDE project files
-  **include/** - Contains USS SW Library in addition to IQmathLib and QmathLib header files
-  **lib/** - Contains the following CCS and IAR libraries
-  Full version of USS SW Library

   -  Non-Algorithmic portion of the library is provided in source code
   -  Algorithmic portion is provided in pre-compiled libraries form with support for different code and memory models

-  Memory Optimized USS SW Libraries

   -  pre-compiled libraries supporting specific algorithms combinations for different code and memory models
   -  for more details on memory optimized libraries please refer to the following section

-  MSP-IQMATHLIB pre-compiled libraries are included in this directory.