![]() |
![]() |
|
MSP430UltrasonicLibrary
02_20_00_16
|
#include <msp430.h>#include <stdint.h>#include <stdbool.h>#include "ussSwLib.h"#include "USS_Lib_HAL.h"#include "common/ussSwLibCommonSAPH.h"#include "common/ussSwLibCommonSDHS.h"#include "common/ussSwLibCommonHSPLL.h"#include "common/ussSwLibCommonUSS.h"#include "common/USSGenericRegDef.h"
Functions | |
| USS_message_code | USS_updateSDHSConfiguration (USS_SW_Library_configuration *config) |
| The following function updates the SDHS module configuration based on user defined USS_Capture_Configuration struct in "ussSwLib_userConfig.c". Note: This API must be called everytime a USS_Capture_Configuration parameter is updated. This API performs the following SDHS module configuration. More... | |
| USS_message_code | USS_updateHSPLLConfiguration (USS_SW_Library_configuration *config) |
| The following function updates the HSPLL module configuration based on user defined USS_HSPLL_Configuration struct in "ussSwLib_userConfig.c". Note1: This API must be called everytime a USS_HSPLL_Configuration parameter is updated. Note2: If "pllOutputFreq_inHz" is modified in USS_HSPLL_Configuration struct, user must call USS_updateSDHSCapture API since SDHS modulator optimization bits might need to be updated. This API performs the following HSPLL module configuration checks: More... | |
| USS_message_code | USS_updateSAPHConfiguration (USS_SW_Library_configuration *config) |
| The following function updates the SAPH module configuration based on user defined USS_Measurement_Configuration struct in "ussSwLib_userConfig.c". Note: This API must be called everytime a USS_Measurement_Configuration parameter is updated. This API performs the following SAPH module configuration checks: More... | |
| USS_message_code | USS_updateUUPSConfiguration (USS_SW_Library_configuration *config) |
| The following function updates the UUPS module configuration based on user defined USS_Trigger_Configuration struct in "ussSwLib_userConfig.c". Note1: This API must be called every time a USS_Trigger_Configuration parameter is updated. Note2: This API will assert HSPLL.PLLXTEN bit when USS_Triger_Configuration_RTC_Timer_Trigger, USS_Triger_Configuration_External_Trigger1 or USS_Triger_Configuration_External_Trigger2. Selecting USS_Triger_Configuration_Software_Trigger will deassert HSPLL.PLLXTEN bit. This API performs the following checks: More... | |
| USS_message_code | USS_updateUSSInterruptsConfiguration (USS_SW_Library_configuration *config) |
| The following function updates the UUPS module interrupt configuration based on user defined USS_Interrupt_Configuration struct in "ussSwLib_userConfig.c". Note: This API must be called every time an USS_Interrupt_Configuration parameter is updated. This API performs the following checks: More... | |
| USS_message_code | USS_resetUSSModule (USS_SW_Library_configuration *config, bool reconfigUSSModule) |
| This function allows application to reset the USS module. It is recommended that this API is used when an USS SW Library API return a HSPLL unlock error. The API allows user to control the reconfiguration of the measurement. If reconfigUSSModule == true then the measurement is reconfigured. If reconfigUSSModule == false then the USS module will have the default module configuration after a power-up clear (PUC) reset. Note: This functionality is only available in MSP430FR604x Rev B or later silicon. If the code is running on Rev A silicon and this API is called the API will return the following error message USS_meesage_code_silicon_version_does_not_support_this_functionality, it is recommended that the application checks the API return message code to confirm the USS module have been reset successfully. More... | |