![]() |
![]() |
|
MSP430UltrasonicLibrary
02_20_00_16
|
This structure is passed to USS_verifyHSPLLFrequency API and test result will be returned using this structure. More...
#include <ussSwLib.h>
Data Fields | |
| uint32_t | expectedResult |
| uint32_t | actualTestCount |
| Contains the average SAPH timer counts in 1 ACLK period. More... | |
| int32_t | difference |
| Contains the difference between expected and actualTestCount SAPH. More... | |
This structure is passed to USS_verifyHSPLLFrequency API and test result will be returned using this structure.
| uint32_t _USS_calibration_hspll_results_::expectedResult |
Contains the expected Test count value. this is calculated based on USS_HSPLL_Configuration and USS_System_Configuration parameters
Referenced by USS_verifyHSPLLFrequency().
| uint32_t _USS_calibration_hspll_results_::actualTestCount |
Contains the average SAPH timer counts in 1 ACLK period.
Referenced by USS_verifyHSPLLFrequency().
| int32_t _USS_calibration_hspll_results_::difference |
Contains the difference between expected and actualTestCount SAPH.
Referenced by USS_verifyHSPLLFrequency().