![]() |
![]() |
|
MSP430UltrasonicLibrary
02_20_00_16
|
The following structure allows user to specify single and dual tone configuration. More...
#include <ussSwLib.h>
Data Fields | |
| uint8_t | F1DutyCycle |
| uint8_t | F2DutyCycle |
| uint8_t | numOfF1Cycles |
| uint8_t | numOfF2Cycles |
The following structure allows user to specify single and dual tone configuration.
| uint8_t _USS_Pulse_Single_Dual_Tone_Configuration_::F1DutyCycle |
In single tone mode, it specifies the single tone duty cycle. In dual tone mode, it specifies the first tone duty cycle.
Referenced by commonConfigurePPGDutyCyle(), and commonValidateSAPHconfigruation().
| uint8_t _USS_Pulse_Single_Dual_Tone_Configuration_::F2DutyCycle |
In dual tone mode, it specifies the second tone duty cycle. In single tone mode, this parameter is not used.
Referenced by commonConfigurePPGDutyCyle(), and commonValidateSAPHconfigruation().
| uint8_t _USS_Pulse_Single_Dual_Tone_Configuration_::numOfF1Cycles |
In single tone, specifies the number on the single tone cycles. In dual tone, it specifies the number of first tone cycles.
Referenced by commonConfigurePPGDutyCyle(), and commonValidateSAPHconfigruation().
| uint8_t _USS_Pulse_Single_Dual_Tone_Configuration_::numOfF2Cycles |
In dual tone, specifies the number cycles for the second tone cycles. In single tone mode, this parameter is not used.
Referenced by commonConfigurePPGDutyCyle(), and commonValidateSAPHconfigruation().