![]() |
![]() |
|
MSP430UltrasonicLibrary
02_20_00_16
|
Contains USS SW Lib HSPLL Configuration. More...
#include <ussSwLib.h>
Data Fields | |
| USS_HSPLL_input_clock_freq | ussXtalFreq |
| USS_HSPLL_input_clock_type | HSPLLInputCLKType |
| USS_HSPLL_output_clk_freq | pllOutputFreq |
| bool | outputPLLXtal |
| uint16_t | hspllTolerance |
| uint16_t | ussXTALsettlingCount |
Contains USS SW Lib HSPLL Configuration.
| USS_HSPLL_input_clock_freq _USS_HSPLL_Configuration_::ussXtalFreq |
Referenced by commonValidateHSPLLconfiguration(), and USS_updateHSPLLConfiguration().
| USS_HSPLL_input_clock_type _USS_HSPLL_Configuration_::HSPLLInputCLKType |
Referenced by USS_updateHSPLLConfiguration().
| USS_HSPLL_output_clk_freq _USS_HSPLL_Configuration_::pllOutputFreq |
If this paramater is modified during runtime, two update APIs need to called; USS_updateHSPLLConfiguration and USS_updateSDHSCapture. USS_updateSDHSCapture needs to be select the correct modulator optimization bits and obtain maximum performance of the SDHS based on the new HSPLL frequency.
Registers modified:HSPLL.CTL.PLLM and SAPH.CTL7.MODOPTI
Referenced by commonGetHSPLLFreqInHz(), commonSDHSConfigModOpt(), commonValidateHSPLLconfiguration(), commonValidateSAPHconfigruation(), commonValidateSDHSconfigruation(), USS_updateHSPLLConfiguration(), and USS_verifyHSPLLFrequency().
| bool _USS_HSPLL_Configuration_::outputPLLXtal |
true = outputs HSPLL crystal , false = does not outputs HSPLL crystal
Registers modified:HSPLL.PLLXTCTL.XTOUTOFF
Referenced by USS_updateHSPLLConfiguration().
| uint16_t _USS_HSPLL_Configuration_::hspllTolerance |
number of hspll cycle variance tolerance. Value can be between 0-255 This parameter is required when calling USS_verifyHSPLLFrequency
Referenced by USS_verifyHSPLLFrequency().
| uint16_t _USS_HSPLL_Configuration_::ussXTALsettlingCount |
Specifies the number of LFXT cycles needed to allow USS XT to settle. ussXTALsettlelingCount = ceiling[(LFXTFrequency_inHz)*(settling_in_Sec)] For example if settling time for USSXT is 120usec and LFXTFrequency is configure for 32768 Hz. Then ussXTALsettlelingCount = ceiling[(32768)*(120e-6)] = 4 Please refer to the device datasheet for recommended USSXT settling time ussXTALsettlelingCount must a non-zero positive value Please also refer to USS_startLowPowerUltrasonicCapture API for more detail regarding this parameter usage during low power capture.
Referenced by commonStabilizeOscillator(), commonValidateHSPLLconfiguration(), and USS_commonTriggerSingleCapture().