HCI_EXT_SetRxGainDone
---------------------
:Opcode: 0x0400
:Event Description: This event is sent to indicate the RF receiver gain has been set, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_SetTxPowerDone
----------------------
:Opcode: 0x0401
:Event Description: This event is sent to indicate the RF transmitter power has been set, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_OnePacketPerEventDone
-----------------------------
:Opcode: 0x0402
:Event Description: This event is sent to indicate the One Packet Per Event feature has been enabled or disabled, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_DecryptCommandDone
--------------------------
:Opcode: 0x0405
:Event Description: This event is sent to indicate Decryption has completed.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table

:Decrypted Data: 128 bit decrypted data block. The most significant octet of plainTextData corresponds to plainTextData using the notation specified in FIPS 197.

 :Size: 16 byte(s)
 :Range: Any 16 byte value


HCI_EXT_WriteLocalFeatureSupportDone
------------------------------------
:Opcode: 0x0406
:Event Description: This event is sent to indicate the Set Local Supported Features command has completed.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_SetFastTxResponseTimeDone
---------------------------------
:Opcode: 0x0407
:Event Description: This event is sent to indicate the Set Fast Transmit Response Time feature has been enabled or disabled, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_SetBDADDRDone
---------------------
:Opcode: 0x040C
:Event Description: This event is sent to indicate the devices BLE address has been set, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_SetSCADone
------------------
:Opcode: 0x040D
:Event Description: This event is sent to indicate the devices SCA has been set, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_DisconnectImmedDone
---------------------------
:Opcode: 0x0413
:Event Description: This event is sent to indicate the Disconnect Immediate command has completed, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_PER
-----------
:Opcode: 0x0414
:Event Description: This event is sent to indicate the Packet Error Rate Reset or Read command has completed, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table

:PER Command Type: Read or Reset

 :Size: 1 byte(s)
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0                     Reset PER Counters
         1                     Read PER Counters
         ===================== ========================================================

:RX Pkts: Number of received packets.

 :Condition: ( cmdVal!=0x00 && cmdStat==0x00)
 :Size: 2 byte(s)
 :Range: Any 2 byte value

:RX CRC Fails: Number of received packets with CRC error.

 :Condition: ( cmdVal!=0x00 && cmdStat==0x00)
 :Size: 2 byte(s)
 :Range: Any 2 byte value

:Events: Number of connection events.

 :Condition: ( cmdVal!=0x00 && cmdStat==0x00)
 :Size: 2 byte(s)
 :Range: Any 2 byte value

:Missed Events: Number of missed connection events.

 :Condition: ( cmdVal!=0x00 && cmdStat==0x00)
 :Size: 2 byte(s)
 :Range: Any 2 byte value



HCI_EXT_ResetSystemDone
-----------------------
:Opcode: 0x041D
:Event Description: This event is sent to indicate the Reset System command has completed, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_NumComplPktsLimitDone
-----------------------------
:Opcode: 0x041F
:Event Description: This event is sent to indicate the Number Completed Packets Limit command has completed, or that there was an error.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table


HCI_EXT_GetConnInfoDone
-----------------------
:Opcode: 0x0420
:Event Description: This event is sent to indicate the Get Connection Information command has completed.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table

:Alloc Conns: Total number of allocated connections

 :Size: 1 byte(s)
 :Range: 

:Active Conns: Number of currently active connections

 :Size: 1 byte(s)
 :Range: 


An array of size "numConn" will be returned containing the parameters starting here:

:Conn Handle: Connection Handle

 :Size: 1 byte(s)
 :Range: 

:Conn Role: 

 :Size: 1 byte(s)
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x22                  LMP/LL Response Timeout
         0x23                  LMP Error Transaction Collision
         0x24                  LMP PDU Not Allowed
         0x25                  Encryption Mode Not Acceptable
         0x26                  Link Key Can Not be Changed
         0x27                  Requested QoS Not Supported
         0x28                  Instant Passed
         0x29                  Pairing With Unit Key Not Supported
         0x2A                  Different Transaction Collision
         0x2B                  Reserved
         0x2C                  QoS Unacceptable Parameter
         0x2D                  QoS Rejected
         0x2E                  Channel Assessment Not Supported
         0x2F                  Insufficient Security
         0x30                  Parameter Out Of Mandatory Range
         0x31                  Reserved
         0x32                  Role Switch Pending
         0x33                  Reserved
         0x34                  Reserved Slot Violation
         0x35                  Role Switch Failed
         0x36                  Extended Inquiry Response Too Large
         0x37                  Simple Pairing Not Supported By Host
         0x38                  Host Busy - Pairing
         0x39                  Connection Rejected Due To No Suitable Channel Found
         0x3A                  Controller Busy
         0x3B                  Unacceptable Connection Interval
         0x3C                  Directed Advertising Timeout
         0x3D                  Connection Terminated Due To MIC Failure
         0x3E                  Connection Failed To Be Established
         0x3F                  MAC Connection Failed
         0x40                  Coarse Clock Adjust Rejected
         0x41                  Type0 Submap Not Defined
         0x42                  Unknown Advertising Identifier
         0x43                  Limit Reached
         0x44                  Operation Cancelled by Host
         ===================== ========================================================

:Peer Addr: 

 :Size: 6 byte(s)
 :Range: 

:Peer Addr Type: 

 :Size: 1 byte(s)
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x00                  Public
         0x01                  Random
         0x02                  Public Identity
         0x03                  Random Identity
         ===================== ========================================================


The array of parameters ends here.

HCI_EXT_SetMaxDataLengthDone
----------------------------
:Opcode: 0x0421
:Event Description: This event is sent to indicate the Set Max Data Length command has completed.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table




HCI_EXT_LLTestModeDone
----------------------
:Opcode: 0x0470
:Event Description: LL Test Mode event.

**Event Parameters**

:Status: 

 :Size: 1 byte(s)
 :Range: See Status Table

:Command Opcode: 

 :Size: 2 byte(s)
 :Range: See Command Table