The Network Terminal Application
*********************************

The **Network Terminal** example provide a command-line interface that enables running basic operations.
The following menu should appear on the terminal. 
 
	.. figure:: resources/IMG-NetworkTerminal.png
	   :scale: 100%
	   :width: 720px	

	   Terminal Network Example
 
 | Typing ``help`` will show this menu.
 | Typing the name of a command will show the required parameters.
 | The role (AP or station) should be started before any other command, e.g. with ``wlan_sta_role_up`` or ``wlan_ap_role_up``.
 | Starting an access-point will enable mobile devices to connect to the CC33XX.
 | Starting a station role will enable commands such as ``wlan_scan`` and ``wlan_connect``.
 | Once connected to an access point, you can use ``send` and ``receive`` (over LWIP - the reference network stack).
 | For more details on the application, check the example's ``README`` file.