.. _`CC33XX Host-Driver Porting Guide`: ../porting-guide.html
.. _`CC33XX Getting Started Guide`: getting-started.html


Software Overview
*****************
The software development kit directory structure is broken down into a few major directories at the root to allow 
easy differentiation between documentation, examples, and other source code. From the root directory, 
the sub-directories are:

* ``docs/``: All documentation for the SDK
* ``examples/``: Source code and project definitions for example projects in the SDK
* ``source/drivers/net/wifi``: Source code for the cc33xx Wi-Fi driver (and pre-built libraries)
* ``source/net/wifi_interface``: Wi-Fi stack API (see wlan_commands.h)
* ``source/third_party``: 3rd party software
* ``tools/``: CC33xx firmware and programming scripts 


System Architecture
===================

This figure shows a block diagram of the CC33xx + Sitara MCU solution at a high level.
For **MCU hosts**, this CC33XX package introduces the **Thick-MAC** concept where the WPA Supplicant and the connection management are implemented within the CC33XX device. 
This configuration reduces the footprint of the host application and simplifies the Wi-Fi control.
Note that having the Supplicant inside the device is different from the **Linux Transceiver** partitioning used by the **MPU** based hosts.   

.. figure:: resources/BD-CC33XX-ThickMAC.png
    :name: fig-cc33xx-thick-mac-block-diagram
    :align: center

    Thick MAC block Diagram

In this solution, there is an external serial flash that stores the Sitara AM243x application image. 
Upon boot, the application image will be copied to the host's internal RAM and run from it.
The CC33XX firmware and bootloader code are also stored on the flash. The CC33xx host driver will install the firmware on the CC33XX device whenever the application turns on Wi-Fi. 
Check `CC33XX Getting Started Guide`_ for more details on running an application.
The AM243x communicates with the CC33xx over SPI. For more details on the host interface, see the `CC33XX Host-Driver Porting Guide`_.