HCI_EXT_SetRxGainDone¶
| Opcode: | 0x0400 |
|---|---|
| Event Description: | |
| This event is sent to indicate the RF receiver gain has been set, or that there was an error. | |
Event Parameters
| Status: |
|
||||
|---|---|---|---|---|---|
| Command Opcode: |
|
HCI_EXT_SetTxPowerDone¶
| Opcode: | 0x0401 |
|---|---|
| Event Description: | |
| This event is sent to indicate the RF transmitter power has been set, or that there was an error. | |
Event Parameters
| Status: |
|
||||
|---|---|---|---|---|---|
| Command Opcode: |
|
HCI_EXT_OnePacketPerEventDone¶
| Opcode: | 0x0402 |
|---|---|
| Event Description: | |
| This event is sent to indicate the One Packet Per Event feature has been enabled or disabled, or that there was an error. | |
Event Parameters
| Status: |
|
||||
|---|---|---|---|---|---|
| Command Opcode: |
|
HCI_EXT_DecryptCommandDone¶
| Opcode: | 0x0405 |
|---|---|
| Event Description: | |
| This event is sent to indicate Decryption has completed. | |
Event Parameters
| Status: |
|
||||
|---|---|---|---|---|---|
| Command Opcode: |
|
||||
| Decrypted Data: | 128 bit decrypted data block. The most significant octet of plainTextData corresponds to plainTextData using the notation specified in FIPS 197.
|
HCI_EXT_WriteLocalFeatureSupportDone¶
| Opcode: | 0x0406 |
|---|---|
| Event Description: | |
| This event is sent to indicate the Set Local Supported Features command has completed. | |
Event Parameters
| Status: |
|
||||
|---|---|---|---|---|---|
| Command Opcode: |
|
HCI_EXT_SetFastTxResponseTimeDone¶
| Opcode: | 0x0407 |
|---|---|
| Event Description: | |
| This event is sent to indicate the Set Fast Transmit Response Time feature has been enabled or disabled, or that there was an error. | |
Event Parameters
| Status: |
|
||||
|---|---|---|---|---|---|
| Command Opcode: |
|
HCI_EXT_SetBDADDRDone¶
| Opcode: | 0x040C |
|---|---|
| Event Description: | |
| This event is sent to indicate the devices BLE address has been set, or that there was an error. | |
Event Parameters
| Status: |
|
||||
|---|---|---|---|---|---|
| Command Opcode: |
|
HCI_EXT_SetSCADone¶
| Opcode: | 0x040D |
|---|---|
| Event Description: | |
| This event is sent to indicate the devices SCA has been set, or that there was an error. | |
Event Parameters
| Status: |
|
||||
|---|---|---|---|---|---|
| Command Opcode: |
|
HCI_EXT_DisconnectImmedDone¶
| Opcode: | 0x0413 |
|---|---|
| Event Description: | |
| This event is sent to indicate the Disconnect Immediate command has completed, or that there was an error. | |
Event Parameters
| Status: |
|
||||
|---|---|---|---|---|---|
| Command Opcode: |
|
HCI_EXT_PER¶
| Opcode: | 0x0414 |
|---|---|
| Event Description: | |
| This event is sent to indicate the Packet Error Rate Reset or Read command has completed, or that there was an error. | |
Event Parameters
| Status: |
|
||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|
| Command Opcode: |
|
||||||||||
| PER Command Type: | |||||||||||
Read or Reset
|
|||||||||||
| RX Pkts: | Number of received packets.
|
||||||||||
| RX CRC Fails: | Number of received packets with CRC error.
|
||||||||||
| Events: | Number of connection events.
|
||||||||||
| Missed Events: | Number of missed connection events.
|
||||||||||
HCI_EXT_ResetSystemDone¶
| Opcode: | 0x041D |
|---|---|
| Event Description: | |
| This event is sent to indicate the Reset System command has completed, or that there was an error. | |
Event Parameters
| Status: |
|
||||
|---|---|---|---|---|---|
| Command Opcode: |
|
HCI_EXT_NumComplPktsLimitDone¶
| Opcode: | 0x041F |
|---|---|
| Event Description: | |
| This event is sent to indicate the Number Completed Packets Limit command has completed, or that there was an error. | |
Event Parameters
| Status: |
|
||||
|---|---|---|---|---|---|
| Command Opcode: |
|
HCI_EXT_GetConnInfoDone¶
| Opcode: | 0x0420 |
|---|---|
| Event Description: | |
| This event is sent to indicate the Get Connection Information command has completed. | |
Event Parameters
| Status: |
|
||||
|---|---|---|---|---|---|
| Command Opcode: |
|
||||
| Alloc Conns: | Total number of allocated connections
|
||||
| Active Conns: | Number of currently active connections
|
An array of size “numConn” will be returned containing the parameters starting here:
| Conn Handle: | Connection Handle
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| Conn Role: |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Peer Addr: |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Peer Addr Type: |
|
The array of parameters ends here.
HCI_EXT_SetMaxDataLengthDone¶
| Opcode: | 0x0421 |
|---|---|
| Event Description: | |
| This event is sent to indicate the Set Max Data Length command has completed. | |
Event Parameters
| Status: |
|
||||
|---|---|---|---|---|---|
| Command Opcode: |
|
HCI_EXT_LLTestModeDone¶
| Opcode: | 0x0470 |
|---|---|
| Event Description: | |
| LL Test Mode event. | |
Event Parameters
| Status: |
|
||||
|---|---|---|---|---|---|
| Command Opcode: |
|