The Network Terminal Application

The Network Terminal example provide a command-line interface that enables running basic operations. The following menu should appear on the terminal.

../../_images/IMG-NetworkTerminal.png

Fig. 9 Terminal Network Example

Typing help will show this menu.
Typing the name of a command will show the required parameters.
The role (AP or station) should be started before any other command, e.g. with wlan_sta_role_up or wlan_ap_role_up.
Starting an access-point will enable mobile devices to connect to the CC33XX.
Starting a station role will enable commands such as wlan_scan and wlan_connect.
Once connected to an access point, you can use send` and ``receive (over LWIP - the reference network stack).
For more details on the application, check the example’s README file.