NimBLE Bluetooth Stack¶
Overview¶
Apache Mynewt offers the world’s first fully open-source Bluetooth Low Energy (BLE) or Bluetooth Smart stack fully compliant with Bluetooth 5 specifications. It is called NimBLE.
Features¶
- NimBLE complies with Bluetooth Core Specification 5.0 which makes it an ideal wireless technology for the Internet of Things (IoT).
- LE Advertising Extensions
- 2M PHY for higher throughput
- Coded PHY for LE Long Range
- High Duty Cycle Non-Connectable Advertising
- Channel Selection Algorithm #2 to utilize channels in more efficient way
- LE Privacy 1.2 for frequent changes to the device address to make it difficult to track for outsiders
- LE Secure Connections featuring FIPS-compliant algorithms
- LE Data Length Extension for higher throughput
Host Component¶
- Logical Link Control and Adaptation Protocol (L2CAP): provides logical channels, named L2CAP channels, which are multiplexed over one or more logical links to provide packet segmentation and reassembly, flow control, error control, streaming, QoS etc.
- Security Manager (SM): uses Security Manager Protocol (SMP) for pairing and transport specific key distribution for securing radio communication
- Attribute protocol (ATT): allows a device (Server) to expose certain pieces of data, known as Attributes, to another device (Client)
- Generic Attribute Profile (GATT): a framework for using the ATT protocol to exchange attributes encapsulated as Characteristics or Services
- Generic Access Profile (GAP): a base profile which all Bluetooth devices implement, which in the case of LE, defines the Physical Layer, Link Layer, L2CAP, Security Manager, Attribute Protocol and Generic Attribute Profile
- Host Controller Interface (HCI): the interface between the host and controller either through software API or by a hardware interface such as SPI, UART or USB
Software Architecture¶
APIs¶
NimBLE-APIs reference can be found on the MyNewt website