AM243 Guide¶
Overview¶
This Getting Started Guide demonstrates how to start evaluating the CC33xx “Thick MAC”. The reference platform contains the AM243x LaunchPad (AM243x-LP) and the CC33xx Lx Base Board. Below are the instructions for building and running the Wi-Fi example (Network Terminal) from the CC33xx MCU package on the reference platform. The MCU package is a plugin that is based on content (such as TI drivers for peripherals, LWIP network stack, FreeRTOS OS adaptation) available in the base SDK (MCU-PLUS-AM243X-SDK). Guidance about porting to other platforms is available through the CC33XX Host-Driver Porting Guide.
Prerequisites¶
- Hardware
- Software
- MCU-PLUS-AM243X-SDK (version 08.05.00.24)
- Follow the AM243 Getting Started Guide to get AM243 up and running
- CC33XX_MCU_package
- CCS 10.3 and up
- TI_Clang 1.3.0 LTS
- Python 3.7 (see instructions in Sitara LP Manual)
- SysConfig version 1.19 or below
Folder Structure of “cc33xx_mcu_package”¶
- ccs_projects/ - Projects to build required libraries
- ble_host_nimble
- ble_interface
- lwip
- wifi_host_driver
- wifi_interface
- wifi_platform_cc33xx
- docs/ - User guides and API references
- examples/ - Example applications
- CC3xx_ble_wifi_provisioning
- CC3xx_thick_mac_network_terminal
- source/ - Drivers and libraries source code
- Wi-Fi Stack API is under source/ti/net/wifi_interface
- cc33xx Driver is under source/ti/drivers/net/wifi
- NimBLE Stack is under source/third_party/nimble
- tools/ -
- programing - contains flash programming (Python) scripts
- wifi_fw - contains CC33xx .bin files
Setup - Sitara AM243x and CC33xx¶
For Information on the Sitara LaunchPad please refer to LP-AM243_EVM-SETUP.
To use the CC3301 with Linux you may stack the CC3301 BoosterPack to the Sitara EVM LP-AM243. When connecting make sure to align the 5v and GND of both boards to result in the picture below;
The table below shows the header pin interface between the AM243 LaunchPad and the BP-CC3301. For more information on the header pin assignment for the BP-CC3301, please refer to the BP-CC33XX Hardware User’s Guide.
| Sitara Pin | BP-CC3301 | Description |
|---|---|---|
| 21 | P1.21 | 5V |
| 22 | P1.22 | GND |
| 3 | P1.3 | LP-AM243:RX / BP-CC3301: TX |
| 4 | P1.4 | LP-AM243:TX / BP-CC3301: RX |
| 5 | P1.5 | nRESET |
| 8 | P1.8 | WLAN IRQ |
| 7 | P1.7 | SPI CLK |
| 37 | P2.37 | BP-CC3301: CTS |
| 38 | P2.36 | BP-CC3301: RTS |
| 18 | P2.18 | SPI CS |
| 14 | P2.15 | SPI PICO |
| 15 | P2.14 | SPI POCI |
Power Connections:
Connect the Sitara to its power supply and to the PC.
Note
The Sitara needs a 5V / 3A power supply. When powered correctly, 3 green LEDs will turn on.
When Disconnecting/Connecting the Sitara, always make sure you do it in the following sequence:
PLUG IN Connect Power (USB-C), then Connect Data (micro USB) PLUG OUT Disconnect Data (Micro USB), then Disconnect Power (USB-C)
Import projects and compile in CCS¶
- Go to
File->Import - Choose
C/C++ -> CCS Projects - Browse… ->
<cc33xx_mcu_package>/ - Choose all -
wifi_host_driver,wifi_platform_cc33xx,wifi_stack_interface,lwip,ble_host_nimble,ble_interfaceandCC3xxx_network_terminal - First compile the Wi-Fi and BLE projects, then compile the
network_terminalapplication
Program the Flash¶
Before running the example, the RAM bootloader and CC33xx Firmware need to be programmed to the flash on the AM243.
The content of the 3 files can be found under <cc33xx_mcu_package>/tools/wifi_fw.
Note
The image is loaded and executed from the AM243x MSRAM. To save RAM space the binaries are stored in the flash and read during the FW init.
The binaries should be programmed to a pre-defined offset in the flash, as shown below:
Binary Name Description Location Offset <app-name>.appimage Application Image (see 3) under app project output folder 0x00080000 cc33xx_fw.bin CC33XX Firmware under tools/cc33xx_firmware/ 0x00800000 cc33xx_2nd_loader.bin RAM Bootloader under tools/cc33xx_firmware/ 0x00900000 The application image programming is optional. The application image can be executed from flash (see run from flash)
After the successful compilation of the application, the binary image (
.appimageor.appimage.hs_fs(for secure devices) file, e.g.cc3xxx_network_terminal.appimage) can be found in the Release/ folder inside the project.
Programming Instructions:¶
Configure the LaunchPad to UART boot according to AM243x UART Boot Mode.
If you are using a secure MCU (LP-AM243 PROC1093B or newer) - open the
<cc33xx_mcu_package>/tools/secured_programmingfolder (in a command line window). If you are using an older LP version - move to the<cc33xx_mcu_package>/tools/programming/folder.Set up the programmer’s configuration file (if needed, see below)
In the secured_programming folder, there are 2 configuration files:
only_wifi_fw.cfg- contains just the Firmware binariesprogram_application_and_wifi_fw.cfg- contains both the Firmware binaries and the application image.
By default the
program_application_and_wifi_fw.cfgis set to the default locations of the firmware. The location of the application imagecc3xxx_network_terminal.appimage.hs_fswill need to be set manuallyRun the uart_uniflash.py python script:
In Windows:
python3 uart_uniflash.py -p COM<XDS uart number> --cfg=<config-file-edited-in-step-3>.cfgIn Linux:
python3 uart_uniflash.py -p /dev/ttyACM<XDS uart number> --cfg=<config-file-edited-in-step-3>.cfgexample:
python3 uart_uniflash.py -p /dev/ttyACM3 --cfg=only_wifi_fw.cfg
Below is a screenshot of a successful execution:
Exit from UART boot (return the switch pins).
Run the example from flash¶
When loading the code from flash (make sure to follow step 3.b in the Programing instructions), configure the LP for AM243x QSPI Boot Mode.
- Open a serial terminal (see Serial Terminal Configuration).
- Pressing the reset button (see platform_figure) on the launchpad will trigger the application.
Serial Terminal Configuration:¶
COM Port: Listed asApplications/User UART(see note below)Baud-rate: 115200Data bits: 8Stop bits: 1Parity: NoneFlow Control: NoneNote
The COM port can be determined via Device Manager in Windows or via ls /dev/tty* in Linux.