CC33XX API Documentation  2.30.00.15
Public Attributes | List of all members
device_info_t Struct Reference

Public Attributes

uint8_t mac_address [(4)][(6)]
 
uint8_t struct_is_updateed
 
uint8_t fuse_rom_structure_version
 
uint8_t device_part_number
 
uint8_t boot_rom_version
 
uint8_t pg_version
 
uint8_t metal_version
 
uint8_t disable_5g
 
uint8_t disable_6g
 
uint8_t disable_ble
 
uint64_t udi
 

The documentation for this struct was generated from the following file: