CC33XX API Documentation  2.30.00.15
Public Attributes | List of all members
dbg_cntr_trnspt_t Struct Reference

Public Attributes

uint32_t counters_timeLastReset_Ms
 
uint32_t counters_timeLastUpdate_Ms
 
uint32_t txRate
 
uint32_t link_tx_dbgStackTimeFirstPacket_Ms
 
uint32_t link_tx_dbgStackTimeLastPacket_Ms
 
uint32_t link_tx_dbgStackEntrNumByteSent
 
uint32_t link_tx_dbgStackEntNumPktsXfered
 
uint32_t link_tx_dbgTimeFirstPacket_Ms
 
uint32_t link_tx_dbgTimeLastPacket_Ms
 
uint32_t link_tx_dbgNumPktsSent
 
uint32_t link_tx_dbgNumBytesSent
 
uint32_t link_tx_dbgNumPktsBusy
 
uint32_t link_tx_dbgNumPktsAcBusy
 
uint32_t link_tx_dbgNumPktsXfered
 
uint32_t link_tx_dbgNumPktsSuccess
 
uint32_t link_tx_dbgNumPktsError
 
uint32_t link_tx_dbgNumTxCmplt
 
uint32_t link_tx_dbgNumTxCmpltOk
 
uint32_t link_tx_dbgNumTxCmpltError
 
uint32_t link_tx_dbgNumTxCmpltOkBytes
 
uint32_t link_tx_dbgNumTxCmpltFailBytes
 
uint32_t rxRate
 
uint32_t rxstat_RecvOk
 
uint32_t rxstat_DirectedBytesRecv
 
uint32_t rxstat_DirectedFramesRecv
 
uint32_t rxstat_MulticastBytesRecv
 
uint32_t rxstat_MulticastFramesRecv
 
uint32_t rxstat_BroadcastBytesRecv
 
uint32_t rxstat_BroadcastFramesRecv
 
uint32_t link_rx_recvFromWlan
 
uint32_t link_rx_recvBytesFromWlan
 
uint32_t link_rx_sendToUwd
 
uint32_t link_rx_sendToDataDispatcher
 
uint32_t link_rx_discardWrongHlid
 
uint32_t link_rx_discardHlidClose
 
uint32_t link_rx_discardBaEvent
 
uint32_t link_rx_discardUnknownClass
 

The documentation for this struct was generated from the following file: